2038252_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2038252_en-US

2038252_en-US

Build Error for Android 15.0.0_1.0.0 BSP Source

Hi,

I downloaded the Android 15.0.0_1.0.0 (L6.6.52_2.2.0 BSP) source from the NXP site and attempted to build it. However, I encountered the following error while compiling several .cpp files:


~/imx-android-15/android_build$ lunch evk_8mp-trunk_staging-userdebug
~/imx-android-15/android_build$ ./imx-make.sh -j11 2>&1
(...)
d3d346dec8/obj/hardware/nxp/wlan/wifi_hal/wifi_hal.o.d -o out/soong/.intermediates/hardware/nxp/wlan/wifi_hal/libwifi-hal-nxp/android_vendor_arm64_armv8-a_cortex-a53_static_cfi/e560d7b19ebf7276b3e850d3d346dec8/obj/hardware/nxp/wlan/wifi_hal/wifi_hal.o hardware/nxp/wlan/wifi_hal/wifi_hal.cpp
In file included from hardware/nxp/wlan/wifi_hal/wifi_hal.cpp:43:
hardware/nxp/wlan/wifi_hal/common.h:22:10: fatal error: 'wifi_hal.h' file not found
   22 | #include "wifi_hal.h"
      |          ^~~~~~~~~~~~
1 error generated.
[  2% 1044/42576] //frameworks/opt/net/wifi/libwifi_system_iface:libwifi-system-iface clang++ interface_tool.cpp
ninja: build stopped: subcommand failed.
09:56:02 ninja failed with: exit status 1

#### failed to build some targets (02:05 (mm:ss)) ####


* Build Host: Ubuntu Desktop 22.04 LTS

* EVK : i.MX 8M Plus

It seems that the issue is caused by the absence of the wifi_hal.h file in the hardware/nxp/wlan/wifi_hal directory.


Could you please provide guidance on how to resolve this issue?


Re: Build Error for Android 15.0.0_1.0.0 BSP Source

Hi, Harvey,


I followed your instructions, and the build succeeded.

Thanks,

Best regards,

David KS

Re: Build Error for Android 15.0.0_1.0.0 BSP Source

Hi,

Please follow up the guide - ANDROID_USERS_GUIDE 

Configuration example as below

i.MX 8M Plus EVK board $ lunch evk_8mp-nxp_stable-userdebug


Regards

Harvey

标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 08:40 PM
更新人: