2037499_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2037499_en-US

2037499_en-US

S32K1xx lpUART driver Implement

Hello NXP Teams

I'm using the SW32K1_S32M24x FreeRTOS 10.5.1 library and would like to add a UART driver under the driver layer.

Is there any sample code I can reference?

UART_driver.png


thank you

Re: S32K1xx lpUART driver Implement

Hi,

trying selecting IP level demo example, there is just IP level components

 

2025-02-06_12-22-28.png2025-02-06_12-23-33.png

BR, Petr

Re: S32K1xx lpUART driver Implement

Hi PetrS

I have imported the example project from S32K1 AUTOSAR R21-11 RTD 2.0.0 P04 D2404 Example Project, but this sample project only includes examples for the MCAL layer.

I would like to implement peripheral devices at the driver layer.
Is there any sample project available for download?

thank you

Example ProjectExample ProjectExample ProjectMACL layerMACL layerMACL layerDriver layerDriver layerDriver layer

Re: S32K1xx lpUART driver Implement

Hi,

you can refer to RTD demo directly

 

BR, Petr

Re: S32K1xx lpUART driver Implement

Hi PetrS,

Thank you for your reply.

Since there is no demo code for implementing peripherals on the driver layer with FreeRTOS, could you kindly provide sample code for peripheral devices at the driver layer?

I appreciate your help!

peripherals_device.png 

 

Re: S32K1xx lpUART driver Implement

Hi,

I am not aware of RTD demo for this, but maybe you can refer to below example using SDK
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/EXAMPLE-S32k144-UART-printf-scanf-unde...

BR, Petr

Re: S32K1xx lpUART driver Implement

FreeRTOS_Lib.png

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 08:41 PM
更新者: