2032492_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2032492_en-US

2032492_en-US

S32K1xx SDK in S32DS

Hello,

I'm using S32DS 2018.R1 for years. I want to upgrade to v3.6.0, But I'm not able to find the latest S32 SDK in zip format. I installed the exe version, but it does not seem to be usable in S32DS. 

Why doesn't the zip version appear in the download area ? Where is it available ?

I already asked on this thread, with no answers : SDK in zip where to download - NXP Community

Thank you for supporting

Franck

Re: S32K1xx SDK in S32DSThanks. Very clear and helpful :Re: S32K1xx SDK in S32DS

Personally I have tested the above mentioned RTDs with the S32DS 3.6 without any issues (so far). Additionally, some customers are using it the same way.

However officially, it is recommended to follow the installation flow of each RTD in its respective release notes.

On the other hand, you do not need to uninstall the 3.6 , you can have both of them (3.5 and 3.6 versions) installed at the same time.

Re: S32K1xx SDK in S32DS

Hi,

Thank you for this answer. Very helpful !

You mention the latest version is fully tested with S32DS 3.5. Do you expect it to work with S32DS 3.6, or should I uninstall it and stick to 3.5 ?

Thanks again for the support

Franck

Re: S32K1xx SDK in S32DS

Hi,

Thank you so much for your interest in our products and for using our community.

There is no more SDK updates. Now we provide Real Time Drivers (RTD). You can found them in the following way:

For S32K1, please go to Design Resources -> Software -> Real-Time Drivers for S32K1 -> Automotive SW - S32K1_S32M24x - Real-Time Drivers for Cortex-M

For S32K3, please go to Design Resources -> Software -> S32K3 Standard Software -> Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M

The latest RTD version for S32K1 is the patch S32K1_S32M24X Real Time Drivers AUTOSAR R21-11 Version 2.0.0 P04, however you need to install the S32K1_S32M24X Real Time Drivers AUTOSAR 4.4 & R21-11 Version 2.0.0 before.

The latest RTD version for S32K3 is the S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 5.0.0.

At the moment both of them are fully tested in S32DS 3.5. Please follow the installation flow of each RTD in its respective release notes.

Hope it helps you.

Have a nice day!

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 11:32 AM
更新者: