2030939_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2030939_en-US

2030939_en-US

FEE_Example_S32K344 does not work, inits with Null_PTR

The example from the RTD for FEE_Example_s32k344 does not work as it never initializes due to the MemAcc_init and Fee_init being given Null_PTRs, I have managed to find MemAcc_Config/MemAcc_BOARD_InitPeripherals_Config(for 342) for MemAcc_Init, But i cannot find the Fee_ConfigType define for Fee_Init, am I missing an RTD update or something?

pb632146_0-1737421837405.png

pb632146_1-1737421895027.png



Re: FEE_Example_S32K344 does not work, inits with Null_PTRThe example actually works if I remove all the example assertions which appear to be reading incorrectly? The functions work if the example asserts are skipped over.

Now I am more confused on why the example on 342 does not function.
Re: FEE_Example_S32K344 does not work, inits with Null_PTRAny suggestion as to what may be issue of MEMIF_UNINIT?Re: FEE_Example_S32K344 does not work, inits with Null_PTRThis is being run on the S32K3X4EVB-T172
Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 11:38 AM
Updated by: