2030511_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2030511_en-US

2030511_en-US

Documentation_OTA_Secure-Boot_88MW320

There are no documents, only examples. Please help me find the required documents

Re: Documentation_OTA_Secure-Boot_88MW320

Hi,

I will answer you in the internal case.

Regards,

Daniel.

Re: Documentation_OTA_Secure-Boot_88MW320

Hello, 

Please help with some document that explains the workflows, or any general secureboot.c, secureboot.h and boot.c and boot.h files would work for me. 

Additionally if there would be documents explaining the MQTT and HTTP flow it will be really helpful.  @DanielRuvalcaba 

Re: Documentation_OTA_Secure-Boot_88MW320

Hello,

What about bootloaders? is there a specific boot.c and boot.h or secureboot.c and secureboot.h

Also, apart from the documents in that SDK bundle, is there anything else that is available? I need something for HTTP, MQTT for application development.


Re: Documentation_OTA_Secure-Boot_88MW320

Hi,

Unfortunately, all the documentation regarding MCUXpresso SDK is the one available in the docs directory of the SDK bundle.

We don’t have a document with specific instructions for secure boot using MCUXpresso SDK.

Regards,

Daniel.

Re: Documentation_OTA_Secure-Boot_88MW320

Hello I am using SDK version 2.9.13 for RDMW320-R0 (88MW320_xx_xxxx) which was downloaded from MCUXpresso SDK builder

The Issue is when I download the documentation generated along with the SDK, I don't getApplication notes or other stuff for OTA, Custom Bootloader Development, Secure Boot, HTTP/HTTPS, MQTT, MbedTLS and similar API's in detail. 

Re: Documentation_OTA_Secure-Boot_88MW320

Hi,

What SDK are you using?

Regards,

Daniel.

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 08:53 PM
Updated by: