2027850_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2027850_en-US

2027850_en-US

S32G3 LLCE 1.0.9 Compatibility with RTD 5.0

Hi,

According to the LLCE release notes, version 1.0.9 was tested on RTD 4.0.2. I’m wondering if it is compatible with RTD 5.0. Upgrading to RTD 5.0 would make the project incompatible with older versions, so if LLCE 1.0.9 doesn’t work with RTD 5.0, I’d prefer to avoid spending time upgrading and then having to downgrade later.

Thanks,

XD

Re: S32G3 LLCE 1.0.9 Compatibility with RTD 5.0

Hello @XD,

I have received updates related to you questions. The LLCE 1.0.9 has being officially tested with RTD 5.0.0. , you can check said information in the S32G Software Offering, please check table Integrated Software Bundle 2024.11. Please not this is a secure file, for which you will need to get access, for this please contact your FAE or NXP representative.

Sorry for the misinformation I shared before.


Best regards

Re: S32G3 LLCE 1.0.9 Compatibility with RTD 5.0

Hi @alejandro_e ,

Thank you for your quick response. I appreciate it.

Thanks,

XD

Re: S32G3 LLCE 1.0.9 Compatibility with RTD 5.0

Hello @XD,

It is good to support you again. As you have seeing already, LLCE 1.0.9 (which is the latest version) was tested with RTD 4.0.2, so that is the officially supported version, although it may properly work with version 5.0.0, this has not being officially tested and therefore we do not have any document indicating if it is compatible or not. So I would recommend keeping version 4.0.2 since, as you said, migrating versions requires some workload and in the end it may be problematic for your project.


Let me know if you have more questions about this topic.

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 08:56 PM
Updated by: