Hello!
I need to count all the write-through requests to the memory hierarchy. To do so, I thought that the Com:55 performance monitor was the best fit. However, in the event collumn it says that the monitor counts "Write-through store translation hits", while the description collumn says that the monitor counts "Write-through stores translated".
It is not clear to me if the Com:55 performance monitor counts write-through store translation hits to the translation lookaside buffer or if it counts all Write-through stores translations. Which interpretation is correct?
Best regards,
Matheus.
1) Yes, correct.
2) Yes, correct.
3) Certainly it does.
"translated" should point to virtual addresses i.e. store hits with enabled cache with write through