2025686_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2025686_en-US

2025686_en-US

S32 K118 Internal clock Lin

I use S32k118, there is no external crystal oscillator, so i use internal clock. 

The problem is that the system is works fine in debug mode.  And If power off, then power on, it can't run normally.

Attached is the clock config. Is there anything special when use internal clock? Could you give me some supports?

Thanks very much!

Re: S32 K118 Internal clock Lin

Solved, Thank you very much!

Re: S32 K118 Internal clock Lin

Hi Jianfeng2,

If you are using S32K1 SDK, please check if "START_FROM_FLASH" Symbols are missing? refer to the discussion:   S32K188 runs with debugger, but not witout

If you suspect the clock is inaccurate, please observe the frequency of internal clock through the CLKOUT pin.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 08:58 PM
更新者: