Hello
I'm designing a new product using the IMXRT1062 controller. I've already interfaced with SRAM and verified that it's working. I'm now planning to interface with SDRAM as well, so that I can access both SRAM and SDRAM as needed.
Is it possible to interface with both SRAM and SDRAM using the IMXRT1062?
Hi @VishalAvg ,
Thanks for your interest in NXP MIMXRT series!
Yes, this can be done with SEMC. The SEMC is a multi-standard memory controller optimized for both high-performance and low pin-count. It can support multiple external memories in the same application with shared address and data pins. The interfaces supported include SDRAM, NOR Flash, SRAM, NAND Flash, and 8080 display interface.
Best regards,
Gavin