! This is the command i build for the imx93evk
$ mkdir imx-yocto-bsp
$ cd imx-yocto-bsp
$ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml
$ repo sync
$ mkdir -p downloads
$ cd downloads
$ mkdir linux-imx; cd linux-imx
$ git clone https://github.com/nxp-imx/linux-imx.git
$ cd ../..
$ export BSPDIR=$(pwd)
$ DISTRO=fsl-imx-wayland MACHINE=imx93-11x11-lpddr4x-evk source imx-setup-release.sh -b buildwayland
$ bitbake imx-image-multimedia
after building finish, the directory
imx-yocto-bsp/buildwayland/tmp/sysroots-components/imx93_11x11_lpddr4x_evk/imx-boot/boot
will contain
imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot
! is using
$ sudo ./uuu -b emmc_all imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot
! a correct way to update the image that reflect the kernel changes i made in the linux-imx?
! what is the recommended way to only build the linux kernel and replace the kernel only,
is it
$ cd linux-imx
$ make imx93_11x11_evk_defconfig
$ make
! and which image should i burn specifically for replacing the kernel?
BR, Colin
When you finish rebuild you can use the scp commend to copy the kernel images to your board
Here do you just need to rebuilt and update the kernel on the board?