2018385_ja-JP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2018385_ja-JP

2018385_ja-JP

S32G-VNP-RDB3 100BASE-T1ポートを開く方法。

こんにちは。

S32G-VNP-RDB3ボードを使用しています。私はyoctoビットベイクBSP42.0(fsl-image-auto)を使用しています。SDカードから起動します。

100BASE-T1(MOLEX MINI 50 J53)で100BASE-T1を使いたいです。

100BASE-T1 SJA1110 ポート: P10(100BASE-T1) を有効にする方法の次のアクションを教えてください。

どうもありがとうございます。

Wzlinux_0-1734938266392.png 

次はブートアップログです。

NOTICE:  Reset status: Power-On Reset
NOTICE:  BL2: v2.10.0   (release):bsp42.0-2.10
NOTICE:  BL2: Built : 19:50:36, Sep 12 2024
NOTICE:  BL2: Booting BL31


U-Boot 2022.04+g5a6f62071f+p0 (Sep 06 2024 - 07:11:20 +0000)

SoC:   NXP S32G399A rev. 1.0
CPU:   ARM Cortex-A53 r0p4 @ max 1300 MHz
Model: NXP S32G399A-RDB3
DRAM:  3.5 GiB
Core:  306 devices, 25 uclasses, devicetree: board
MMC:   FSL_SDHC: 0
Loading Environment from MMC... OK
s32cc_serdes_phy serdes@40480000: Using mode 0 for SerDes subsystem
pci_s32cc pcie@40400000: Configuring as RootComplex
pci_s32cc pcie@40400000: Failed to get link up
In:    serial@401c8000
Out:   serial@401c8000
Err:   serial@401c8000
Board revision: RDB3 Revision E
PCIe:   BusDevFun       VendorId   DeviceId   Device Class       Sub-Class
__________________________________________________________________________
pcie@40400000 RootComplex
|   `-- 01:00.00        0x1957     0x4300     Bridge device           0x04
Net:
Warning: ethernet@4033c000 (eth0) using random MAC address - 7e:d8:f2:25:32:d4
eth0: ethernet@4033c000
Found PFE version 0x0101 (S32G3)
PFEng firmware file 'mmc@0:1:s32g_pfe_class.fw' loading failed: -2

Found PFE version 0x0101 (S32G3)
PFEng firmware file 'mmc@0:1:s32g_pfe_class.fw' loading failed: -2

Found PFE version 0x0101 (S32G3)
PFEng firmware file 'mmc@0:1:s32g_pfe_class.fw' loading failed: -2

Hit any key to stop autoboot:  0
switch to partitions #0, OK
mmc0 is current device
15415304 bytes read in 646 ms (22.8 MiB/s)
Booting from mmc ...
60416 bytes read in 7 ms (8.2 MiB/s)
## Flattened Device Tree blob at 83000000
   Booting using the fdt blob at 0x83000000
   Using Device Tree in place at 0000000083000000, end 0000000083011bff
   fixup: pfe1: update phy addr to 0x8
Failed to configure XPCS1_1
Failed to update XPCS1 for SerDes1

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 6.6.32-rt32-g49d9f8bb25e0-dirty (oe-user@oe-host) (aarch64-fsl-linux-gcc (GCC) 11.4.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT Thu Sep 12 09:32:29 UTC 2024
[    0.000000] Machine model: NXP S32G3 Reference Design Board (S32G-VNP-RDB3)
[    0.000000] earlycon: linflex0 at MMIO 0x00000000401c8000 (options '115200n8')
[    0.000000] printk: legacy bootconsole [linflex0] enabled
[    0.000000] OF: reserved mem: 0x0000000034000000..0x000000003407ffff (512 KiB) nomap non-reusable pfebufs@34000000
[    0.000000] OF: reserved mem: 0x0000000034080000..0x000000003409ffff (128 KiB) nomap non-reusable pfebufs@34080000
[    0.000000] Reserved memory: created DMA memory pool at 0x0000000083200000, size 3 MiB
[    0.000000] OF: reserved mem: initialized node pfebufs@83200000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x0000000083200000..0x00000000835dffff (3968 KiB) nomap non-reusable pfebufs@83200000
[    0.000000] OF: reserved mem: 0x00000000835e0000..0x00000000835fffff (128 KiB) map non-reusable pfebufs@835e0000
[    0.000000] OF: reserved mem: 0x0000000084000000..0x0000000084ffffff (16384 KiB) nomap non-reusable shm@84000000
[    0.000000] OF: reserved mem: 0x00000000c0000000..0x00000000c03fffff (4096 KiB) nomap non-reusable shm@c0000000
[    0.000000] OF: reserved mem: 0x00000000c0400000..0x00000000c07fffff (4096 KiB) nomap non-reusable shm@c0400000
[    0.000000] OF: reserved mem: 0x00000000d0000000..0x00000000d000007f (0 KiB) nomap non-reusable shm@d0000000
[    0.000000] OF: reserved mem: 0x00000000d0000080..0x00000000d00000ff (0 KiB) nomap non-reusable shm@d0000080
[    0.000000] OF: reserved mem: 0x00000000ff600000..0x00000000ff7fffff (2048 KiB) nomap non-reusable atf@ff600000
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   [mem 0x0000000100000000-0x00000008dfffffff]
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x00000000831fffff]
[    0.000000]   node   0: [mem 0x0000000083200000-0x00000000835dffff]
[    0.000000]   node   0: [mem 0x00000000835e0000-0x0000000083ffffff]
[    0.000000]   node   0: [mem 0x0000000084000000-0x0000000084ffffff]
[    0.000000]   node   0: [mem 0x0000000085000000-0x00000000bfffffff]
[    0.000000]   node   0: [mem 0x00000000c0000000-0x00000000c07fffff]
[    0.000000]   node   0: [mem 0x00000000c0800000-0x00000000cfffffff]
[    0.000000]   node   0: [mem 0x00000000d0001000-0x00000000ff5fffff]
[    0.000000]   node   0: [mem 0x00000000ff600000-0x00000000ff7fffff]
[    0.000000]   node   0: [mem 0x00000000ff800000-0x00000000ffffffff]
[    0.000000]   node   0: [mem 0x0000000880000000-0x00000008dfffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008dfffffff]
[    0.000000] On node 0, zone DMA: 1 pages in unavailable ranges
[    0.000000] cma: Reserved 256 MiB at 0x00000000ef600000 on node -1
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] psci: SMC Calling Convention v1.4
[    0.000000] percpu: Embedded 19 pages/cpu s40040 r8192 d29592 u77824
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] CPU features: detected: ARM errata 1165522, 1319367, 1530923, or 1530924
[    0.000000] alternatives: applying boot alternatives
[    0.000000] Kernel command line: console=ttyLF0,115200 root=/dev/mmcblk0p2 rootwait rw earlycon
[    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 903167
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] software IO TLB: area num 8.
[    0.000000] software IO TLB: mapped [mem 0x00000000eb600000-0x00000000ef600000] (64MB)
[    0.000000] Memory: 3223892K/3670012K available (9536K kernel code, 654K rwdata, 2928K rodata, 1792K init, 219K bss, 183976K reserved, 262144K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=8, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000]  Trampoline variant of Tasks RCU enabled.
[    0.000000]  Tracing variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 544 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] GICv3: MBI range [167:182]
[    0.000000] GICv3: Using MBI frame 0x0000000050800000
[    0.000000] Root IRQ handler: gic_handle_irq
[    0.000000] GICv3: GICv3 features: 16 PPIs
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000050900000
[    0.000000] ITS: No ITS available, not enabling LPIs
[    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[    0.000000] arch_timer: cp15 timer(s) running at 5.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x127350b88, max_idle_ns: 440795202120 ns
[    0.000001] sched_clock: 56 bits at 5MHz, resolution 200ns, wraps every 4398046511100ns
[    0.008361] Console: colour dummy device 80x25
[    0.012452] Calibrating delay loop (skipped), value calculated using timer frequency.. 10.00 BogoMIPS (lpj=20000)
[    0.022658] pid_max: default: 32768 minimum: 301
[    0.027357] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.034649] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.044061] RCU Tasks: Setting shift to 3 and lim to 1 rcu_task_cb_adjust=1.
[    0.050739] RCU Tasks Trace: Setting shift to 3 and lim to 1 rcu_task_cb_adjust=1.
[    0.058406] rcu: Hierarchical SRCU implementation.
[    0.063007] rcu:     Max phase no-delay instances is 1000.
[    0.068849] smp: Bringing up secondary CPUs ...
[    0.073520] Detected VIPT I-cache on CPU1
[    0.073574] GICv3: CPU1: found redistributor 1 region 0:0x0000000050920000
[    0.073609] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[    0.074187] Detected VIPT I-cache on CPU2
[    0.074225] GICv3: CPU2: found redistributor 2 region 0:0x0000000050940000
[    0.074243] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[    0.074769] Detected VIPT I-cache on CPU3
[    0.074804] GICv3: CPU3: found redistributor 3 region 0:0x0000000050960000
[    0.074823] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[    0.075379] Detected VIPT I-cache on CPU4
[    0.075439] GICv3: CPU4: found redistributor 100 region 0:0x0000000050980000
[    0.075467] CPU4: Booted secondary processor 0x0000000100 [0x410fd034]
[    0.076039] Detected VIPT I-cache on CPU5
[    0.076080] GICv3: CPU5: found redistributor 101 region 0:0x00000000509a0000
[    0.076100] CPU5: Booted secondary processor 0x0000000101 [0x410fd034]
[    0.076644] Detected VIPT I-cache on CPU6
[    0.076684] GICv3: CPU6: found redistributor 102 region 0:0x00000000509c0000
[    0.076705] CPU6: Booted secondary processor 0x0000000102 [0x410fd034]
[    0.077304] Detected VIPT I-cache on CPU7
[    0.077345] GICv3: CPU7: found redistributor 103 region 0:0x00000000509e0000
[    0.077366] CPU7: Booted secondary processor 0x0000000103 [0x410fd034]
[    0.077440] smp: Brought up 1 node, 8 CPUs
[    0.203332] SMP: Total of 8 processors activated.
[    0.208009] CPU features: detected: 32-bit EL0 Support
[    0.213141] CPU features: detected: CRC32 instructions
[    0.218323] CPU: All CPU(s) started at EL2
[    0.222342] alternatives: applying system-wide alternatives
[    0.229681] devtmpfs: initialized
[    0.240940] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.250270] futex hash table entries: 2048 (order: 5, 131072 bytes, linear)
[    0.264821] pinctrl core: initialized pinctrl subsystem
[    0.270465] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[    0.276916] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
[    0.283728] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.291487] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.299488] thermal_sys: Registered thermal governor 'step_wise'
[    0.299596] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.312070] ASID allocator initialised with 65536 entries
[    0.317418] Serial: AMBA PL011 UART driver
[    0.321450] scmi_core: SCMI protocol bus registered
[    0.327322] scmi_protocol scmi_dev.1: Enabled polling mode TX channel - prot_id:16
[    0.334786] arm-scmi firmware:scmi: SCMI Notifications - Core Enabled.
[    0.341026] arm-scmi firmware:scmi: SCMI Protocol v2.0 'NXP:S32G399A' Firmware version 0x0
[    0.356015] platform 4009c240.siul2-pinctrl: Fixed dependency cycle(s) with /soc/siul2@4009c000/siul2-pinctrl@4009c240/jtag_pins
[    0.374276] Modules: 28944 pages in range for non-PLT usage
[    0.374283] Modules: 520464 pages in range for PLT usage
[    0.379905] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[    0.391552] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[    0.397803] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[    0.404571] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[    0.410825] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[    0.417591] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[    0.423844] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[    0.430613] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[    0.444571] SCSI subsystem initialized
[    0.448063] usbcore: registered new interface driver usbfs
[    0.453383] usbcore: registered new interface driver hub
[    0.458687] usbcore: registered new device driver usb
[    0.464177] pps_core: LinuxPPS API ver. 1 registered
[    0.468707] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti 
[    0.477829] PTP clock support registered
[    0.482640] vgaarb: loaded
[    0.485222] clocksource: Switched to clocksource arch_sys_counter
[    0.497180] NET: Registered PF_INET protocol family
[    0.501842] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
[    0.511567] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
[    0.519728] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    0.527392] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[    0.535481] TCP bind hash table entries: 32768 (order: 8, 1048576 bytes, linear)
[    0.543762] TCP: Hash tables configured (established 32768 bind 32768)
[    0.549968] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
[    0.556608] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
[    0.563848] NET: Registered PF_UNIX/PF_LOCAL protocol family
[    0.569666] RPC: Registered named UNIX socket transport module.
[    0.575208] RPC: Registered udp transport module.
[    0.579888] RPC: Registered tcp transport module.
[    0.584575] RPC: Registered tcp-with-tls transport module.
[    0.590044] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.596492] PCI: CLS 0 bytes, default 64
[    0.601939] workingset: timestamp_bits=62 max_order=20 bucket_order=0
[    0.608413] fuse: init (API version 7.39)
[    0.612144] NET: Registered PF_ALG protocol family
[    0.616809] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 248)
[    0.624145] io scheduler mq-deadline registered
[    0.628655] io scheduler kyber registered
[    0.632656] io scheduler bfq registered
[    0.639938] s32cc-siul2-pinctrl 4009c240.siul2-pinctrl: initialized s32 pinctrl driver
[    0.648524] s32cc-siul2-gpio 4009d700.siul2-gpio: No cache defaults, reading back from HW
[    0.656358] s32cc-siul2-gpio 4009d700.siul2-gpio: No cache defaults, reading back from HW
[    0.664805] gpio gpiochip0: Static allocation of GPIO base is deprecated, use dynamic allocation.
[    0.673779] s32cc-siul2-gpio 4009d700.siul2-gpio: No cache defaults, reading back from HW
[    0.681583] s32cc-siul2-gpio 4009d700.siul2-gpio: No cache defaults, reading back from HW
[    0.700880] printk: legacy console [ttyLF0] enabled000 (irq = 23, base_baud = 7812500) is a FSL_LINFLEX
[    0.700880] printk: legacy console [ttyLF0] enabled
[    0.710776] printk: legacy bootconsole [linflex0] disabled
[    0.710776] printk: legacy bootconsole [linflex0] disabled
[    0.725708] 401cc000.serial: ttyLF1 at MMIO 0x401cc000 (irq = 24, base_baud = 7812500) is a FSL_LINFLEX
[    0.736947] s32cc_fccu 4030c000.fccu: FCCU status is 0 (normal)
[    0.745126] sja1110-sw@1 enforce active low on GPIO handle
[    0.752978] spi-nor spi6.0: mx25uw51245g (65536 Kbytes)
[    0.758717] 7 fixed-partitions partitions found on MTD device 0.spi
[    0.765085] Creating 7 MTD partitions on "0.spi":
[    0.769858] 0x000000000000-0x000004000000 : "Flash-Image"
[    0.775609] 0x000000000000-0x000000280000 : "FIP"
[    0.780624] 0x000000280000-0x000000290000 : "U-Boot-Env"
[    0.786257] 0x000000290000-0x000001360000 : "Kernel"
[    0.791550] 0x000001360000-0x000001390000 : "DTB"
[    0.796567] 0x000001390000-0x0000032a0000 : "Rootfs"
[    0.801839] 0x0000032a0000-0x000004000000 : "PFE-Firmware"
[    0.808946] vcan: Virtual CAN interface driver
[    0.813465] slcan: serial line CAN interface driver
[    0.818414] CAN device driver interface
[    0.823242] flexcan 401b4000.can: device registered (reg_base=(____ptrval____), irq(s):
[    0.831367] flexcan 401b4000.can:  30
[    0.835085] flexcan 401b4000.can:  31
[    0.838798] flexcan 401b4000.can:  32
[    0.842512] flexcan 401b4000.can:  33
[    0.846224] flexcan 401b4000.can: )
[    0.850474] flexcan 401be000.can: device registered (reg_base=(____ptrval____), irq(s):
[    0.858601] flexcan 401be000.can:  34
[    0.862319] flexcan 401be000.can:  35
[    0.866031] flexcan 401be000.can:  36
[    0.869745] flexcan 401be000.can:  37
[    0.873457] flexcan 401be000.can: )
[    0.877168] e100: Intel(R) PRO/100 Network Driver
[    0.881937] e100: Copyright(c) 1999-2006 Intel Corporation
[    0.887524] e1000: Intel(R) PRO/1000 Network Driver
[    0.892468] e1000: Copyright (c) 1999-2006 Intel Corporation.
[    0.898311] e1000e: Intel(R) PRO/1000 Network Driver
[    0.903343] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[    0.909370] igb: Intel(R) Gigabit Ethernet Network Driver
[    0.914843] igb: Copyright (c) 2007-2014 Intel Corporation.
[    0.921291] hse-uio 40210000.mu0b: firmware not found
[    0.926814] usbcore: registered new interface driver uas
[    0.932233] usbcore: registered new interface driver usb-storage
[    0.939221] imx_usb 44064000.usb: No over current polarity defined
[    0.959778] ci_hdrc ci_hdrc.0: EHCI Host Controller
[    0.964844] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
[    0.985221] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[    0.990844] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 6.06
[    0.999233] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    1.006559] usb usb1: Product: EHCI Host Controller
[    1.011505] usb usb1: Manufacturer: Linux 6.6.32-rt32-g49d9f8bb25e0-dirty ehci_hcd
[    1.019180] usb usb1: SerialNumber: ci_hdrc.0
[    1.024010] hub 1-0:1.0: USB hub found
[    1.027839] hub 1-0:1.0: 1 port detected
[    1.033057] s32cc-rtc 40060000.rtc: registered as rtc0
[    1.038289] s32cc-rtc 40060000.rtc: setting system clock to 1970-01-01T00:00:00 UTC (0)
[    1.046489] i2c_dev: i2c /dev entries driver
[    1.051171] s32cc-wdt 4010c000.watchdog: S32CC Watchdog Timer Registered. timeout=30s (nowayout=0)
[    1.060424] s32cc-wdt 40200000.watchdog: S32CC Watchdog Timer Registered. timeout=30s (nowayout=0)
[    1.069654] s32cc-wdt 40204000.watchdog: S32CC Watchdog Timer Registered. timeout=30s (nowayout=0)
[    1.078886] s32cc-wdt 40208000.watchdog: S32CC Watchdog Timer Registered. timeout=30s (nowayout=0)
[    1.088135] s32cc-wdt 40500000.watchdog: S32CC Watchdog Timer Registered. timeout=30s (nowayout=0)
[    1.097362] s32cc-wdt 40504000.watchdog: S32CC Watchdog Timer Registered. timeout=30s (nowayout=0)
[    1.106593] s32cc-wdt 40508000.watchdog: S32CC Watchdog Timer Registered. timeout=30s (nowayout=0)
[    1.115823] s32cc-wdt 4050c000.watchdog: S32CC Watchdog Timer Registered. timeout=30s (nowayout=0)
[    1.126324] sdhci: Secure Digital Host Controller Interface driver
[    1.132613] sdhci: Copyright(c) Pierre Ossman
[    1.137034] sdhci-pltfm: SDHCI platform and OF driver helper
[    1.142990] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    1.149899] hse 40211000.mu1b: interface mu1b not active
[    1.155642] usbcore: registered new interface driver usbhid
[    1.161298] usbhid: USB HID core driver
[    1.173231] mmc0: SDHCI controller on 402f0000.mmc [402f0000.mmc] using ADMA
[    1.180511] s32-adc 401f8000.adc: using dma0chan4 for ADC DMA transfers
[    1.187644] s32-adc 401f8000.adc: Device initialized successfully.
[    1.205363] s32-adc 402e8000.adc: using dma1chan16 for ADC DMA transfers
[    1.212536] s32-adc 402e8000.adc: Device initialized successfully.
[    1.217139] mmc0: new high speed SDHC card at address aaaa
[    1.224661] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[    1.224888] mmcblk0: mmc0:aaaa SK32G 29.7 GiB
[    1.234181] s32-siul2-nvmem 4009c000.nvram: Initialized s32cc siul2 nvmem driver
[    1.239108]  mmcblk0: p1 p2
[    1.245055] s32-siul2-nvmem 44010000.nvram: Initialized s32cc siul2 nvmem driver
[    1.255917] NET: Registered PF_INET6 protocol family
[    1.261708] Segment Routing with IPv6
[    1.265473] In-situ OAM (IOAM) with IPv6
[    1.269496] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    1.275914] NET: Registered PF_PACKET protocol family
[    1.281162] can: controller area network core
[    1.285612] NET: Registered PF_CAN protocol family
[    1.290472] can: raw protocol
[    1.293482] can: broadcast manager protocol
[    1.297728] can: netlink gateway - max_hops=1
[    1.302201] 8021q: 802.1Q VLAN Support v1.8
[    1.321752] i2c i2c-0: using pinctrl states for GPIO recovery
[    1.327698] i2c i2c-0: using generic GPIOs for recovery
[    1.333202] pca953x 0-0022: using AI
[    1.343874] rtc-pcf85063 0-0051: registered as rtc1
[    1.348859] i2c i2c-0: IMX I2C adapter registered
[    1.353671] i2c i2c-0: using dma0chan5 (tx) and dma0chan6 (rx) for DMA transfers
[    1.361699] i2c i2c-2: using pinctrl states for GPIO recovery
[    1.367578] i2c i2c-2: using generic GPIOs for recovery
[    1.372951] i2c i2c-2: IMX I2C adapter registered
[    1.377762] i2c i2c-2: using dma1chan17 (tx) and dma1chan18 (rx) for DMA transfers
[    1.385899] i2c i2c-4: using pinctrl states for GPIO recovery
[    1.391774] i2c i2c-4: using generic GPIOs for recovery
[    1.398483] ina2xx 4-0040: power monitor ina231 (Rshunt = 1000 uOhm)
[    1.404962] i2c i2c-4: IMX I2C adapter registered
[    1.409767] i2c i2c-4: using dma1chan19 (tx) and dma1chan20 (rx) for DMA transfers
[    1.417904] phy-s32cc-serdes 40480000.serdes: Using mode 0 for SerDes subsystem
[    1.425692] phy-s32cc-serdes 44180000.serdes: Using mode 4 for SerDes subsystem
[    1.654758] s32cc-pcie 40400000.pcie: Failed to stabilize PHY link
[    1.661032] s32cc-pcie 40400000.pcie: Configuring as RootComplex
[    1.667155] s32cc-pcie 40400000.pcie: host bridge /soc/pcie@40400000 ranges:
[    1.674326] s32cc-pcie 40400000.pcie:       IO 0x5ffffe0000..0x5ffffeffff -> 0x0000000000
[    1.682632] s32cc-pcie 40400000.pcie:      MEM 0x5800000000..0x5ffffdffff -> 0x0000000000
[    1.690943] s32cc-pcie 40400000.pcie: Memory resource size exceeds max for 32 bits
[    2.698755] s32cc-pcie 40400000.pcie: Phy link never came up
[    2.704548] s32cc-pcie 40400000.pcie: iATU: unroll T, 6 ob, 4 ib, align 4K, limit 1024G
[    2.712763] s32cc-pcie 40400000.pcie: eDMA: unroll T, 4 wr, 4 rd
[    3.719039] s32cc-pcie 40400000.pcie: Phy link never came up
[    4.724891] s32cc-pcie 40400000.pcie: Phy link never came up
[    4.731110] s32cc-pcie 40400000.pcie: PCI host bridge to bus 0000:00
[    4.737562] pci_bus 0000:00: root bus resource [bus 00-ff]
[    4.743130] pci_bus 0000:00: root bus resource [io  0x0000-0xffff]
[    4.749400] pci_bus 0000:00: root bus resource [mem 0x5800000000-0x5ffffdffff] (bus address [0x00000000-0x7fffdffff])
[    4.760192] pci 0000:00:00.0: [1957:4300] type 01 class 0x060400
[    4.766302] pci 0000:00:00.0: reg 0x10: [mem 0x5800000000-0x58000fffff]
[    4.773023] pci 0000:00:00.0: reg 0x38: [mem 0x5800000000-0x580000ffff pref]
[    4.780262] pci 0000:00:00.0: supports D1
[    4.784330] pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold
[    4.793569] pci 0000:00:00.0: BAR 0: assigned [mem 0x5800000000-0x58000fffff]
[    4.800816] pci 0000:00:00.0: BAR 6: assigned [mem 0x5800100000-0x580010ffff pref]
[    4.808498] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[    4.814030] pcieport 0000:00:00.0: PME: Signaling with IRQ 52
[    4.820780] s32cc-dwmac 4033c000.ethernet: IRQ eth_wake_irq not found
[    4.827319] s32cc-dwmac 4033c000.ethernet: IRQ eth_lpi not found
[    4.833796] s32cc-dwmac 4033c000.ethernet: User ID: 0x10, Synopsys ID: 0x52
[    4.840867] s32cc-dwmac 4033c000.ethernet:   DWMAC4/5
[    4.845909] s32cc-dwmac 4033c000.ethernet: DMA HW capability register supported
[    4.853320] s32cc-dwmac 4033c000.ethernet: RX Checksum Offload Engine supported
[    4.860731] s32cc-dwmac 4033c000.ethernet: TX Checksum insertion supported
[    4.867701] s32cc-dwmac 4033c000.ethernet: Wake-Up On Lan supported
[    4.874096] s32cc-dwmac 4033c000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[    4.882039] s32cc-dwmac 4033c000.ethernet: Enabled L3L4 Flow TC (entries=8)
[    4.889098] s32cc-dwmac 4033c000.ethernet: Enabled RFS Flow TC (entries=10)
[    4.896162] s32cc-dwmac 4033c000.ethernet: Enabling HW TC (entries=256, max_off=256)
[    4.904018] s32cc-dwmac 4033c000.ethernet: Using 32/32 bits DMA host/device width
[    4.917289] hwmon hwmon1: temp1_input not attached to any thermal zone
[    4.926162] qoriq_thermal 400a8000.tmu: Critical rising/falling temperature threshold = 5 degree(s)
[    4.939279] nxp_s32cc_ddr_perf 403e0000.ddr-perf: probing device
[    4.945593] nxp_s32cc_ddr_perf 403e0000.ddr-perf: device initialized successfully
[    4.953427] clk: Disabling unused clocks
[    4.981066] EXT4-fs (mmcblk0p2): mounted filesystem 7ef8de4c-43d4-4981-a4ac-61482e00b612 r/w with ordered data mode. Quota mode: disabled.
[    4.993129] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    4.999699] devtmpfs: mounted
[    5.002865] Freeing unused kernel memory: 1792K
[    5.007034] Run /sbin/init as init process
[    5.386401] systemd[1]: System time before build time, advancing clock.
[    5.444407] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid)
[    5.475772] systemd[1]: Detected architecture arm64.

Welcome to Auto Linux BSP 42.0 (kirkstone)!

[    5.497910] systemd[1]: Hostname set to .
[    5.927648] systemd[1]: Queued start job for default target Multi-User System.
[    5.965242] systemd[1]: Created slice Slice /system/getty.
[  OK  ] Created slice Slice /system/getty.
[    5.986147] systemd[1]: Created slice Slice /system/modprobe.
[  OK  ] Created slice Slice /system/modprobe.
[    6.009949] systemd[1]: Created slice Slice /system/serial-getty.
[  OK  ] Created slice Slice /system/serial-getty.
[    6.033676] systemd[1]: Created slice User and Session Slice.
[  OK  ] Created slice User and Session Slice.
[    6.057473] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[  OK  ] Started Dispatch Password …ts to Console Directory Watch.
[    6.081401] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[  OK  ] Started Forward Password R…uests to Wall Directory Watch.
[    6.105482] systemd[1]: Reached target Path Units.
[  OK  ] Reached target Path Units.
[    6.125329] systemd[1]: Reached target Remote File Systems.
[  OK  ] Reached target Remote File Systems.
[    6.145305] systemd[1]: Reached target Slice Units.
[  OK  ] Reached target Slice Units.
[    6.165336] systemd[1]: Reached target Swaps.
[  OK  ] Reached target Swaps.
[    6.225646] systemd[1]: Listening on RPCbind Server Activation Socket.
[  OK  ] Listening on RPCbind Server Activation Socket.
[    6.249388] systemd[1]: Reached target RPC Port Mapper.
[  OK  ] Reached target RPC Port Mapper.
[    6.269922] systemd[1]: Listening on Syslog Socket.
[  OK  ] Listening on Syslog Socket.
[    6.289501] systemd[1]: Listening on initctl Compatibility Named Pipe.
[  OK  ] Listening on initctl Compatibility Named Pipe.
[    6.316408] systemd[1]: Journal Audit Socket was skipped because of a failed condition check (ConditionSecurity=audit).
[    6.327108] systemd[1]: Listening on Journal Socket (/dev/log).
[  OK  ] Listening on Journal Socket (/dev/log).
[    6.349641] systemd[1]: Listening on Journal Socket.
[  OK  ] Listening on Journal Socket.
[    6.369803] systemd[1]: Listening on Network Service Netlink Socket.
[  OK  ] Listening on Network Service Netlink Socket.
[    6.393697] systemd[1]: Listening on udev Control Socket.
[  OK  ] Listening on udev Control Socket.
[    6.413500] systemd[1]: Listening on udev Kernel Socket.
[  OK  ] Listening on udev Kernel Socket.
[    6.433567] systemd[1]: Listening on User Database Manager Socket.
[  OK  ] Listening on User Database Manager Socket.
[    6.477471] systemd[1]: Mounting Huge Pages File System...
         Mounting Huge Pages File System...
[    6.497628] systemd[1]: POSIX Message Queue File System was skipped because of a failed condition check (ConditionPathExists=/proc/sys/fs/mqueue).
[    6.512336] systemd[1]: Mounting Kernel Debug File System...
         Mounting Kernel Debug File System...
[    6.533610] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing).
[    6.546133] systemd[1]: Create List of Static Device Nodes was skipped because of a failed condition check (ConditionFileNotEmpty=/lib/modules/6.6.32-rt32-g49d9f8bb25e0-dirty/modules.devname).
[    6.577637] systemd[1]: Starting Load Kernel Module configfs...
         Starting Load Kernel Module configfs...
[    6.599592] systemd[1]: Starting Load Kernel Module drm...
         Starting Load Kernel Module drm...
[    6.623568] systemd[1]: Starting Load Kernel Module fuse...
         Starting Load Kernel Module fuse...
[    6.669659] systemd[1]: Starting RPC Bind...
         Starting RPC Bind...
[    6.689480] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/).
[    6.705360] systemd[1]: Starting Journal Service...
         Starting Journal Service...
[    6.732435] systemd[1]: Starting Load Kernel Modules...
         Starting Load Kernel Modules...
[    6.750655] sja1110: loading out-of-tree module taints kernel.
[    6.756520] SPI driver sja1110 has no spi_device_id for nxp,sja1110-switch
[    6.763040] SPI driver sja1110 has no spi_device_id for nxp,sja1110-uc
[    6.769691] sja1110 spi5.0: probing uc
[    6.773335] sja1110 spi5.1: probing switch
[    6.777589] sja1110 spi5.1: Could not get GPIO from device tree
[    6.784402] sja1110 spi5.1: [sja1110_post_probe_upload_worker] Trying to initialize switch
[    6.793013] sja1110 spi5.1: Direct firmware load for sja1110_switch.bin failed with error -2
[    6.801036] sja1110 spi5.1: request_firmware failed with -2
[    6.806581] sja1110 spi5.0: [sja1110_post_probe_upload_worker] Trying to initialize uC
[    6.814510] sja1110 spi5.0: Direct firmware load for sja1110_uc.bin failed with error -2
[    6.822553] sja1110 spi5.0: request_firmware failed with -2
[    6.833773] systemd[1]: Starting Generate network units from Kernel command line...
         Starting Generate network …ts from Kernel command line...
[    6.859983] systemd[1]: Starting Remount Root and Kernel File Systems...
         Starting Remount Root and Kernel File Systems...
[    6.888086] systemd[1]: Starting Coldplug All udev Devices...
         Starting Coldplug All udev Devices...
[    6.913647] EXT4-fs (mmcblk0p2): re-mounted 7ef8de4c-43d4-4981-a4ac-61482e00b612 r/w. Quota mode: disabled.
[    6.918508] systemd[1]: Started RPC Bind.
[  OK  ] Started RPC Bind.
[    6.942831] systemd[1]: Started Journal Service.
[  OK  ] Started Journal Service.
[  OK  ] Mounted Huge Pages File System.
[  OK  ] Mounted Kernel Debug File System.
[  OK  ] Finished Load Kernel Module configfs.
[  OK  ] Finished Load Kernel Module drm.
[  OK  ] Finished Load Kernel Module fuse.
[  OK  ] Finished Load Kernel Modules.
[  OK  ] Finished Generate network units from Kernel command line.
[  OK  ] Finished Remount Root and Kernel File Systems.
         Mounting FUSE Control File System...
         Mounting Kernel Configuration File System...
         Starting Flush Journal to Persistent Storage...
[    7.205357] systemd-journald[147]: Received client request to flush runtime journal.
         Starting Apply Kernel Variables...
         Starting Create Static Device Nodes in /dev...
[  OK  ] Mounted FUSE Control File System.
[  OK  ] Finished Coldplug All udev Devices.
[  OK  ] Mounted Kernel Configuration File System.
[  OK  ] Finished Flush Journal to Persistent Storage.
[  OK  ] Finished Apply Kernel Variables.
[  OK  ] Finished Create Static Device Nodes in /dev.
[  OK  ] Reached target Preparation for Local File Systems.
         Mounting /tmp...
         Mounting /var/volatile...
         Starting Rule-based Manage…for Device Events and Files...
[  OK  ] Mounted /tmp.
[  OK  ] Mounted /var/volatile.
         Mounting /var/volatile/tmp...
         Starting Load/Save Random Seed...
[  OK  ] Mounted /var/volatile/tmp.
[  OK  ] Reached target Local File Systems.
         Starting Create Volatile Files and Directories...
[  OK  ] Started Rule-based Manager for Device Events and Files.
[  OK  ] Finished Create Volatile Files and Directories.
         Starting Network Time Synchronization...
         Starting Record System Boot/Shutdown in UTMP...
[  OK  ] Finished Record System Boot/Shutdown in UTMP.
[  OK  ] Started Network Time Synchronization.
[  OK  ] Reached target System Initialization.
[  OK  ] Started Daily Cleanup of Temporary Directories.
[  OK  ] Reached target System Time Set.
[  OK  ] Started Daily rotation of log files.
[  OK  ] Reached target Timer Units.
[  OK  ] Listening on D-Bus System Message Bus Socket.
         Starting sshd.socket...
[  OK  ] Listening on sshd.socket.
[  OK  ] Reached target Socket Units.
[  OK  ] Reached target Basic System.
[  OK  ] Started Job spooling tools.
[  OK  ] Started Periodic Command Scheduler.
         Starting D-Bus System Message Bus...
         Starting IPv6 Packet Filtering Framework...
         Starting IPv4 Packet Filtering Framework...
[  OK  ] Started irqbalance daemon.
[  OK  ] Started Hardware RNG Entropy Gatherer Daemon.
[  OK  ] Started System Logging Service.
         Starting Resets System Activity Logs...
         Starting User Login Management...
         Starting OpenSSH Key Generation...
[  OK  ] Finished IPv6 Packet Filtering Framework.
[  OK  ] Finished IPv4 Packet Filtering Framework.
[  OK  ] Finished Resets System Activity Logs.
[  OK  ] Finished OpenSSH Key Generation.
[  OK  ] Reached target Preparation for Network.
         Starting Network Configuration...
[  OK  ] Started Network Configuration.
[  OK  ] Created slice Slice /system/systemd-fsck.
         Starting Network Name Resolution...
[  OK  ] Found device /dev/mmcblk0p1.
         Starting File System Check on /dev/mmcblk0p1...
[  OK  ] Finished File System Check on /dev/mmcblk0p1.
         Mounting /run/media/boot_s32g3-mmcblk0p1...
[  OK  ] Started Network Name Resolution.
[  OK  ] Mounted /run/media/boot_s32g3-mmcblk0p1.
[  OK  ] Reached target Network.
[  OK  ] Reached target Host and Network Name Lookups.
[  OK  ] Started Netperf Benchmark Server.
[  OK  ] Started NFS status monitor for NFSv2/3 locking..
[  OK  ] Started Respond to IPv6 Node Information Queries.
[  OK  ] Started Network Router Discovery Daemon.
         Starting Permit User Sessions...
[  OK  ] Started Xinetd A Powerful Replacement For Inetd.
[  OK  ] Finished Permit User Sessions.
[  OK  ] Started Getty on tty1.
[  OK  ] Started Serial Getty on ttyLF0.
[  OK  ] Reached target Login Prompts.
[  OK  ] Finished Load/Save Random Seed.
[  OK  ] Started D-Bus System Message Bus.
[  OK  ] Started User Login Management.
[  OK  ] Reached target Multi-User System.
         Starting Record Runlevel Change in UTMP...
[  OK  ] Finished Record Runlevel Change in UTMP.

Auto Linux BSP 42.0 s32g399ardb3 ttyLF0

s32g399ardb3 login: root

次はifconfigコマンドの結果です。

root@s32g399ardb3:~# ifconfig
eth0: flags=4099  mtu 1500
        ether 7e:d8:f2:25:32:d4  txqueuelen 1000  (Ethernet)
        RX packets 0  bytes 0 (0.0 B)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 0  bytes 0 (0.0 B)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
        device interrupt 55  base 0xa000

lo: flags=73  mtu 65536
        inet 127.0.0.1  netmask 255.0.0.0
        inet6 ::1  prefixlen 128  scopeid 0x10
        loop  txqueuelen 1000  (Local Loopback)
        RX packets 82  bytes 6220 (6.0 KiB)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 82  bytes 6220 (6.0 KiB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。

Hi, @Wzlinux 

conf/local.conf へのすべての変更を削除することをお勧めします。次に、次の 2 行のみを追加します (コピーして設定ファイルに貼り付けます)。

DISTRO_FEATURES:append = "pfe"

NXP_FIRMWARE_LOCAL_DIR = "/home/bin/fsl-auto-yocto-bsp/sources/meta-alb/meta-alb-bsp/recipes-kernel/pfe/pfe"


その後、次のコマンドを実行して、次のコマンドで再構築します。

bitbake fsl-image-auto -c クリーン & bitbake fsl-image-auto 


BR

チェンイン

Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。こんにちは @chenyin_h
ありがとうございます。
フォロー2行を削除しました。
DISTRO_FEATURES:append = "PFE PFE-スレーブ"
NXP_FIRMWARE_LOCAL_DIR = "/home/bin/fsl-auto-yocto-bsp/sources/meta-alb/meta-alb-bsp/recipes-kernel/pfe/pfe/"
次のものだけを保持します。
DISTRO_FEATURES:append = "pfe"
NXP_FIRMWARE_LOCAL_DIR = "/home/bin/fsl-auto-yocto-bsp/sources/meta-alb/meta-alb-bsp/recipes-kernel/pfe/pfe/"
bitbake fsl-image-auto を使用します
fsl-image-auto-s32g399ardb3.sdcardをSDカードに焼き付けました。
/lib/firmware が空です。
以下は /lib/modules/ です。
root@s32g399ardb3:/lib/firmware# ls
root@s32g399ardb3:/lib/firmware# cd ../

root@s32g399ardb3:/lib/modules/6.6.32-rt32-g49d9f8bb25e0-dirty#LSの
mdio-proxy.ko modules.alias.bin modules.builtin.alias.bin modules.builtin.modinfo modules.dep.bin modules.order modules.symbols の更新
modules.alias modules.builtin modules.builtin.bin modules.dep modules.dev名前 modules.softdep modules.symbols.bin

Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。

Hello, @Wzlinux 

次の2行を削除することをお勧めします。

DISTRO_FEATURES:append = "PFE PFE-スレーブ"
NXP_FIRMWARE_LOCAL_DIR = "/home/bin/fsl-auto-yocto-bsp/sources/meta-alb/meta-alb-bsp/recipes-kernel/pfe/pfe/"

次に、Yoctoイメージを再構築して試してみてください


BR

チェンイン


Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。

こんにちは@chenyin_h
これは私のYocto設定(conf / local.onf)の続きです:

機械。。= 's32g399ardb3'
DISTRO ?= 'fsl-auto'
PACKAGE_CLASSES ?= "package_rpm"
EXTRA_IMAGE_FEATURES ?= "デバッグ調整"
USER_CLASSES ?= "buildstats"
PATCHRESOLVE = "noop"
BB_DISKMON_DIRS??= "\
STOPTASKS、${TMPDIR}、1G、100K \
STOPTASKS,${DL_DIR},1G,100K \
STOPTASKS、${SSTATE_DIR}、1G、100K \
STOPTASKS,/tmp,100M,100K \
ハルト、${TMPDIR}、100M、1K \
ハルト、${DL_DIR}、100M、1K \
ハルト、${SSTATE_DIR}、100M、1K \
ハルト、/ tmp、10M、1K"
PACKAGECONFIG:append:pn-qemu-system-native = "sdl"
CONF_VERSION = "2"

# 並列処理オプション
BB_NUMBER_THREADS = "32"
PARALLEL_MAKE = "-j 24"
DL_DIR = "/home/bin/fsl-auto-yocto-bsp/downloads"
SSTATE_DIR = "/home/bin/fsl-auto-yocto-bsp/sstate-cache"
ACCEPT_FSL_EULA = "1"

DISTRO_FEATURES:append = "pfe"
NXP_FIRMWARE_LOCAL_DIR = "/home/bin/fsl-auto-yocto-bsp/sources/meta-alb/meta-alb-bsp/recipes-kernel/pfe/pfe/"
DISTRO_FEATURES:append = "PFE PFE-スレーブ"
NXP_FIRMWARE_LOCAL_DIR = "/home/bin/fsl-auto-yocto-bsp/sources/meta-alb/meta-alb-bsp/recipes-kernel/pfe/pfe/"

「/home/bin/fsl-auto- に 2 つの s32g_pfe_class.fw s32g_pfe_util.fw ファイルがあります。yocto-bsp/sources/meta-alb/meta-alb-bsp/recipes-kernel/pfe/pfe/"

Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。こんにちは@chenyin_h
これが私のYocto設定です(conf / local.onf)続き:

機械。。= 's32g399ardb3'
DISTRO ?= 'fsl-auto'
PACKAGE_CLASSES ?= "package_rpm"
EXTRA_IMAGE_FEATURES ?= "デバッグ調整"
USER_CLASSES ?= "buildstats"
PATCHRESOLVE = "noop"
BB_DISKMON_DIRS??= "\
STOPTASKS、${TMPDIR}、1G、100K \
STOPTASKS、${DL_DIR}、1G、100K \
STOPTASKS、${SSTATE_DIR}、1G、100K \
STOPTASKS,/tmp,100M,100K \
ハルト、${TMPDIR}、100M、1K \
ハルト、${DL_DIR}、100M、1K \
ハルト、${SSTATE_DIR}、100M、1K \
ハルト、/ tmp、10M、1K"
PACKAGECONFIG:append:pn-qemu-system-native = "sdl"
CONF_VERSION = "2"

# 並列処理オプション
BB_NUMBER_THREADS = "32"
PARALLEL_MAKE = "-j 24"
DL_DIR = "/home/bin/fsl-auto-yocto-bsp/downloads"
SSTATE_DIR = "/home/bin/fsl-auto-yocto-bsp/sstate-cache"
ACCEPT_FSL_EULA = "1"

DISTRO_FEATURES:append = "pfe"
NXP_FIRMWARE_LOCAL_DIR = "/home/bin/fsl-auto-yocto-bsp/sources/meta-alb/meta-alb-bsp/recipes-kernel/pfe/pfe/"
DISTRO_FEATURES:append = "PFE PFE-スレーブ"
NXP_FIRMWARE_LOCAL_DIR = "/home/bin/fsl-auto-yocto-bsp/sources/meta-alb/meta-alb-bsp/recipes-kernel/pfe/pfe/"

「/home/bin/fsl-auto-yocto-bsp/sources/meta-alb/meta-alb-bsp/recipes-kernel/pfe/pfe/」に2つのs32g_pfe_class.fw s32g_pfe_util.fwファイルがあります。

Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。

Hello, @Wzlinux 

あなたのディレクトリの下にpfeng.koがないのは奇妙です、Yoctoのビルド中に「pfe-slave」を設定したかどうかはわかりませんが、テストを行ったところ、次のディレクトリからpfeng.koが見つかりました。

/lib/modules/6.6.32-rt32-00903-g49d9f8bb25e0/kernel/drivers/net/ethernet/nxp/pfe/pfeng.ko

Yoctoの建物の設定を再確認するのを手伝ってくれませんか?

また、PFE Linuxドライバーを手動でビルドする場合は、BSP42に1.7バージョンが必要ですが、Linuxモジュールをビルドするのと同じ方法でビルドできます。


BR

チェンイン


BR

チェンイン

Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。こんにちは@chenyin_h
/lib/modules リストは、以下のとおりです。
root@s32g399ardb3:~# cd /lib/modules/
root@s32g399ardb3:/lib/modules# ls
6.6.32-RT32-G49D9F8BB25E0-ダーティ
root@s32g399ardb3:/lib/modules# cd 6.6.32-rt32-g49d9f8bb25e0-dirty/
root@s32g399ardb3:/lib/modules/6.6.32-rt32-g49d9f8bb25e0-dirty#LSの
カーネル modules.alias modules.builtin modules.builtin.bin modules.dep modules.devname modules.softdep modules.symbols.bin
mdio-proxy.ko modules.alias.bin modules.builtin.alias.bin modules.builtin.modinfo modules.dep.bin modules.order modules.symbols の更新
root@s32g399ardb3:/lib/modules/6.6.32-rt32-g49d9f8bb25e0-dirty#cd kernel/drivers/net/ethernet/nxp/pfe/
root@s32g399ardb3:/lib/modules/6.6.32-rt32-g49d9f8bb25e0-dirty/kernel/drivers/net/ethernet/nxp/pfe#LSの
pfeng-slave.ko
root@s32g399ardb3:/lib/modules/6.6.32-rt32-g49d9f8bb25e0-dirty/kernel/drivers/net/ethernet/nxp/pfe#

/lib/firmware は、以下のとおりです。
root@s32g399ardb3:/lib/firmware# ls
s32g_pfe_class.fw s32g_pfe_util.fw
root@s32g399ardb3:/lib/firmware#

ifconfig -a には PFE ポートがありません。
root@s32g399ardb3:/lib/firmware# ifconfig -a
can0: flags=128 mtu 16
unspec 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00 txqueuelen 10 (UNSPEC)
RX パケット 0 バイト 0 (0.0 B)
RX エラー 0、ドロップ、0、オーバーラン、0、フレーム 0
TX パケット 0 バイト 0 (0.0 B)
TX エラー 0、ドロップ、0 オーバーラン、0 キャリア、0、コリジョン 0

can1: flags=128 mtu 16
unspec 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00 txqueuelen 10 (UNSPEC)
RX パケット 0 バイト 0 (0.0 B)
RX エラー 0、ドロップ、0、オーバーラン、0、フレーム 0
TX パケット 0 バイト 0 (0.0 B)
TX エラー 0、ドロップ、0 オーバーラン、0 キャリア、0、コリジョン 0

eth0: flags=4099 mtu 1500
inet6 fe80::6c70:86ff:fe71:1b8 prefixlen 64 scopeid 0x20
ether 6e:70:86:71:01:b8 txqueuelen 1000 (イーサネット)
RXパケット 50バイト 4462 (4.3 KiB)
RX エラー 0、ドロップ、0、オーバーラン、0、フレーム 0
TX パケット 33 バイト 4973 (4.8 KiB)
TX エラー 0、ドロップ、0 オーバーラン、0 キャリア、0、コリジョン 0
デバイス割り込み 55 ベース0x2000

lo: flags=73 mtu 65536
inet 127.0.0.1 ネットマスク 255.0.0.0
inet6 ::1 prefixlen 128 スコープ ID 0x10
loop txqueuelen 1000 (ローカル ループバック)
RXパケット 82バイト 6220 (6.0 KiB)
RX エラー 0、ドロップ、0、オーバーラン、0、フレーム 0
TX パケット 82 バイト 6220 (6.0 KiB)
TX エラー 0 ドロップ、オーバーラン、0、キャリア、衝突0、0

sit0: flags=128 MTU 1480
unspec 00-00-00-00-00-00-38-9B-00-00-00-00-00-00-00 txqueuelen 1000 (UNSPEC)
RX パケット 0 バイト 0 (0.0 B)
RX エラー 0、ドロップ、0、オーバーラン、0、フレーム 0
TX パケット 0 バイト 0 (0.0 B)
TX エラー 0、ドロップ、0 オーバーラン、0 キャリア、0、コリジョン 0

Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。こんにちは @chenyin_h
ありがとうございます。
私はPFE_Driver_1_5_0.zipをダウンロードしましたこのドライバーの作り方を教えてもらえますか?PFE dirver(どのファイル)をロードする方法は?
Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。

Hi, @Wzlinux 

ご返信ありがとうございます。

ログから、PFE FWは正常に統合されているように見えますが、PFE Linuxドライバーが初期化されていないように見えるため、/ lib / modules /で確認し、PFEドライバーを手動でロードしてみてください。


BR

チェンイン

Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。こんにちは @chenyin_h
ありがとうございます。
私はあなたの方法を使用してbitbakeに成功します。次に、画像をSDカードにフラッシュします。しかし、ifconfig -a には pfe がありません
注意: リセットステータス: 電源投入時リセット
BL2:v2.10.0(リリース):bsp42.0-2.10
注意: BL2: 構築 : 2024年9月12日 19:50:36
注意: BL2: BL31 の起動


Uブート 2022.04+g5a6f62071f+p0(2024年9月6日 - 07:11:20 +0000)

SoC:NXPのS32G399Aリビジョン1.0
CPU:ARM Cortex-A53 r0p4 @最大1300 MHz
モデル:NXP S32G399A-RDB3
DRAM: 3.5 GiB
コア:306デバイス、25 uclass、デバイスツリー:ボード
MMC:FSL_SDHC:0
MMC から環境を読み込んでいます... わかりました
s32cc_serdes_phy serdes@40480000: SerDes サブシステムのモード 0 を使用
pci_s32cc pcie@40400000: RootComplex としての構成
pci_s32cc pcie@40400000: リンクアップに失敗しました
で: serial@401c8000
アウト:serial@401c8000
エラー:serial@401c8000
ボードリビジョン:RDB3リビジョンE
PCIe: BusDevFun VendorId DeviceId デバイス クラス サブクラス
__________________________________________________________________________
pcie@40400000 ルートコンプレックス
|'-- 01:00.00 0x1957 0x4300 ブリッジデバイス0x04
網:
警告:ランダムなMACアドレスを使用するethernet@4033c000(eth0) - 2a:2d:07:9b:27:9c
eth0: ethernet@4033c000
PFEバージョン0x0101(S32G3)が見つかりました
pfeng pfeng-base: CLASS ファームウェアのアップロード
pfeng pfeng-base: EMAC0 ブロックが初期化されました
pfeng pfeng-base: EMAC1 ブロックが初期化されました
pfeng pfeng-base: EMAC2 ブロックが初期化されました
pfeng pfeng-base: CLASS ブロックの有効化
pfeng pfeng-base: PFE プラットフォームが正常に開始されました (マスク: 7)
s32cc_serdes_phy serdes@44180000: SerDes サブシステムのモード 4 の使用
s32cc_serdes_phy serdes@44180000: 2 μs 後に XPCS0 で安定した RX が検出されました
、eth1:pfe0s32cc_serdes_phy serdes@44180000:XPCS1で不安定なRXが検出されました
、eth2:pfe1、eth3:pfe2
自動起動を停止するには、任意のキーを押します:0
パーティション#0に切り替えて、OK
mmc0 は現在のデバイスです
15415304バイトを646ミリ秒で読み取り(22.8MiB/秒)
mmc から起動しています ...
60416バイトを6ミリ秒で読み取り(9.6 MiB/秒)
## 83000000 のフラット化されたデバイスツリーブロブ
fdt blob を使用して 0x83000000 で起動する
デバイスツリーを0000000083000000の位置で使用し、0000000083011bff を終了します。
修正: PFE1: PHY Addr を 0x8 に更新します
XPCS1_1の設定に失敗しました
SerDes1 の XPCS1 を更新できませんでした

カーネルを起動しています...

[ 0.000000] 物理CPU上でのLinuxの起動 0x0000000000 [0x410fd034]
[ 0.000000] Linuxバージョン6.6.32-rt32-g49d9f8bb25e0-dirty(OE-user@oe-ホスト)(aarch64-fsl-linux-gcc(GCC)11.4.0、GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT Thu Sep 12 09:32:29 UTC 2024
[ 0.000000] マシンモデル:NXP S32G3リファレンスデザインボード(S32G-VNP-RDB3)
[ 0.000000] earlycon: MMIO 0x00000000401c8000 の linflex0 (オプション '115200n8')
[ 0.000000] printk: レガシー ブートコンソール [linflex0] 有効
[ 0.000000] OF: 予約済みメモリ: 0x0000000034000000..0x000000003407ffff (512 KiB) nomap 再利用可能なpfebufs@34000000
[ 0.000000] OF: 予約済みメモリ: 0x0000000034080000..0x000000003409ffff (128 KiB) nomap 再利用可能なpfebufs@34080000
[ 0.000000] 予約済みメモリ: 0x0000000083200000、サイズ 3 MiB で DMA メモリ プールを作成
[ 0.000000] OF: 予約済みメモリ: 初期化されたノード pfebufs@83200000、互換性のある ID shared-dma-pool
[ 0.000000] OF: 予約済みメモリ: 0x0000000083200000..0x00000000835dffff (3968 KiB) nomap 再利用可能なpfebufs@83200000
[ 0.000000] OF: 予約済みメモリ: 0x00000000835e0000..0x00000000835fffff (128 KiB) マップ再利用可能なpfebufs@835e0000
[ 0.000000] OF: 予約済みメモリ: 0x0000000084000000..0x0000000084ffffff (16384 KiB) nomap 再利用可能なshm@84000000
[ 0.000000] OF: 予約済みメモリ: 0x00000000c0000000..0x00000000c03fffff (4096 KiB) nomap 再利用可能なshm@c0000000
[ 0.000000] OF: 予約済みメモリ: 0x00000000c0400000..0x00000000c07fffff (4096 KiB) nomap 再利用可能なshm@c0400000
[ 0.000000] OF: 予約済みメモリ: 0x00000000d0000000..0x00000000d000007f (0 KiB) nomap 再利用不可shm@d0000000
[ 0.000000] OF: 予約済みメモリ: 0x00000000d0000080..0x00000000d00000ff (0 KiB) nomap 再利用可能なshm@d0000080
[ 0.000000] OF: 予約済みメモリ: 0x00000000ff600000..0x00000000ff7fffff (2048 KiB) nomap 再利用不可atf@ff600000
[ 0.000000] ゾーン範囲:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 が空です
[ 0.000000] ノーマル [mem 0x0000000100000000-0x00000008dfffffff]
[ 0.000000] ノードごとに移動ゾーン開始
[ 0.000000] 初期のメモリノードの範囲
[ 0.000000] ノード 0: [mem 0x0000000080000000-0x00000000831fffff]
[ 0.000000] ノード 0: [mem 0x0000000083200000-0x00000000835dffff]
[ 0.000000] ノード 0: [mem 0x00000000835e0000-0x0000000083ffffff]
[ 0.000000] ノード 0: [mem 0x0000000084000000-0x0000000084ffffff]
[ 0.000000] ノード 0: [mem 0x0000000085000000-0x00000000bfffffff]
[ 0.000000] ノード 0: [mem 0x00000000c0000000-0x00000000c07fffff]
[ 0.000000] ノード 0: [mem 0x00000000c0800000-0x00000000cfffffff]
[ 0.000000] ノード 0: [mem 0x00000000d0001000-0x00000000ff5fffff]
[ 0.000000] ノード 0: [mem 0x00000000ff600000-0x00000000ff7fffff]
[ 0.000000] ノード 0: [mem 0x00000000ff800000-0x00000000ffffffff]
[ 0.000000] ノード 0: [mem 0x0000000880000000-0x00000008dfffffff]
[ 0.000000] Initmem セットアップ ノード 0 [mem 0x0000000080000000-0x00000008dfffffff]
[ 0.000000] ノード 0、ゾーン DMA: 使用不可の範囲に 1 ページ
[ 0.000000] cma: ノード -1 の 0x00000000ef600000 で 256 MiB を予約
[ 0.000000] PSCI: DT からのコンジット法のプローブ。
[ 0.000000] psci: ファームウェアで PSCIv1.1 が検出されました。
[ 0.000000] psci: 標準の PSCI v0.2 関数 ID を使用
[ 0.000000] PSCI: MIGRATE_INFO_TYPEはサポートされていません。
[ 0.000000] psci: SMC Calling Convention v1.4
[ 0.000000] percpu: 埋め込み 19 ページ/CPU s40040 r8192 d29592 u77824
[ 0.000000] CPU0 で VIPT I キャッシュが検出されました
[ 0.000000] CPU機能:検出:GICシステムレジスタCPUインターフェース
[ 0.000000] CPU 機能: 検出: ARM エラータ 845719
[ 0.000000] CPU 機能: 検出: ARM エラータ 1165522、1319367、1530923、または 1530924
[ 0.000000] alternatives: ブートの代替を適用する
[ 0.000000] カーネルコマンドライン: console=ttyLF0,115200 root=/dev/mmcblk0p2 rootwait rw earlycon
[ 0.000000] Dentry キャッシュ ハッシュ テーブル エントリ: 524288 (順序: 10、4194304 バイト、線形)
[ 0.000000] inode-cache ハッシュ テーブル エントリ: 262144 (順序: 9、2097152 バイト、線形)
[ 0.000000] 1つのゾーンリストを構築し、モビリティのグループ化をオンにしました。総ページ数:903167
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] ソフトウェア IO TLB: エリア番号 8.
[ 0.000000] ソフトウェア IO TLB: マッピング [mem 0x00000000eb600000-0x00000000ef600000] (64MB)
[ 0.000000] メモリ: 3223892K/3670012K 使用可能 (9536K カーネル コード、654K rwdata、2928K rodata、1792K init、219K bss、183976K 予約済み、262144K cma 予約済み)
[ 0.000000] SLUB: HWalign=64、Order=0-3、MinObjects=0、CPUs=8、Nodes=1
[ 0.000000] rcu: プリエンプティブル階層 RCU の実装。
[ 0.000000] rcu: RCU イベント トレースが有効になっています。
[ 0.000000] タスク RCU のトランポリン バリアントが有効になりました。
[ 0.000000] タスク RCU のトレース バリアントが有効になっています。
[ 0.000000] rcu: RCU の計算値であるスケジューラー登録遅延は 25 jiffies です。
[ 0.000000] NR_IRQS: 64、nr_irqs: 64、事前割り当て済み IRQ: 0
[ 0.000000] GICv3: GIC: 分割 EOI/非アクティブ化モードを使用
[ 0.000000] GICv3: 544 SPI が実装されています
[ 0.000000] GICv3: 0 拡張 SPI が実装されました
[ 0.000000] GICv3: MBI 範囲 [167:182]
[ 0.000000] GICv3: MBI フレーム 0x0000000050800000 を使用
[ 0.000000] ルート IRQ ハンドラ: gic_handle_irq
[ 0.000000] GICv3: GICv3 機能: 16 PPI
[ 0.000000] GICv3:CPU0:再配布者0領域0:0x0000000050900000が見つかりました
[ 0.000000] ITS: 利用可能な ITS がありません。LPI が有効になっていません
[ 0.000000] rcu: srcu_init: 競合に基づいてsrcu_structサイズを設定します。
[ 0.000000] arch_timer: 5.00MHz で動作する cp15 タイマー (phys)。
[ 0.000000] ClockSource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x127350b88, max_idle_ns: 440795202120 ns
[ 0.000001] sched_clock: 5MHz で 56 ビット、解像度 200ns、4398046511100ns ごとに折り返す
[ 0.008364] コンソール: カラー ダミー デバイス 80x25
[ 0.012454] 遅延ループのキャリブレーション (スキップ)、タイマー周波数を使用して計算された値..10.00 ボゴミップス (lpj=20000)
[ 0.022659] pid_max:デフォルト:32768最小:301
[ 0.027358] マウントキャッシュハッシュテーブルエントリ:8192(順序:4、65536バイト、線形)
[ 0.034652] マウントポイントキャッシュハッシュテーブルエントリ:8192(順序:4、65536バイト、線形)
[ 0.044061] RCU タスク: shift を 3 に、lim を 1 に設定 rcu_task_cb_adjust=1。
[ 0.050739] RCU タスク トレース: shift を 3 に、lim を 1 に設定 rcu_task_cb_adjust=1。
[ 0.058406] rcu: 階層型 SRCU の実装。
[ 0.063006] rcu: 最大位相の遅延なしインスタンスは 1000 です。
[ 0.068860] smp: セカンダリ CPU を起動しています ...
[ 0.073532] CPU1でVIPT Iキャッシュが検出されました
[ 0.073585] GICv3:CPU1:再配布1領域0:0x0000000050920000が見つかりました
[ 0.073622] CPU1:セカンダリプロセッサを起動0x0000000001[0x410fd034]
[ 0.074197] CPU2でVIPT Iキャッシュが検出されました
[ 0.074233] GICv3:CPU2:再配布2領域0:0x0000000050940000が見つかりました
[ 0.074253] CPU2:セカンダリプロセッサを起動0x0000000002 [0x410fd034]
[ 0.074783] CPU3でVIPT Iキャッシュが検出されました
[ 0.074820] GICv3:CPU3:再配布3領域0:0x0000000050960000が見つかりました
[ 0.074839] CPU3:セカンダリプロセッサの起動0x0000000003 [0x410fd034]
[ 0.075390] CPU4でVIPT Iキャッシュが検出されました
[ 0.075449] GICv3:CPU4:再配布100領域0:0x0000000050980000が見つかりました
[ 0.075479] CPU4:セカンダリプロセッサの起動0x0000000100 [0x410fd034]
[ 0.076058] CPU5でVIPT Iキャッシュが検出されました
[ 0.076099] GICv3:CPU5:再配布101地域0:0x00000000509a0000が見つかりました
[ 0.076119] CPU5:セカンダリプロセッサの起動0x0000000101 [0x410fd034]
[ 0.076665] CPU6でVIPT Iキャッシュが検出されました
[ 0.076709] GICv3:CPU6:再配布102リージョン0:0x00000000509c0000が見つかりました
[ 0.076728] CPU6:セカンダリプロセッサの起動0x0000000102 [0x410fd034]
[ 0.077337] CPU7でVIPT Iキャッシュが検出されました
[ 0.077379] GICv3: CPU7: 再配布 103 領域 0:0x00000000509e0000 が見つかりました
[ 0.077400] CPU7:起動したセカンダリプロセッサ 0x0000000103 [0x410fd034]
[ 0.077473] smp: 1 ノード、8 CPU を起動
[ 0.203366] SMPの 合計8つのプロセッサがアクティブになりました。
[ 0.208042] CPU機能:検出:32ビットEL0サポート
[ 0.213173] CPU機能:検出:CRC32命令
[ 0.218356] CPU:すべてのCPUがEL2で開始されました
[ 0.222375] alternatives: システム全体の代替案の適用
[ 0.229714] devtmpfs: 初期化済み
[ 0.240999] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.250332] futexハッシュテーブルエントリ:2048(順序:5、131072バイト、線形)
[ 0.264835] pinctrl core: 初期化された pinctrl サブシステム
[ 0.270477] NET: 登録済み PF_NETLINK/PF_ROUTE プロトコル ファミリ
[ 0.276933] DMA: 原子割り当て用に事前に割り当てられた 512 KiB GFP_KERNEL プール
[ 0.283746] DMA: 事前割り当て済み 512 KiB GFP_KERNEL|アトミック割り当て用のGFP_DMAプール
[ 0.291506] DMA: 事前割り当て済み 512 KiB GFP_KERNEL|アトミック割り当て用のGFP_DMA32プール
[ 0.299508] thermal_sys:登録サーマルガバナー「step_wise」
[ 0.299617] hw-breakpoint: 6 つのブレークポイントと 4 つのウォッチポイントレジスタが見つかりました。
[ 0.312090] ASID アロケーターが 65536 エントリで初期化されました
[ 0.317438] シリアル: AMBA PL011 UART ドライバ
[ 0.321472] scmi_core:SCMIプロトコルバスが登録されています
[ 0.327323] scmi_protocol scmi_dev.1:ポーリング モードを有効にした TX チャネル - prot_id:16
[ 0.334788] arm-scmi firmware:scmi: SCMI 通知 - コアが有効。
[ 0.341026] arm-scmi firmware:scmi: SCMI Protocol v2.0 'NXP:S32G399A' ファームウェア バージョン 0x0
[ 0.355994] プラットフォーム 4009c240.siul2-pinctrl:/soc/siul2@4009c000/siul2-pinctrl@4009c240/jtag_pins による依存関係のサイクルを固定
[ 0.374260] モジュール: 非 PLT 使用の範囲で 28944 ページ
[ 0.374266] モジュール: PLT の使用範囲に 520464 ページ
[ 0.379885] HugeTLB: 登録ページサイズ 1.00 GiB、事前割り当て済み 0 ページ
[ 0.391532] HugeTLB: 0 KiB の vmemmap を 1.00 GiB ページで解放できます
[ 0.397784] HugeTLB: 登録ページサイズ 32.0 MiB、事前割り当て済み 0 ページ
[ 0.404552] HugeTLB: 0 KiB の vmemmap を 32.0 MiB ページで解放できます
[ 0.410803] HugeTLB: 登録ページサイズ 2.00 MiB、事前割り当て済み0ページ
[ 0.417571] HugeTLB: 0 KiB vmemmap を 2.00 MiB ページで解放できます
[ 0.423823] HugeTLB: 登録ページサイズ 64.0 KiB、事前割り当て済み0ページ
[ 0.430593] HugeTLB: 0 KiB の vmemmap を 64.0 KiB のページで解放できます
[ 0.444580] SCSI サブシステムが初期化されました
[ 0.448069] usbcore:新しいインターフェースドライバーUSBFを登録しました
[ 0.453392] usbcore:新しいインターフェースドライバーハブを登録しました
[ 0.458696] usbcore:新しいデバイスドライバUSBを登録しました
[ 0.464183] pps_core:LinuxPPS API ver. 1 登録済み
[ 0.468713] pps_core:ソフトウェア版5.3.6 - 著作権2005-2007ロドルフォジョメッティ
[ 0.477836] PTPクロックサポート登録
[ 0.482652] vgaarb:ロード済み
[ 0.485231] clocksource: clocksource arch_sys_counterに切り替えました
[ 0.497185] NET: 登録済みの PF_INET プロトコル ファミリ
[ 0.501851] IP IDハッシュテーブルエントリ:65536(順序:7、524288バイト、線形)
[ 0.511580] tcp_listen_portaddr_hashハッシュテーブルエントリ:2048(順序:3、32768バイト、線形)
[ 0.519741] Table-perturb ハッシュ テーブル エントリ: 65536 (順序: 6、262144 バイト、線形)
[ 0.527404] TCP がハッシュ テーブル エントリを確立: 32768 (順序: 6、262144 バイト、線形)
[ 0.535493] TCPバインドハッシュテーブルエントリ:32768(順序:8、1048576バイト、線形)
[ 0.543769] TCP:ハッシュテーブルが設定されました(32768バインド32768が確立されました)
[ 0.549976] UDPハッシュテーブルエントリ:2048(順序:4、65536バイト、線形)
[ 0.556614] UDP-Lite ハッシュ テーブル エントリ: 2048 (順序: 4、65536 バイト、線形)
[ 0.563860] NET: 登録済み PF_UNIX/PF_LOCAL プロトコル ファミリ
[ 0.569674] RPC:登録された名前のUNIXソケットトランスポートモジュール。
[ 0.575214] RPC: 登録済みの udp トランスポート モジュール。
[ 0.579895] RPC: 登録された tcp トランスポート モジュール。
[ 0.584581] RPC: 登録された tcp-with-tls トランスポート モジュール。
[ 0.590051] RPC:登録されたtcp NFSv4.1バックチャネルトランスポートモジュール。
[ 0.596498] PCI: CLS 0 バイト、デフォルト 64
[0.601962]ワーキングセット:timestamp_bits = 62 max_order = 20 bucket_order = 0
[ 0.608434] ヒューズ:init(APIバージョン7.39)
[ 0.612164] NET:登録済みPF_ALGプロトコルファミリ
[ 0.616832] ブロック層 SCSI 汎用 (bsg) ドライバー バージョン 0.4 が読み込まれました (メジャー 248)
[ 0.624167] IOスケジューラMQ-DEADLINE登録
[ 0.628677] IOスケジューラKyber登録済み
[ 0.632677] IOスケジューラBFQ登録
[ 0.639941] s32cc-siul2-pinctrl 4009c240.siul2-pinctrl:初期化された S32 Pinctrl ドライバー
[ 0.648537] s32cc-siul2-gpio 4009d700.siul2-gpio:キャッシュのデフォルトなし、HWからの読み取り
[ 0.656371] s32cc-siul2-gpio 4009d700.siul2-gpio:キャッシュのデフォルトなし、HWからの読み取り
[ 0.664815] gpio gpiochip0: GPIO ベースの静的割り当ては非推奨です。動的割り当てを使用してください。
[ 0.673796] s32cc-siul2-gpio 4009d700.siul2-gpio:キャッシュのデフォルトなし、HWからの読み取り
[ 0.681599] s32cc-siul2-gpio 4009d700.siul2-gpio:キャッシュのデフォルトなし、HWからの読み取り
[ 0.700909] printk: レガシーコンソール [ttyLF0] enabled000 (irq = 23, base_baud = 7812500) は FSL_LINFLEX
[ 0.700909] printk: レガシーコンソール [ttyLF0] 有効
[ 0.710804] printk: レガシー ブートコンソール [linflex0] が無効
[ 0.710804] printk: レガシー ブートコンソール [linflex0] が無効
[ 0.725709] 401cc000.serial:MMIO 0x401cc000 での ttyLF1 (irq = 24, base_baud = 7812500) は FSL_LINFLEX
[ 0.736960] s32cc_fccu 4030c000.fccu:FCCU ステータスは 0 (正常)
[ 0.745147] sja1110-sw@1 GPIOハンドルにアクティブローを強制します
[ 0.753001] SPIノールSPI6.0:mx25uw51245g (65536 キロバイト)
[ 0.758734] MTD デバイス 0.spi に 7 つの固定パーティション パーティションが見つかりました
[ 0.765102] "0.spi"に7つのMTDパーティションを作成します。
[ 0.769874] 0x000000000000-0x000004000000 : 「フラッシュイメージ」
[ 0.775622] 0x000000000000-0x000000280000 : 「FIP」
[ 0.780633] 0x000000280000-0x000000290000 : "U-boot-Env"
[ 0.786268] 0x000000290000-0x000001360000 : カーネル
[ 0.791565] 0x000001360000-0x000001390000 : "DTB"
[ 0.796578] 0x000001390000-0x0000032a0000 : "Rootfs"
[ 0.801851] 0x0000032a0000-0x000004000000 : 「PFEファームウェア」
[ 0.808968] vcan: 仮想CANインターフェースドライバ
[ 0.813487] slcan:シリアルラインCANインターフェースドライバ
[ 0.818438] CANデバイスドライバインターフェース
[ 0.823267] FlexCan 401B4000.can:登録済みデバイス (reg_base=(____ptrval____), irq(s):
[ 0.831392] FlexCan 401B4000.can:30
[ 0.835110] FlexCan 401B4000.can:31
[ 0.838823] FlexCan 401B4000.can:32
[ 0.842536] FlexCan 401B4000.can:33
[ 0.846247] FlexCan 401B4000.can:)
[ 0.850493] FlexCan 401BE000.CAN:登録済みデバイス (reg_base=(____ptrval____), irq(s):
[ 0.858620] flexcan 401be000.can:34
[ 0.862339] FlexCan 401BE000.CAN:35
[ 0.866051] FlexCan 401BE000.CAN:36
[ 0.869764] FlexCan 401BE000.CAN:37
[ 0.873475] FlexCan 401BE000.CAN:)
[ 0.877190] e100: インテル(R) PRO/100 ネットワーク ドライバ
[ 0.881961] e100:Copyright(c) 1999-2006 Intel Corporation
[ 0.887547] e1000: インテル(R) PRO/1000 ネットワーク ドライバ
[ 0.892492] e1000:著作権(c)1999-2006 Intel Corporation。
[ 0.898335] e1000e: インテル(R) PRO/1000 ネットワーク ドライバ
[ 0.903368] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 0.909394] igb: インテル(R) ギガビット イーサネット ネットワーク ドライバ
[ 0.914867] igb:著作権(c)2007-2014インテルコーポレーション。
[ 0.921312] hse-uio 40210000.mu0b:ファームウェアが見つかりません
[ 0.926833] usbcore: 新しいインターフェースドライバーUASを登録しました
[ 0.932251] usbcore:新しいインターフェースドライバーのUSBストレージを登録しました
[ 0.939239] imx_usb 44064000.usb:過電流極性が定義されていません
[ 0.959790] ci_hdrc ci_hdrc.0:EHCI ホスト コントローラー
[ 0.964857] ci_hdrc ci_hdrc.0:新しいUSBバスが登録され、バス番号1が割り当てられています
[ 0.985229] ci_hdrc ci_hdrc.0:USB 2.0 開始、EHCI 1.00
[ 0.990852] usb usb1: 新しい USB デバイスが見つかりました、idVendor=1d6b、idProduct=0002、bcdDevice= 6.06
[ 0.999242] usb usb1: 新しい USB デバイス文字列: Mfr=3、Product=2、SerialNumber=1
[ 1.006567] usb usb1: 製品: EHCI ホストコントローラ
[ 1.011514] usb usb1:メーカー:Linux 6.6.32-rt32-g49d9f8bb25e0-dirtyehci_hcd
[1.019191] usb usb1:シリアル番号:ci_hdrc.0
[ 1.024019] ハブ 1-0:1.0:USBハブが見つかりました
[ 1.027847] ハブ 1-0:1.0: 1 ポートが検出されました
[ 1.033065] S32CC-RTC 40060000.RTC:RTC0として登録
[ 1.038296] S32CC-RTC 40060000.RTC:システムクロックを 1970-01-01T00:00:00 UTC (0) に設定する
[ 1.046497] i2c_dev: I2c /dev entries ドライバー
[ 1.051174] S32CC-WDT 4010C000.ウォッチドッグ:S32CCウォッチドッグタイマ登録タイムアウト=30秒 (nowayout=0)
[ 1.060426] S32CC-WDT 40200000.ウォッチドッグ:S32CCウォッチドッグタイマ登録タイムアウト=30秒 (nowayout=0)
[ 1.069658] S32CC-WDT 40204000.ウォッチドッグ:S32CCウォッチドッグタイマ登録タイムアウト=30秒 (nowayout=0)
[ 1.078888] S32CC-WDT 40208000.ウォッチドッグ:S32CCウォッチドッグタイマ登録タイムアウト=30秒 (nowayout=0)
[ 1.088135] S32CC-WDT 40500000.ウォッチドッグ:S32CCウォッチドッグタイマ登録タイムアウト=30秒 (nowayout=0)
[ 1.097363] S32CC-WDT 40504000.ウォッチドッグ:S32CCウォッチドッグタイマ登録タイムアウト=30秒 (nowayout=0)
[ 1.106593] S32CC-WDT 40508000.ウォッチドッグ:S32CCウォッチドッグタイマ登録タイムアウト=30秒 (nowayout=0)
[ 1.115824] S32CC-WDT 4050C000.ウォッチドッグ:S32CCウォッチドッグタイマ登録タイムアウト=30秒 (nowayout=0)
[ 1.126319] sdhci: セキュア デジタル ホスト コントローラー インターフェイス ドライバー
[ 1.132603] sdhci:著作権(c)Pierre Ossman
[ 1.137025] sdhci-pltfm: SDHCIプラットフォームおよびOFドライバーヘルパー
[ 1.142978] SMCCC:SOC_ID:ARCH_SOC_ID実装されていません、スキップします....
[ 1.149892] HSE 40211000.mu1b:インターフェイス MU1b がアクティブでない
[ 1.155642] usbcore:新しいインターフェースドライバーusbhidを登録しました
[ 1.161300] usbhid: USB HIDコアドライバ
[ 1.173232] mmc0: 402f0000.mmc [402f0000.mmc] の SDHCI コントローラーADMAの使用
[ 1.180525] S32-ADC 401F8000.adc:ADC DMA 転送に dma0chan4 を使用
[ 1.187669] S32-ADC 401F8000.ADC:デバイスが正常に初期化されました。
[ 1.205376] S32-ADC 402E8000.adc:ADC DMA 転送に dma1chan16 を使用
[ 1.212559] S32-ADC 402E8000.adc:デバイスが正常に初期化されました。
[ 1.216889] mmc0: 新しい高速 SDHC カード (アドレス aaaa)
[ 1.224683] hw perfevents: armv8_cortex_a53 PMU ドライバーで有効、7 つのカウンターが利用可能
[ 1.224912] mmcblk0: mmc0:aaaa SK32G 29.7 GiB
[ 1.234210] s32-siul2-nvmem 4009c000.nvram:初期化された s32cc siul2 nvmem ドライバー
[ 1.239113] mmcblk0: p1 p2
[ 1.245068] s32-siul2-nvmem 44010000.nvram:初期化された s32cc siul2 nvmem

ドライバー[ 1.255958] NET:登録済みPF_INET6プロトコルファミリ[
1.261902] IPv6
によるセグメント
ルーティング[ 1.265646] IPv6 を使用した In-situ OAM (IOAM)[ 1.269674]
sit: IPv6、IPv4、MPLS over IPv4 トンネリング
ドライバー[ 1.276098] NET: 登録済みPF_PACKETプロトコルファミリ[




1.281336] CAN:
コントローラエリアネットワークコア[ 1.285784] NET: 登録済みPF_CANプロトコルファミリ[ 1.290644]

CAN: raw プロトコル[ 1.293656]
CAN: ブロードキャスト マネージャ プロトコル[ 1.297901] CAN: NetLink ゲートウェイ - max_hops=1[ 1.302373] 8021q: 802.1Q VLAN サポート v1.8[ 1.321937]
i2c i2c-0:
GPIO
リカバリに pinctrl ステートを使用[ 1.327881] i2c i2c-0:リカバリに汎用GPIOを使用[ 1.333392] pca953x 0-0022: AIを使用[ 1.344052] RTC-PCF85063 0-0051: RTC1として登録[ 1.349034] i2c
i2c-0: IMX I2C アダプタ登録済み[ 1.353853] I2C I2C-0:
DMA 転送に DMA0chan5 (tx) と dma0chan6 (rx) を使用[ 1.361855] i2c i2c-2: GPIO リカバリに pinctrl
ステートを使用[ 1.367730] i2c i2c-2: 汎用 GPIO をリカバリーに使用[ 1.373103] i2c i2c-2: IMX I2C アダプタ登録済み[ 1.377912] I2C I2C-2: DMA転送にDMA17(TX)およびDMA1chan18(RX)を使用[ 1.386045] I2C I2C-4: GPIO リカバリに Pinctrl ステートを使用[ 1.391918] i2c i2c-4: 汎用
GPIO を使用したリカバリ[ 1.398619] ina2xx 4-0040: パワー モニタ
ina231 (Rshunt = 1000 uOhm)[ 1.405096] i2c i2c-4:
IMX I2C アダプタ登録済みBR />[ 1.409903] i2c
i2c-4: DMA 転送に dma1chan19 (tx) と dma1chan20 (rx) を使用[
1.418063] phy-s32cc-serdes 40480000.serdes:SerDes サブシステムのモード 0 の使用
[ 1.425859] phy-s32cc-serdes 44180000.serdes:SerDes サブシステムのモード 4 の使用
[ 1.654607] s32cc-pcie 40400000.pcie:PHY リンクを安定させることができませんでした
[ 1.660883] s32cc-pcie 40400000.pcie:RootComplex としての構成
[ 1.667010] s32cc-pcie 40400000.pcie:ホストブリッジ /soc/pcie@40400000 の範囲:
[ 1.674183] s32cc-pcie 40400000.pcie:IO 0x5ffffe0000..0x5ffffeffff-> 0x0000000000
[ 1.682489] s32cc-pcie 40400000.pcie:MEM 0x5800000000..0x5ffffdffff-> 0x0000000000
[ 1.690802] s32cc-pcie 40400000.pcie:メモリ リソース サイズが 32 ビットの最大値を超えている
[ 2.698614] s32cc-pcie 40400000.pcie:Phy リンクが起動しない
[ 2.704402] s32cc-pcie 40400000.pcie:iATU: 展開 T、6 ob、4 ib、位置合わせ 4K、制限 1024G
[ 2.712604] s32cc-pcie 40400000.pcie:eDMA:T、4 wr、4 rdを展開
[ 3.718882] s32cc-pcie 40400000.pcie:Phy リンクが起動しない
[ 4.724737] s32cc-pcie 40400000.pcie:Phy リンクが起動しない
[ 4.730933] s32cc-pcie 40400000.pcie:PCI ホスト・ブリッジからバス 0000:00
[ 4.737385] pci_bus 0000:00: ルート バス リソース [バス 00-FF]
[ 4.742953] pci_bus 0000:00: ルート バス リソース [IO 0x0000-0xffff]
[ 4.749223] pci_bus 0000:00: ルート バス リソース [mem 0x5800000000-0x5ffffdffff] (バス アドレス [0x00000000-0x7fffdffff])
[ 4.760015] PCI 0000:00:00.0:[1957:4300] 01式0x060400
[ 4.766124] PCI 0000:00:00.0:登録0x10:[MEM 0x5800000000-0x58000fffff]
[ 4.772846] PCI 0000:00:00.0:登録0x38:[MEM 0x5800000000-0x580000ffff Pref]
[ 4.780090] PCI 0000:00:00.0:D1をサポート
[ 4.784158] PCI 0000:00:00.0:PME# D0 D1 D3hot D3cold からサポート
[ 4.793387] PCI 0000:00:00.0:小節 0: 割り当て済み [mem 0x5800000000-0x58000fffff]
[ 4.800634] PCI 0000:00:00.0:小節 6: 代入 [mem 0x5800100000-0x580010ffff pref]
[ 4.808316] PCI 0000:00:00.0:PCI ブリッジから [bus 01-ff] へ
[ 4.813852] PCIeport 0000:00:00.0:PME:IRQ 52 によるシグナリング
[ 4.820529] s32cc-dwmac 4033c000.ethernet:IRQ eth_wake_irq見つかりません
[ 4.827072] S32CC-DWMAC 4033C000.イーサネット:IRQ eth_lpi見つかりません
[ 4.833567] s32cc-dwmac 4033c000.ethernet:ユーザーID:0x10、Synopsys ID:0x52
[ 4.840635] s32cc-dwmac 4033c000.ethernet:DWMAC4/5の
[ 4.845680] s32cc-dwmac 4033c000.ethernet:DMA HW機能レジスタをサポート
[ 4.853092] s32cc-dwmac 4033c000.ethernet:RXチェックサムオフロードエンジン対応
[ 4.860507] s32cc-dwmac 4033c000.ethernet:TX チェックサム挿入をサポート
[ 4.867478] s32cc-dwmac 4033c000.ethernet:Wake-Up On Lan 対応
[ 4.873869] s32cc-dwmac 4033c000.ethernet:HW ウォッチドッグ タイマーによる RX 軽減の有効化
[ 4.881812] s32cc-DWMAC 4033c000.ethernet:L3L4 フロー TC の有効化 (entries=8)
[ 4.888875] s32cc-dwmac 4033c000.ethernet:有効な RFS フロー TC (エントリ = 10)
[ 4.895942] s32cc-dwmac 4033c000.ethernet:HW TC の有効化 (entries=256, max_off=256)
[ 4.903796] s32cc-dwmac 4033c000.ethernet:32/32ビットDMAホスト/デバイス幅を使用
[ 4.917131] HWMON HWMON1:temp1_inputどのサーマルゾーンにも取り付けられていません
[ 4.925993] qoriq_thermal 400a8000.tmu:臨界上昇/下降温度しきい値 = 5 度
[ 4.939101] nxp_s32cc_ddr_perf 403e0000.ddr-perf:プロービング装置
[ 4.945436] nxp_s32cc_ddr_perf 403e0000.ddr-perf:デバイスが正常に初期化されました
[ 4.953236] clk: 未使用のクロックを無効化
[ 4.984505] EXT4-fs (mmcblk0p2): ファイルシステム 96ed4b7d-2fa5-411c-b5c1-f04b002b7095 r/w を順序付けデータ モードでマウントしました。クォータ モード: 無効。
[ 4.996558] VFS: デバイス 179:2 にルート (ext4 ファイルシステム) がマウントされました。
[ 5.003237] devtmpfs:マウント済み
[ 5.006406] 未使用のカーネルメモリの解放:1792K
[ 5.010573] /sbin/initをinitプロセスとして実行
[ 5.380856] systemd[1]: ビルド時間の前のシステム時間、クロックの進行。
[ 5.435938] systemd[1]: systemd 250.5+ をシステムモードで実行 (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid)
[ 5.467296] systemd[1]: アーキテクチャ arm64 を検出しました。

Auto Linux BSP 42.0 (kirkstone) へようこそ!

[ 5.489934] systemd[1]: ホスト名を に設定します。
[ 5.504734] systemd[1]: ランダムジェネレータからマシンIDを初期化しています。
[ 5.939390] systemd[1]: デフォルトのターゲットマルチユーザーシステムのキューに入れられた開始ジョブ。
[ 5.993560] systemd[1]: スライス /system/getty を作成しました。
[ わかりました ]スライスを作成 Slice /system/getty.
[ 6.014301] systemd[1]: スライス /system/modprobe を作成しました。
[ わかりました ]スライス Slice /system/modprobe を作成しました。
[ 6.037982] systemd[1]: スライス /system/serial-getty を作成しました。
[ わかりました ]スライス Slice /system/serial-getty を作成しました。
[ 6.061664] systemd[1]: スライス User と Session Slice を作成しました。
[ わかりました ]スライス User と Session Slice を作成しました。

オートリナックスBSP 42.0 s32g399ardb3 ttyLF0

S32G399ARDB3ログイン:ルート
root@s32g399ardb3:~# ls
root@s32g399ardb3:~# ifconfig -a
can0: flags=128 mtu 16
unspec 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00 txqueuelen 10 (UNSPEC)
RX パケット 0 バイト 0 (0.0 B)
RX エラー 0、ドロップ、0、オーバーラン、0、フレーム 0
TX パケット 0 バイト 0 (0.0 B)
TX エラー 0、ドロップ、0 オーバーラン、0 キャリア、0、コリジョン 0

can1: flags=128 mtu 16
unspec 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00 txqueuelen 10 (UNSPEC)
RX パケット 0 バイト 0 (0.0 B)
RX エラー 0、ドロップ、0、オーバーラン、0、フレーム 0
TX パケット 0 バイト 0 (0.0 B)
TX エラー 0、ドロップ、0 オーバーラン、0 キャリア、0、コリジョン 0

eth0: flags=4099 mtu 1500
ether 2a:2d:07:9b:27:9c txqueuelen 1000 (イーサネット)
RX パケット 0 バイト 0 (0.0 B)
RX エラー 0、ドロップ、0、オーバーラン、0、フレーム 0
TX パケット 0 バイト 0 (0.0 B)
TX エラー 0、ドロップ、0 オーバーラン、0 キャリア、0、コリジョン 0
デバイス割り込み 55 ベース0xa000

lo: flags=73 mtu 65536
inet 127.0.0.1 ネットマスク 255.0.0.0
inet6 ::1 prefixlen 128 スコープ ID 0x10
loop txqueuelen 1000 (ローカル ループバック)
RXパケット 82バイト 6220 (6.0 KiB)
RX エラー 0、ドロップ、0、オーバーラン、0、フレーム 0
TX パケット 82 バイト 6220 (6.0 KiB)
TX エラー 0、ドロップ、0 オーバーラン、0 キャリア、0、コリジョン 0

sit0: flags=128 MTU 1480
unspec 00-00-00-00-00-00-38-9B-00-00-00-00-00-00-00 txqueuelen 1000 (UNSPEC)
RX パケット 0 バイト 0 (0.0 B)
RX エラー 0、ドロップ、0、オーバーラン、0、フレーム 0
TX パケット 0 バイト 0 (0.0 B)
TX エラー 0、ドロップ、0 オーバーラン、0 キャリア、0、コリジョン 0

Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。

Hello, @Wzlinux 

私の意見から。

1.PFE1.8の使用をお勧めしますFWは、BSP42.0リリースノートに記載されています。

2. conf/local.conf で、あなたはDISTRO_FEATURES_append += "pfe"を使用しているようですが、代わりに、 DISTRO_FEATURES:append = " pfe"を使用することをお勧めします。


BR

チェンイン

Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。

Hello, @Wzlinux 

PFE FWは、次のリンクからダウンロードできます。

https://www.nxp.com/app-autopackagemgr/automotive-software-package-manager:AUTO-SW-PACKAGE-MANAGER

chenyin_h_1-1735108999806.png



BR

チェンイン

Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。こんにちは@chenyin_h
お返事ありがとうございます。
私は情報をconf/local.confファイルに追加します

機械。。= 's32g399ardb3'
DISTRO ?= 'fsl-auto'
PACKAGE_CLASSES ?= "package_rpm"
EXTRA_IMAGE_FEATURES ?= "デバッグ調整"
USER_CLASSES ?= "buildstats"
PATCHRESOLVE = "noop"
BB_DISKMON_DIRS??= "\
STOPTASKS、${TMPDIR}、1G、100K \
STOPTASKS、${DL_DIR}、1G、100K \
STOPTASKS、${SSTATE_DIR}、1G、100K \
STOPTASKS,/tmp,100M,100K \
ハルト、${TMPDIR}、100M、1K \
ハルト、${DL_DIR}、100M、1K \
ハルト、${SSTATE_DIR}、100M、1K \
ハルト、/ tmp、10M、1K"
PACKAGECONFIG:append:pn-qemu-system-native = "sdl"
CONF_VERSION = "2"

# 並列処理オプション
BB_NUMBER_THREADS = "32"
PARALLEL_MAKE = "-j 24"
DL_DIR = "/home/bin/fsl-auto-yocto-bsp/downloads"
SSTATE_DIR = "/home/bin/fsl-auto-yocto-bsp/sstate-cache"
ACCEPT_FSL_EULA = "1"
DISTRO_FEATURES_append += "PFE"
NXP_FIRMWARE_LOCAL_DIR = "/home/bin/fsl-auto-yocto-bsp/build_s32g399ardb3/PFE_Firmware_1_10_0/"

PFE_Firmware_1_10_0フォルダには、s32g_pfe_class.fwファイルs32g_pfe_util.fwファイルがあります。

しかし、bitbake fsl-image-autoコマンドを実行するとします。エラーがあります。

エラー: 変数DISTRO_FEATURES_appendファイル: /home/bin/fsl-auto-yocto-bsp/build_s32g399ardb3/conf/local.conf 行: 25 には、古いオーバーライド構文を使用した操作が含まれています。新しいビットベイクで使用する前に、このレイヤー/メタデータを変換してください。
エラー:/ home / bin / fsl-auto-yocto-bsp / sources / poky / bitbake / lib / b /__init__.pyを解析できません

この問題について調べるのを手伝ってもらえますか?感謝。
Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。こんにちは@chenyin_h
ありがとうございます。
s32g_pfe_class.fw fwファイルとs32g_pfe_util.fwファイルを取得する方法を教えてください。
Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。

Hello, @Wzlinux 

イメージの生成に使用したコマンドにはPFEサポートは含まれていませんので、詳細についてはBSP UMの7.3.4章を読むことをお勧めします。

chenyin_h_0-1735028981521.png

また、@jiajun_chengのインプットに感謝します


BR

チェンイン

Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。

Hi, @Wzlinux :

最初に提供していただいたログで、私は見ました

[    6.750655] sja1110: loading out-of-tree module taints kernel.
[    6.756520] SPI driver sja1110 has no spi_device_id for nxp,sja1110-switch
[    6.763040] SPI driver sja1110 has no spi_device_id for nxp,sja1110-uc
[    6.769691] sja1110 spi5.0: probing uc
[    6.773335] sja1110 spi5.1: probing switch
[    6.777589] sja1110 spi5.1: Could not get GPIO from device tree
[    6.784402] sja1110 spi5.1: [sja1110_post_probe_upload_worker] Trying to initialize switch
[    6.793013] sja1110 spi5.1: Direct firmware load for sja1110_switch.bin failed with error -2
[    6.801036] sja1110 spi5.1: request_firmware failed with -2
[    6.806581] sja1110 spi5.0: [sja1110_post_probe_upload_worker] Trying to initialize uC
[    6.814510] sja1110 spi5.0: Direct firmware load for sja1110_uc.bin failed with error -2
[    6.822553] sja1110 spi5.0: request_firmware failed with -2

 100baseT1ポートはsja1110にあり、ロード後にpfeポートのメッセージが表示されますsja1110_uc.bin

jiajun_cheng_0-1735026544097.png



Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。こんにちは @chenyin_h
感謝。
以下は ifconfig -a result です。PFE 情報はありません。その理由を教えてもらえますか?ビルドをフォローしてBitbakeを使用しました。
1. $ .nxp-setup-alb.sh -M S32G399ARDB3
2.bitbake fsl-image-auto(英語)
3.sudo dd if=.sdcardof=/dev/sd bs=1M &&; sync


以下はifconfig -aコマンドの結果です///////////////////////////////////
オートリナックスBSP 42.0 s32g399ardb3 ttyLF0

S32G399ARDB3ログイン:ルート
root@s32g399ardb3:~# ls
root@s32g399ardb3:~# ifconfig -a
can0: flags=128 mtu 16
unspec 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00 txqueuelen 10 (UNSPEC)
RX パケット 0 バイト 0 (0.0 B)
RX エラー 0、ドロップ、0、オーバーラン、0、フレーム 0
TX パケット 0 バイト 0 (0.0 B)
TX エラー 0、ドロップ、0 オーバーラン、0 キャリア、0、コリジョン 0

can1: flags=128 mtu 16
unspec 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00 txqueuelen 10 (UNSPEC)
RX パケット 0 バイト 0 (0.0 B)
RX エラー 0、ドロップ、0、オーバーラン、0、フレーム 0
TX パケット 0 バイト 0 (0.0 B)
TX エラー 0、ドロップ、0 オーバーラン、0 キャリア、0、コリジョン 0

eth0: flags=4099 mtu 1500
ether 7a:89:31:63:1c:48 txqueuelen 1000 (イーサネット)
RX パケット 0 バイト 0 (0.0 B)
RX エラー 0、ドロップ、0、オーバーラン、0、フレーム 0
TX パケット 0 バイト 0 (0.0 B)
TX エラー 0、ドロップ、0 オーバーラン、0 キャリア、0、コリジョン 0
デバイス割り込み 55 ベース0x2000

lo: flags=73 mtu 65536
inet 127.0.0.1 ネットマスク 255.0.0.0
inet6 ::1 prefixlen 128 スコープ ID 0x10
loop txqueuelen 1000 (ローカル ループバック)
RXパケット 82バイト 6220 (6.0 KiB)
RX エラー 0、ドロップ、0、オーバーラン、0、フレーム 0
TX パケット 82 バイト 6220 (6.0 KiB)
TX エラー 0、ドロップ、0 オーバーラン、0 キャリア、0、コリジョン 0

sit0: flags=128 MTU 1480
unspec 00-00-00-00-00-00-38-9B-00-00-00-00-00-00-00 txqueuelen 1000 (UNSPEC)
RX パケット 0 バイト 0 (0.0 B)
RX エラー 0、ドロップ、0、オーバーラン、0、フレーム 0
TX パケット 0 バイト 0 (0.0 B)
TX エラー 0、ドロップ、0 オーバーラン、0 キャリア、0、コリジョン 0
Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。

Hello, @Wzlinux 

100baseT1 ポートは sja1110 上にあり、デフォルトでは PFE_MAC0 に接続されています。

まず、ビルドされたイメージに PFE サポートを追加し (ビルド済みのイメージにはデフォルトで PFE サポートが含まれている可能性があります)、Linux シェルに入った後、ifconfig -a で pfeX ポートが表示される場合があります。

次に、100base-T1 ポート経由で PFE0 に ping を実行してみてください。(このポートがホストのようにテストデバイスに直接接続されていると仮定します)


BR

チェンイン


Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。こんにちは@chenyin_h
ご返信ありがとうございます。
はい、100-base-T1を50コネクタから接続できます。

私の質問は、SWから100-base-T1ポートをどのように有効にできるかということです。
BSP42.0をSDカードに書き込んでSDカードから起動した後、デフォルトで有効になっていますか(例:SJA1110 P10 100-BASE-T1)
イーサネットイネーブルガイドから、100-base-T1はSJA1110によって制御されることを学びましたが、最初にSJA1110を有効にする必要がありますか?それらがデフォルトで有効になっているかどうか(BSP42.0 fsl-image-auto )?
Re:S32G-VNP-RDB3 100BASE-T1ポートを開く方法。

Hello, @Wzlinux 

投稿ありがとうございます。

RDB3には、J53 Mini 50コネクタと100-Base-T1用のハーネスケーブルがあります。このケーブルをテスト・デバイスに接続してテストできます。

ケーブルに接続する特定のデバイスがない場合は、RJ45-100BASET1コンバーターを購入してテストすることをお勧めします。


BR

チェンイン

Tags (1)
No ratings
Version history
Last update:
‎01-05-2026 02:54 AM
Updated by: