Hi xianlong,
Sorry for the inconvenience we bring you!
Thank you for the report.
A few months ago, design team confirmed that the ADC MUX information about S32K310 and S32K311 in S32K3RM v9 is not complete, and gave us S32K311_ADC_Mux_Control.xlsx. The reference manual will be updated in the next version.
I tried to modify the ADC pins in S32DS Pins Tool this morning, but as you mentioned, the macro definitions Siul2_Port_Ip_AdcInterleaves are not defined, so after Siul2_Port_Ip_Init is called, Siul2_Port_Ip_WriteDCMConfiguration will not modify the DCMRWF4 register of S32K310 and S32K311.
I'm afraid that writing to registers is the only option at the moment. I'm asking the AE team when RTD will fix this.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------