2010721_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2010721_en-US

2010721_en-US

S32K3xx MCU programmer and debugger

Hi ,

   Kindly suggest cost effective S32K3xx cortex m7  programmer and debugger




regards,

Karmegan C

Re: S32DS IDE installation and development package installation for s32k3xx

Hello,

Sorry, this is different topic.

I am not able to help here. Always respect the release notes of RTD packages, otherwise the packages will not be compatible.

Best regards,

Peter

Re: S32DS IDE installation and development package installation for s32k3xx

Hi,

    After S32DS 3.5 IDE installation, I opened an example Flex CAN project  from RTD  s32kxx and built it. I got the errors as are below,

In file included from ../board/Siul2_Port_Ip_Cfg.c:42:
../board/Siul2_Port_Ip_Cfg.h:46:10: fatal error: Siul2_Port_Ip_Types.h: No such file or directory
46 | #include "Siul2_Port_Ip_Types.h"

C:/Users/karme/workspaceS32DS.3.5/FlexCAN_Ip_Example_S32K344/RTD/include/CanIf.h:52:10: fatal error: CanIf_Cfg.h: No such file or directory
52 | #include "CanIf_Cfg.h"
| ^~~~~~~~~~~~~
compilation terminated.
make: *** [RTD/src/subdir.mk:38: RTD/src/CanIf.o] Error 1
In file included from ../RTD/src/Can_43_FLEXCAN.c:104:
C:/Users/karme/workspaceS32DS.3.5/FlexCAN_Ip_Example_S32K344/RTD/include/Can_43_FLEXCAN.h:110:10: fatal error: Soc_Ips.h: No such file or directory
110 | #include "Soc_Ips.h"
| ^~~~~~~~~~~

How to fix these mistakes I need your help with the S32DS IDE, S32K3xx development package, and RTD installation since I believe there may have been errors in the package and IDE installation time.
There are drivers for the boot loader, CAN, UDS, and FLASHING S32K342 in the RTD or S32K3xx development packages.

Re: S32K3xx MCU programmer and debugger

Hello,

There is wide variety of devices you can use.

It depends on how serious you will go with your development.

Very basic - is embedded open SDA - free on the evaluation boards.

basic - PE micro

advanced - iSystem, GHS probe

Pro - Lauterbach

Best regards,

Peter

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 12:37 PM
Updated by: