2009128_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2009128_en-US

2009128_en-US

Single-ended CLRC663 RF design

Hi, 


I have a question related to the single-ended CLRC663 RF circuit design. The datasheet mentions that the receiver can be configured in single-end mode by connecting RxN and RxP and setting the quasi differential mode in the rcv_rx_single register. 

May I know how to configure the single-ended mode for TxN and TxP? Can I connect TxN and TxP? If so, is there any register setting for the TxN and TxP?

Thanks,

Heng


NFC Frontend SolutionsRe: Single-ended CLRC663 RF design

Hi Tomas,

Thanks for the confirming.

Heng

Re: Single-ended CLRC663 RF design

Hello hengma


Yes, for single ended, the target impedance would be around 10 Ohms. 

Once you tune your system to 10 Ohm, please also check the trasmitter current. You should not exceed the maximum TVDD current. 


BR

Tomas 

Re: Single-ended CLRC663 RF design

Hi Tomas,


One more question, what is the desired impedance for the single-end solution? For the differential solution, the desired impedance is between 18 and 20 ohms for maximum field strength and power transfer. For the single-end solution, will the desired impedance become 10 ohms when measuring the TX and GND?

Thanks,

Heng

Re: Single-ended CLRC663 RF design

Hello @hengma , 


Correct, Once both Tx paths are anabled and they are in phase. The maximum power of the TX driver can be used. 

If only one TX side is enabled (TxEn), the power is reduced by 50%. 


BR

Tomas 

Re: Single-ended CLRC663 RF design

Hi Tomas,

Thanks for your prompt reply.

In order to use a single-ended transmitter solution, shall I configure both Tx1Inv and Tx2Inv to 1 or 0? In this case, both TxN and TxP will deliver a non-inverted or inverted 13.56 MHz carrier, which is in phase. 

Also, may I know the setting of TxEn? Can we define the source of the transmitter using the setting of TxEn?

Thanks,

Heng

Re: Single-ended CLRC663 RF design

Hello hengma,


You should be able to change the phase of the TX signal using the following register. If both signal are in phase (TX1 and TX2). You should be able to connect them and get proper signal and waveform. 

Tomas_Parizek_0-1733494355197.pngTomas_Parizek_0-1733494355197.png

BR

Tomas 

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 09:16 PM
Updated by: