MCUXpresso Secure Provisioning v10 BEE USER KEYSHI:
After burning and writing my image through security tools in unsigned, the code can run normally.. No problem...
But when using BEE user keys unsigned encryption, the code does not work properly. Isn't that where the problem lies?. The keys are all the same
1733448057456.png
1733448123207.png
1733448222073.png
1733448278916.png Re: MCUXpresso Secure Provisioning v10 BEE USER KEYSThis issue has been resolved because the XIP encryption enable pin in BOOT_CFG [1] was not connected to highRe: MCUXpresso Secure Provisioning v10 BEE USER KEYSHi,
I see you have two application "boot" and "app". Which of them does not work? What exactly means "the code does not work properly"?
What exactly mean "The keys are all the same"? I can see you are using single key for BEE Engine 0. Are there any other keys?