2008466_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2008466_en-US

2008466_en-US

RW612 - wifi_mqtt example "download firmware failed"

I have a FRDM-RW612 board, and I'm trying to run the "wifi_mqtt" example from the SDK (version 2.16.100, build 858, 2024-10-02) using MCUXpresso IDE v24.9 (currently the latest release).  I'm able to build it and download it using the built-in MCU-Link.  But when I run it, I get the following:

************************************************
MQTT client example
************************************************
[i] Initializing Wi-Fi connection...
[wifi_io] Error: Download firmware failed
[wifi] Error: imu_wifi_init failed. status code -1
[wlcm] Error: wifi_init failed. status code -1
[!] WPL Init failed: 1

If I enable CONFIG_WIFI_IO_DEBUG, I just get a few more lines of output.  Here's the relevant code snippet:

imu_wifi_init() from wifi-imu.cimu_wifi_init() from wifi-imu.cimu_wifi_init() from wifi-imu.c

Commenting line 1612 has no effect.  Resetting the board manually or unplugging and replugging it produces the same result.  I read doc/readme.md, and it mentions "select Wi-Fi module macro in the app_config.h. (see #define WIFI__BOARD_)."  This is the contents of app_config.h:

app_config.happ_config.happ_config.h

Am I doing something wrong?  This should be an out-of-the-box example, I'm not sure why it's failing.  Thanks.

Dana M.

Product: WiFi RW6XXRe: RW612 - wifi_mqtt example "download firmware failed"

Ha, nope, that was it.  It would be super useful for folks if there was a mention of that specific user manual and section in the readme.md for the Wi-Fi sample projects.  I've developed on NXP MCUs for a long time, but having to put a separate binary blob into flash first using a separate manual J-Link command is a new trick. 

For those out there running Windows, here's a useful batch file for programming the firmware.  Put it in component\conn_fwloader\fw_bin and edit the path to JLink.exe if needed.


@set JLINK="C:\Program Files\SEGGER\JLink\JLink.exe"
@set FIRMWARE="rw61x_sb_wifi_a2.bin"
@set FLASH_ADDRESS=0x08400000
@set COMMAND_FILE="jlink_command.txt"
@echo loadbin %FIRMWARE%,%FLASH_ADDRESS% > %COMMAND_FILE%
@echo quit >> %COMMAND_FILE%
%JLINK% -device RW612 -if SWD -speed 4000 -CommandFile %COMMAND_FILE%
@pause

 Thanks for the pointer.

Dana M.

Re: RW612 - wifi_mqtt example "download firmware failed"

Hi,

Could you please confirm you downloaded the Wi-Fi firmware using J-Link?

Please check section 4.1.1 in UM11799 (available in your SDK bundle).

Regards,

Daniel.

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 11:02 PM
Updated by: