Hello,
How to use the onboard debugger? After checking the getting started, I choosed the predefined debug configuration for PEmicro as seen in screenshot:
but I always got an error:
Error in services launch sequence
PEmicro GDB Launch Failure : Unable to auto-detect debug hardware. Please specify on the command-line. If running from Eclipse, check the launch Debug Configuration settings. Halting.
Can somebody help me here? Do I have to install some kind of driver?
Thanks a lot.
Hi,
From the image shared above, we can see that the USB port has not been detected (in port box).
We suggest changing the USB cable, see the Default Jumper Configuration and trying again, check if the port is recognized in the Device Manager and refresh the Debug Configurations window.
If no changes are observed, please verify if the PEMicro Debugging Support package requires an update.
Note: No changes are required in the Debug Configuration for the examples.
Hope it helps you.
BR,
IsaulO.