hi NXP
I want to enable secure boot Android14 on IMX8MP platform, when i exec cmd in uboot found following some error:
u-boot=> hab_status
Secure boot enabled
HAB Configuration: 0xcc, HAB State: 0x99
--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x1c 0x45 0x33 0x18 0xc0 0x00
0xca 0x00 0x14 0x00 0x02 0xc5 0x1d 0x00
0x00 0x00 0x0a 0x10 0x40 0x1f 0xad 0xc0
0x00 0x00 0x30 0x20
STS = HAB_FAILURE (0x33)
RSN = HAB_INV_SIGNATURE (0x18)
CTX = HAB_CTX_COMMAND (0xC0)
ENG = HAB_ENG_ANY (0x00)
--------- HAB Event 2 -----------------
event data:
0xdb 0x00 0x1c 0x45 0x33 0x18 0xc0 0x00
0xca 0x00 0x14 0x00 0x02 0xc5 0x1d 0x00
0x00 0x00 0x0a 0x10 0x40 0x1f 0xad 0xc0
0x00 0x00 0x30 0x20
STS = HAB_FAILURE (0x33)
RSN = HAB_INV_SIGNATURE (0x18)
CTX = HAB_CTX_COMMAND (0xC0)
ENG = HAB_ENG_ANY (0x00)
u-boot=>
Secure boot enabled
HAB Configuration: 0xcc, HAB State: 0x99
--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x1c 0x45 0x33 0x18 0xc0 0x00
0xca 0x00 0x14 0x00 0x02 0xc5 0x1d 0x00
0x00 0x00 0x0a 0x10 0x40 0x1f 0xad 0xc0
0x00 0x00 0x30 0x20
STS = HAB_FAILURE (0x33)
RSN = HAB_INV_SIGNATURE (0x18)
CTX = HAB_CTX_COMMAND (0xC0)
ENG = HAB_ENG_ANY (0x00)
--------- HAB Event 2 -----------------
event data:
0xdb 0x00 0x1c 0x45 0x33 0x18 0xc0 0x00
0xca 0x00 0x14 0x00 0x02 0xc5 0x1d 0x00
0x00 0x00 0x0a 0x10 0x40 0x1f 0xad 0xc0
0x00 0x00 0x30 0x20
STS = HAB_FAILURE (0x33)
RSN = HAB_INV_SIGNATURE (0x18)
CTX = HAB_CTX_COMMAND (0xC0)
ENG = HAB_ENG_ANY (0x00)
how Can I do fix this error
Please find the attachment.
Regards
Harvey
Sorry, I can't understand it , please give me the detail steps or docs.
Hi @liangyan
The given context is HAB_CTX_COMMAND, this means the remaining bytes correspond to the CSF command that caused the event. You can refer to the HAB API v4 from the CST tool, and there is
Regards
Harvey