Hello Community,
We need to flash, debug and read logs from the iMX93's M33 processor, using the MCUXpresso VSCode extension. Would any of the following options allow us to use SWD/SWO with the iMX93:
The Getting Started doc for the iMX93 mentions only the Segger J-Link Plus.
Enrique
Hi @enrique001!
At the moment we only validate the Segger J-Link Plus.
According to the documentation of Segger the MCU-Link Pro with J-Link LITE firmware should support iMX processors too, but that are not validated by us.
You can contact to Segger to confirm if MCU-Link Pro with J-Link LITE firmware supports iMX93.
Best Regards!
Chavira