2006445_zh-CN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2006445_zh-CN

2006445_zh-CN

MPX2102AP AND MPX2102GP

原设计了一款适合于AP系列的压力传感器电路,利用它输出的两个电压的压差去计算压力,现在想直接用GP系列去替换,电路上不做任何修改,现在发现输出的压差很小,电路设计上无法满足。然后想问下,GP在使用电路设计上与AP系列有什么区别,也是利用它的两个输出压差去作为压力计算吗?

Re: MPX2102AP AND MPX2102GP

请看你的新的ticket回复的:

Re: HOW TO USE THE MPX2202GP - NXP Community

Re: MPX2102AP AND MPX2102GP

在电路使用上呢,比如说我将传感器输出的两个电压先放大,在相减,如果不考虑代码上的差异,电路上有需要修改的地方吗

Re: MPX2102AP AND MPX2102GP

Hi ZIMO

请看他们的区别:

guoweisun_0-1733299405727.pngguoweisun_0-1733299405727.png

The differential voltage output of the sensor is directly
proportional to the differential pressure applied.


The absolute sensor has a built-in reference vacuum. The
output voltage will decrease as vacuum, relative to ambient,
is drawn on the pressure (P1) side.


The output voltage of the differential or gauge sensor
increases with increasing pressure applied to the pressure


希望能帮到您!

多谢!

Tags (1)
No ratings
Version history
Last update:
‎02-04-2026 07:22 AM
Updated by: