2006445_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2006445_en-US

2006445_en-US

mpx2102ap and mpx2102gp

I designed a pressure sensor circuit for the AP series and used the difference between its two output voltages to calculate pressure, but now I want to replace it with the GP series without any modification to the circuit, and now I realize that the output pressure difference is so small that the circuit design is not satisfactory. Then I would like to ask, what is the difference between the GP and AP series in terms of circuit design, and is it also utilizing the difference between its two output voltages for pressure calculation?

Re: MPX2102AP AND MPX2102GP

Please see your new ticket reply's:

Re: HOW TO USE THE MPX2202GP - NXP Community

Re: MPX2102AP AND MPX2102GP

What about circuit usage, for example, if I amplify the two voltages from the sensor output and subtract them in phase, are there any modifications that need to be made to the circuit without taking into account the differences in code?

Re: MPX2102AP AND MPX2102GP

Hi ZIMO

See the difference between them:

guoweisun_0-1733299405727.png

The differential voltage output of the sensor is directly
proportional to the differential pressure applied.


The absolute sensor has a built-in reference vacuum. The
output voltage will decrease as vacuum, relative to ambient,
is drawn on the pressure (P1) side.


The output voltage of the differential or gauge sensor
increases with increasing pressure applied to the pressure


I hope this helps!

Thanks a lot!

Tags (1)
No ratings
Version history
Last update:
‎02-04-2026 07:21 AM
Updated by: