2005415_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2005415_en-US

2005415_en-US

RT1050 EVK SWO

Using the Hello World SWO project, I am still unable to get SWO (or ITM console) to work.

-MCUXpresso v24.9

- R428 installed (EVKB)

- EVK has LPCLink2 firmware flashed

- launch file and sdk manifest both have has_swo to true (not sure why recent SDKs do not have this set to true by default?). SDK version 2.16

I'm still missing something though, as things are not working.

I believe the processor is configured properly, as I see activity on the SWO pin (confirming that pins and clocks are set properly). There is no output on ITM Console. Therefore I believe I'm missing some setting in the the IDE/debugger.

The SWO Trace Config tab lets me change the clock speed. Before selecting the 'Change' button, the SWO and Trace Console shows the below (so far, so good):

Generic ROM base address: 0xE00FD000


***---------- Identify CoreSight Components ----------***

Unchecked ROM Table class 15 at address E0043000

Identified component Address 0xE0040000 CID1 = 144 PID0 = 169 PID1 = 185 PID2 = 11 PID3 = 0 DEVARCH = 0x0 Revision = 0

Identified component Address 0xE0041000 CID1 = 144 PID0 = 117 PID1 = 185 PID2 = 27 PID3 = 0 DEVARCH = 0x47704A13 Revision = 1

Identified component Address 0xE0042000 CID1 = 144 PID0 = 6 PID1 = 185 PID2 = 75 PID3 = 0 DEVARCH = 0x0 Revision = 4

Identified component Address 0xE000E000 CID1 = 224 PID0 = 12 PID1 = 176 PID2 = 11 PID3 = 0 Revision = 0

Identified component Address 0xE0001000 CID1 = 224 PID0 = 2 PID1 = 176 PID2 = 11 PID3 = 0 Revision = 0

Identified component Address 0xE0002000 CID1 = 224 PID0 = 14 PID1 = 176 PID2 = 11 PID3 = 0 Revision = 0

Identified component Address 0xE0000000 CID1 = 224 PID0 = 1 PID1 = 176 PID2 = 11 PID3 = 0 Revision = 0


otsl_1-1733170687860.png

Clicking the Change button presents me with the dialog to set clock speeds. Detect does not work. When I add the two clock speeds (Core: 600MHz and Trace 132MHz), with SWO configured by IDE, I see the following messages in the SWO and Trace Console:

***---------- Considered CoreSight Components ----------***

Error creating CoreSight component CS_DWT at address 0xE0001000

Error creating CoreSight component CM7_ITM at address 0xE0000000

Error creating CoreSight component CM7F_TPIU at address 0xE0040000

Error creating CoreSight component CM7_MIMXRT_ETM at address 0xE0041000


otsl_0-1733170359493.png
 
i.MXRT 105x回复: RT1050 EVK SWO

Thanks for your update and additions!

I did have to use several of the debuggers specified in the AN to get it to work in my previous tests, and I will document your experience. Thank you for your contribution!

回复: RT1050 EVK SWO

Just wanted to confirm that, contrary to the support statement above, the onboard debugger DOES support SWO (as it should, because the configuration is electrically the same as using an external LPCLink2 debugger).

To get the SWO trace facility to work (using the 25.03.00 SDK), I needed to modify the manifest file within the SDK (to set SWO to true), then reinstall the SDK within the IDE. The second important part is that if the debugger is in all-stop mode, all configuration changes (setting clock speeds, and enabling the console) need to be done with program execution paused. If the debugger is in non-stop mode, these can be done while running. 

回复: RT1050 EVK SWO

Hi @otsl.

The LPC-Link2 mentioned in the AN is an external standalone debugger. Just flashing the firmware with the on-board debugger does not fulfil the condition.


回复: RT1050 EVK SWO

The on-board debugger is detected as: "Probe Firmware: LPC-LINK2 CMSIS-DAP V5.460 (NXP Semiconductors)". The application note (which I have read) says LinkServer LPC-Link2 is supported. The EVK has SWO routed to the on-board debugger as "TDO_SWO".

I can't see why it is not supported in the configuration I have. Are you saying that despite meeting the above requirements, it is not supported?



回复: RT1050 EVK SWO

Hi @otsl ,

Thanks for your interest in NXP MIMXRT series!

SWO is dependent on the debugger. Simply using the on-board debugger is not an option.

Gavin_Jia_0-1733470299810.png


Please kindly refer to the AN13234 How to Enable SWO Trace for i.MX RT10xx Series. It is more recommended to use an external JLink debugger.

Best regards,
Gavin

标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 09:21 PM
更新人: