Hi,
I'm considering using i.MX 8M plus processor for video encoding with H.264/H.265 codecs.
Application will receive two uncompressed unencrypted digital video input streams 1080p60 through MIPI CSI-2 interfaces. Both videos should be compressed to reduce data throughput and transmitted out through 1 GE interface.
I'm wondering if Video Processing Unit in the i.MX 8M plus processor is capable to encode simultaneously two video streams?
Is there anybody who has hands-on experience with similar application and can estimate VPU performance and capabilities?
Thanks,
Hi @joanxie ,
Could VPU handle simultaneous encoding of two reduced input video streams?
Say 2x 1080p30, or 2x 1080i30, or 2x 720p30?
Could this work?
Thanks,
i.mx8mp has dual mipi csi, each one can support 1080p@60, but VPU couldn't handle two 1080p@60 steaming encoding, imx8mp vpu only can handle encoding up to 1080p@60,