2004149_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2004149_en-US

2004149_en-US

code warrior floating license 注册license时提供的ip 有限制么,局域网ip可以么

JimmyXubuhler_0-1732865672368.png


Re: Code Warrior Floating License Is there any restriction on the IP provided when registering the license? Can the LAN IP be used?

Thank you so much!!

Re: Code Warrior Floating License Is there any restriction on the IP provided when registering the license? Can the LAN IP be used?

Did any error messages pop up during the compilation process? If no error messages appear, there should be no problem. But if errors still appear, you'd better confirm with Jorge again, license-related issues, he is an expert and can give you more professional advice.

Re: Code Warrior Floating License Is there any restriction on the IP provided when registering the license? Can the LAN IP be used?Thank you very much for your reply. I can now compile the code and build the target normally. Is there any hidden danger of compilation or license compliance in the compiled files?Re: code warrior floating license 注册license时提供的ip 有限制么,局域网ip可以么

Hi Jimmy Xu,

很抱歉你的问题还没有被解决。License支持哪一个版本,standard 还是 professional, 这取决于你购买时的选择。

Celeste_Liu_0-1733367727569.png


Professional的功能是最全的,Standard功能会少一些。

老实说,CodeWarrior license 不是我的专业领域。我看到你还有一个private ticket, 已经有license team的support在跟进了。

希望 license team 的同事能够顺利解决你的问题,如有任何新的情况,请及时告知我们。

BRs,

Celeste

Re: Code Warrior Floating License Is there any restriction on the IP provided when registering the license? Can the LAN IP be used?Without starting the server, lincese shows two lines of error (network problem, I can't post the picture), combined with the previous results: the lower line is activated. Does the license only support the standard edition MCU 10.5 version, but not the professional edition MCU 10.5?Re: code warrior floating license 注册license时提供的ip 有限制么,局域网ip可以么

Hello JimmyXu,

我找到了下面的链接:Floating License -Environment Variables. - NXP Community

里面提到环境变量的设置,我不确定它是否与你遇到的问题有关,你可以试一下。

除此之外,你还可以尝试一下移除license,然后重新导入并重启codeWarrior,看看是否有效果。

BRs,

Celeste

Re: code warrior floating license 注册license时提供的ip 有限制么,局域网ip可以么

JimmyXubuhler_0-1733275111696.png

使用code warrior floating license,在官网生成license.dat后,在服务器上运行lmtools,服务正常启动。

JimmyXubuhler_1-1733275242785.png


client 使用和server相同的license.dat ,启动code warrior后报错

JimmyXubuhler_0-1733275111696.png


如何解决?


Re: code warrior floating license 注册license时提供的ip 有限制么,局域网ip可以么

Hello Jimmy,

我认为局域网是可以的,你可以尝试下。

BRs,

Celeste

Re: Code Warrior Floating License Is there any restriction on the IP provided when registering the license? Can the LAN IP be used?

JimmyXubuhler_0-1733277510813.png

Pop-up window when opening code warrior

Re: Code Warrior Floating License Is there any restriction on the IP provided when registering the license? Can the LAN IP be used?

JimmyXubuhler_0-1733360560569.png

This is the picture


Tags (1)
No ratings
Version history
Last update:
‎01-06-2026 01:35 AM
Updated by: