2003960_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2003960_en-US

2003960_en-US

The image generated by the provisioning tool does not match, I did not see "FCFB

1111111111.png2222222.png33333.png

##########################################################################################################
生成构建脚本: build_image_lnx.sh
生成构建脚本: build_image_win.bat
生成构建脚本: build_image_mac.sh
正在执行脚本C:\Users\Administrator\secure_provisioning00\build_image_win.bat
###脚本: 构建镜像: C:\Users\Administrator\secure_provisioning00\build_image_win.bat
Build HAB image
nxpimage hab export -c "C:\Users\Administrator\secure_provisioning00\bd_files\imx_application_gen_win.bd"  -o "D:\RT1052_Example Code\Example\1.led_test\hello_world_boot.bin"  "C:\Users\Administrator\secure_provisioning00\source_images\hello_world.srec"
Success. (HAB container: D:\RT1052_Example Code\Example\1.led_test\hello_world_boot.bin created.)
nxpimage succeeded
### Build flashloader as unsigned bootable image ###
nxpimage hab export -c "C:\Users\Administrator\secure_provisioning00\bd_files\unsigned_MIMXRT1050_flashloader_win.bd"  -o "C:\Users\Administrator\secure_provisioning00\bootable_images\unsigned_MIMXRT1050_flashloader.bin"  "C:\nxp\MCUX_Provi_v10\bin\_internal\data\targets\MIMXRT1050\flashloader.srec"
Success. (HAB container: C:\Users\Administrator\secure_provisioning00\bootable_images\unsigned_MIMXRT1050_flashloader.bin created.)
nxpimage succeeded
###脚本“构建镜像”的结果: 成功(返回代码= [0]成功)
操作的状态: 成功: 构建镜像
Re: The image generated by the provisioning tool does not match, I did not see "FCFBIndeed, this issue has been resolved. thank you.Re: The image generated by the provisioning tool does not match, I did not see "FCFBHi,
in your screenshot I can see the file name has "SDRAM" in it, but also in the screenshot the DCD is not configured, it might be the root cause why the application does not run.

Regards,
Libor
Re: The image generated by the provisioning tool does not match, I did not see "FCFB

Hi,

may be the training video can help you. There should be all steps captured:

Secure Boot on the i.MX RT10xx Crossover MCUs | NXP Semiconductors


If you cannot find any information in the user guide, please let us know what information is missing. It is not possible to provide help without information:

- what you want to do

- what the problem is.

Re: The image generated by the provisioning tool does not match, I did not see "FCFBCan't I run the LED program even after writing it in PROVISION TOOL? The image construction is incorrect. I can run it using KEIL's original image. Is it not possible to follow the official manual step by step? The documentation for this tool is not detailed enough. I can't use it.Re: The image generated by the provisioning tool does not match, I did not see "FCFB

Hi, MCUXpresso Secure Provisioning tool does not generate the image with FCB, the FCB is written to flash as extra step. The FCB can be specified either as simplified or full configuration.

Kindly review generated write script for details.


Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 02:34 PM
Updated by: