sdphost succeeded, HAB disabled
### Build flashloader as unsigned bootable image ###
nxpimage hab export -c "C:\Users\Administrator\secure_provisioning00\bd_files\unsigned_MIMXRT1050_flashloader_win.bd" -o "C:\Users\Administrator\secure_provisioning00\bootable_images\unsigned_MIMXRT1050_flashloader.bin" "C:\nxp\MCUX_Provi_v10\bin\_internal\data\targets\MIMXRT1050\flashloader.srec"
Success. (HAB container: C:\Users\Administrator\secure_provisioning00\bootable_images\unsigned_MIMXRT1050_flashloader.bin created.)
nxpimage succeeded
### Write FlashLoader ###
sdphost -p COM9,115200 -j -- write-file 0x20001C00 "C:\Users\Administrator\secure_provisioning00\bootable_images\unsigned_MIMXRT1050_flashloader.bin"
Status (HAB mode) = 1450735702 (0x56787856) Hab Is Disabled (Unlocked).
Response status = 2290649224 (0x88888888) Write File Success.
sdphost succeeded, HAB disabled
### Start FlashLoader ###
sdphost -p COM9,115200 -j -- jump-address 0x20001C00
Status (HAB mode) = 1450735702 (0x56787856) Hab Is Disabled (Unlocked).
sdphost succeeded, HAB disabled
### Waiting FlashLoader to be initialized for 3 seconds ###
### Timeout wait value can be adjusted from Preferences ###
### Check presence of FlashLoader ###
blhost -t 2000 -p COM9,115200 -j -- get-property 1 0
SpsdkNoDeviceFoundError: No devices for given interface 'uart' and parameters 'port=COM9, baudrate=115200, timeout=2000' was found.
blhost failed

Hi,
I'd recommend to download SDK from http://mcuxpresso.nxp.com and try to debug the flashloader example project to find the problem,
In MCUXpresso Secure Provisioning tool we provide pre-compiled flashloader from the SDK which works with EVK board. If you need custom flashloader, you can replace the provided flashloader, which can be found in \nxp\MCUX_Provi_v9\bin\_internal\data\targets\MIMXRT1050\flashloader.srec
Replacing the MCU will solve the problem, I used my own hardware board. thank you
Hello,
you have not provided enough information about your setup and hardware - do you use your own HW, od do you use NXP EVK(B)?
Anyway, in your screenshot I can see that the "ROM bootloader" is active (ISP after reboot). In this case only the sdphost can communicate with ROM and is used for uploading flashloader. Once flashloader is active, only after that you can use blhost.
In case flashloader is not present or did not start, it emits `SpsdkNoDeviceFoundError: No devices for given interface 'uart' and parameters...` error.
In your script output it seems that flashloader either was not ready yet, or it did not start. Have you tried to increase the timeout in Preferences do reduce the list of potential errors?
Regards,
Libor