dear nxp
When I add SW32K3xx_S32DS_3.5.0_D2303.zip thur offline as below,
How can I find what I have added in this list?
Thanks,
Bryan
Hi Bryan,
According to the installation package name.
Or refer to HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5 to install one by one.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------