2000792_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2000792_en-US

2000792_en-US

s32g sja1110 startup

Hi,

I am developing the functions of SJA1110 recently, and I know very little about it. Currently, the SJA1110 S32 SDK is being applied for by the supplier. I can only learn about the functions of SJA1110 through "S32G2_LinuxBSP_39.0_User_Manual.pdf" and posts on the forum. So I have the following questions:
1. What are the functions of SJA1110 S32 SDK? Can I use this SDK to configure the port functions of SJA1110 on S32DS? Because the network interface of our customized version is slightly different from that of S32G2-VNP-RDB2
2. At present, because the SJA1110 S32 SDK is being applied for, I downloaded Godvip1.1.0 from the official website. From the user manual, I saw that the supported linux bsp version is 39, and extracted the sja1110 firmware from it. So I also downloaded yocto's bsp39 in my linux environment, and modified the build/conf/local.conf file, added the paths of sja1110_uc.bin and sja1110_switch.bin, and finally compiled and generated the .sdcard file, burned the image to my SD card, and finally loaded it in S32G2-VNP-RDB2. I set SW12 to 1-0 and started from norflash. Finally, I found from the serial port log that the SJA1110 function was not enabled. I put the log in the attachment. Please help me analyze the reason and give suggestions. Thank you
3. Finally, I would like to ask, for the development of SJA1110, my understanding is that data is written to SJA1110 through SPI, so it should be feasible for A core or M core control;
3.1 But why do I see in the forum that everyone is basically developing based on A core?
3.2 If you want to modify the port function of SJA1110, how should you modify it?
Please give me some suggestions, thank you~

SJA1110 S32G2 S32G-VNP-RDB2 

回复: s32g sja1110 startup

hi,jiajun_cheng

Thank you for your reply.

For details, see 4. SJA1110 Port4 PHY Speed Configuration in the S32G-VNP-RDB2 Reference Design Ethernet Enablement Guide (download linkS32G-VNP-RDB2 Reference Design Ethernet Enablement Guide)

In addition, “Upload successfully verified” means SJA1110 image loaded successfully, and SJA1110 Port will work on your configuration

Hope it can help you.

BR

Joey



回复: s32g sja1110 startup

Hi, @Joey_z :

In the afternoon, my SJA1110 SDK application was approved, and I followed" S32G-VNP-RDB3 Ethernet Enablement Guide"Loaded switch_uc.bin.For the configuration of sja1110, is there any article for RDB2 development board.Is there any article that explains it in more detail?


s32g274ardb2 login: root
root@s32g274ardb2:~# dmesg | grep sja1110
[    0.548540] gpio-24 (sja1110-rst-phy-t1): hogged as output/low
[    0.553963] gpio-81 (sja1110-rst-core): hogged as output/low
[    0.619550] sja1110-sw@1 enforce active low on chipselect handle
[    8.417247] sja1110: loading out-of-tree module taints kernel.
[    8.417843] SPI driver sja1110 has no spi_device_id for nxp,sja1110-switch
[    8.417852] SPI driver sja1110 has no spi_device_id for nxp,sja1110-uc
[    8.417961] sja1110 spi5.0: probing uc
[    8.418121] sja1110 spi5.1: probing switch
[    8.418445] sja1110 spi5.1: Could not get GPIO from device tree
[    8.418473] sja1110 spi5.1: [sja1110_post_probe_upload_worker] Trying to initialize switch
[    8.418628] sja1110 spi5.1: Direct firmware load for sja1110_switch.bin failed with error -2
[    8.418641] sja1110 spi5.1: request_firmware failed with -2
[    8.418648] sja1110 spi5.0: [sja1110_post_probe_upload_worker] Trying to initialize uC
[    8.425720] sja1110 spi5.0: [sja1110_init_hw] loaded fw 'sja1110_uc.bin'
[    8.425740] sja1110 spi5.0: [sja1110_pre_uc_upload] Found firmware of size 126400
[    8.425844] sja1110 spi5.0: [sja1110_pre_uc_upload] firmware appears to be valid
[    8.425896] sja1110 spi5.0: [sja1110_pre_uc_upload] \xc2\xb5C not ready for download (Status=0x31)
[    8.426017] sja1110 spi5.0: Uploading firmware...
[    8.733955] sja1110 spi5.0: Upload successfully verified!


回复: s32g sja1110 startup

hi,jiajun_cheng

Thank you for contacting us.
1. I will further test the problems encountered in put sja1110_uc.bin and sja1110_switch.bin in /lib/firmwarene.Thank you  for your information.
2. In addition, Refer to UGS32G-VNP-RDB3-ethernet-enablem-guide.pdf (3.sJA1110 Port Configuration) Section 3 (download link S32G-VNP-RDB3 Ethernet:S32G-VNP-RDB3 Ethernet Enablement User Guide). The  User Guide describes how to configure port functionality for SJA1110 using the S32DS.
3. I think data is written to SJA1110 through SPI, and it should be ok to control SJA1110 with A core or M core. I will conduct internal consultation on the specific reasons and reply to you as soon as possible after getting the result.

Hope it can help you.

BR

Joey

回复: s32g sja1110 startup

After reading this article, I chose to put sja1110_uc.bin and sja1110_switch.bin in /lib/firmware, and the log is as follows

root@s32g274ardb2:~# dmesg | grep sja
[ 0.544308] gpio-345 (sja1110-rst-phy-t1): hogged as output/low
[ 0.549823] gpio-402 (sja1110-rst-core): hogged as output/low
[ 0.615697] sja1110-sw@1 enforce active low on chipselect handle
[ 7.283003] sja1110: loading out-of-tree module taints kernel.
[ 7.290192] SPI driver sja1110 has no spi_device_id for nxp,sja1110-switch
[ 7.290198] SPI driver sja1110 has no spi_device_id for nxp,sja1110-uc
[ 7.290309] sja1110 spi5.0: probing uc
[ 7.290468] sja1110 spi5.1: probing switch
[ 7.290781] sja1110 spi5.1: Could not get GPIO from device tree
[ 7.290809] sja1110 spi5.1: [sja1110_post_probe_upload_worker] Trying to initializ e switch
[ 7.294511] sja1110 spi5.1: [sja1110_init_hw] loaded fw 'sja1110_switch.bin'
[ 7.294621] sja1110 spi5.1: [sja1110_pre_switch_upload] Found switch config of siz e 2236
[ 7.294768] sja1110 spi5.1: Uploading config...
[ 7.373625] sja1110 spi5.1: Successfully configured!
[ 7.373655] sja1110 spi5.0: [sja1110_post_probe_upload_worker] Trying to initializ e uC
[ 7.394231] sja1110 spi5.0: [sja1110_init_hw] loaded fw 'sja1110_uc.bin'
[ 7.394252] sja1110 spi5.0: [sja1110_pre_uc_upload] Found firmware of size 320280
[ 7.394370] sja1110 spi5.0: [sja1110_pre_uc_upload] firmware appears to be valid
[ 7.394422] sja1110 spi5.0: [sja1110_pre_uc_upload] µC not ready for download (Sta tus=0x31)
[ 7.394649] sja1110 spi5.0: Uploading firmware...
[ 8.200328] sja1110 spi5.0: Upload successfully verified!


Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 02:47 PM
Updated by: