I am developing a wearable device using the PC9420 and RT6 series.
It runs on a battery, so I need to charge it.
Question
1.After switching from MODE0 to standby with PWR_DN_EN=1, is it possible to charge it by inputting 5V to VIN?
2.After switching to standby with PWR_DN_EN=1, I would like to turn on the LED when charging is complete. Is this possible if I use the INT pin?
I would like the LED to light only when charging is complete.
Thank you in advance.
Hi
I will test it next this function and give you feedback ASAP!
Hi teruteru5678
Question
1.After switching from MODE0 to standby with PWR_DN_EN=1, is it possible to charge it by inputting 5V to VIN?
[gw]do you mean enable charger function under power down status?
Thanks!
BR