1998885_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1998885_en-US

1998885_en-US

error in installing extension

version:S32DS for S32 Platform 3.4

When I install the extension"S32SDK S32K1XX RTM4.0.3"online,it says"Operation detailsSoftware being installed: com.nxp.s32ds.s32k1.dev.feature.feature.group 1.0.0.202106101451 Missing requirement: com.nxp.s32ds.s32k1.dev.feature.feature.group 1.0.0.202106101451 requires 'org.eclipse.equinox.p2.iu; com.nxp.s32ds.cle.s32k1.s32k142w.dev.feature.feature.group [1.0.0.202106101446,1.0.0.202106101446]' but it could not be found".The screenshot is below.

So I tried to install it offline, but I searched this extension in nxp.com,there is only"S32SDK S32K1XX RTM4.0.2".

The extension"S32K1XX development package"is the same case.

how can i solve this problem?


Re: error in installing extensionit is useful! thanks very muchRe: error in installing extension

Hi @michaelcr97 and @rereli ,

Sorry for the inconvenience we bring you!

it is recommended to change Available S32DS Software Sites to https. This has been discussed in Where can I find it?S32_SDK_S32K1xx_RTM_4.0.3.

S32DS Extensions and Updates https.jpgS32DS Extensions and Updates https.jpg


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

Re: error in installing extension

Where is the red X.Is it?But i think it is a red + hahahah~

rereli_1-1732497776374.jpegrereli_1-1732497776374.jpeg



Re: error in installing extension

Actually in my case, if I go to help->installation details-> and I expand S32Design Studio I will find that eclipse requirments market with a red "x", seems those were not installed. I attached a picture:

michaelcr97_0-1732442307684.pngmichaelcr97_0-1732442307684.png


Re: error in installing extensionI will send an email to nxp.If i get reply, i will update here.Re: error in installing extension

unfortunately it didn`t worked to install it offline too

Re: error in installing extension

I`m trying to install those extensions offline, I will come up with updates here if I will succeed.

Re: error in installing extensionYes,actually,i can't install every extension online in this tab.Re: error in installing extension

Hello, I get the same error when I try to install a different development package than yours, but from the same tab.

标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 02:50 PM
更新人: