1998675_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1998675_en-US

1998675_en-US

Target Reset Pattern

Hello,all

Can the I3C module of the LPC55xx family of chips send a "Target Reset Pattern" through a configuration register?Whether the T-bit of the I3C command is automatically calculated by the hardware or can be configured by software.

LPC55xxRe: Target Reset Pattern

Hi @lb_h 

In the LPC55xx family, the I3C module does not have a dedicated configuration register to directly send the “Target Reset Pattern.” However, it supports sending custom command sequences, which can be used to generate the reset pattern manually by software.

The T-bit is typically calculated automatically by the hardware based on the I3C command.

BR

Harry

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 02:50 PM
Updated by: