1998038_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1998038_en-US

1998038_en-US

XTALI/XTALO Tolerances

the datasheet of the i.MX RT1050(Page 16, i.MX RT1050 Crossover Processors Data Sheet for Consumer Products, Rev. 2, 03/2021) mentions for XTALI/XTALO:

If this clock is used as a reference for USB, then there are strict frequency tolerance and jitter
requirements. See OSC24M chapter and relevant interface specifications chapters for details.

i cant find any information on this is the Datasheet, reference manual of GW Development Guide.


can anyone provide me this information? 

Re: XTALI/XTALO Tolerances

Thank you for your swift Reply!

Re: XTALI/XTALO Tolerances

This was mentioned on previous versions of the HW development guide but I think it was removed as there could be specific tolerance requirement for different applications. 

The +-50 ppm accuracy is required for the Ethernet while the +-100 ppm accuracy is required for the USB, this is for the 4digits RTs. 

Best regards,
Omar

Re: XTALI/XTALO Tolerances

and of course do i mean HW Development Guide i.s.o.  GW Development Guide


タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 02:53 PM
更新者: