Hi,
I am trying to use an S32 debug probe to connect to our custom S32K344 board in DS. Although the connection test passes, the device and core do not appear in the debugger configuration window. When I check the available list, only S32G2/3 options are shown. I have already installed the S32K development package and upgraded to the latest S32K RTD version. Can anyone advise on how to get the probe working with the S32K MCU?"
Thanks,
XD
Hi
According to the information in chapter 2.1 Release content of S32K3xx_Development_Package_Release_Notes_3.5.13_RTM.pdf, S32 Debug Probe does not seem to support S32K344.
2.1 Release content
• Support for wizards creating application and library projects for the S32K3xx processor family
• GCC version 10.2.0 20200910, build 1728 revision g5963bc8.
• GCC version 9.2.0 20190812 build 1649 revision gaf57174.
• Green Hills 2021.1.4 compiler support.
• WindRiver DIAB 7.0.6 compiler support.
• IAR 8.50.10 compiler support.
• PEmicro debug probes support for RAM and FLASH configurations (Integrate new PnE 5.8.7 into S32K3xx development package)
• Lauterbach probe support for running from RAM and FLASH
• IAR debugger support.
• TASKING debugger support.
• Segger debugger support.
• VDK Debugger support
• S32 Configuration Tools support (Pins, Clocks, Peripherals, DCD (DCF Tool), IVT).
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------