1994059_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1994059_en-US

1994059_en-US

Inquiry About Error Occurring When Deleting Pins in S32DS3.5 RTD 4.0.0

Hello, I have a question about assigning pins using S32DS3.5 RTD 4.0.0, and I would like to ask for your help.


studyseok8466_0-1731541336816.png

[Image 1]


In Image 1, you can see the default PTA0 GPIO pin and the PTE26 pin that I configured.

At this stage, there are no particular errors.


studyseok8466_1-1731541354515.png

[Image 2]


In Image 2, I deleted the PTA0 pin since it is not being used.


studyseok8466_2-1731541368139.png

[Image 3]

studyseok8466_3-1731541372322.png

[Image 4]


However, as shown, an error occurs. This error seems to indicate an issue with the Siul2_Port module, as demonstrated in [Image 3] and [Image 4].

Why does this error occur?

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 10:19 PM
更新者: