1993708_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1993708_en-US

1993708_en-US

PTE13 ADC1_S19 and VRC_CTRL

Hello,

I am facing issues with reading the analog channel s32k344, specifically on port PTE13 ADC1_S19. I found something on the forum about VRC_CTRL. I tried disabling this function, but then the readings became 0.


What might I be forgetting to configure for the ADC readings to work?

Re: PTE13 ADC1_S19 and VRC_CTRLThanks, its working. I took another MCU. Unfortunately the issue has been caused, because ADC pin stopped working.Re: PTE13 ADC1_S19 and VRC_CTRL

Pay attnention to following thread:
https://community.nxp.com/t5/S32K/S32K3-PTE13-ADC1-S19-acquisition-abnormal-jumps/td-p/1606820

If VRC_CTRL is disabled, then you can use it as ADC channel. Check whether you don't have it driven by GPIO or other function to GND (SIU configuration for PTE13 i.e.GPIO[141]) or whether this signal is not externally pulled down.

标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 03:04 PM
更新人: