1993674_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1993674_en-US

1993674_en-US

Yocto iMX8M Plus boot kernel loop with "eth_lpi not found"

iMX8M Plus configured for Yocto on Variscite DART-MX8M-PLUS, booting from eMMC.

While starting the kernel it fails to ever finish booting as it loops, printing "IRQ eth_lpi not found" messages over and over. I suspect the issue might be with the device tree but do not know for certain and also do not know how this would be remedied.

Boot log is attached.

Thank you in advance for any guidance.

i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlusYocto ProjectRe: Yocto iMX8M Plus boot kernel loop with "eth_lpi not found"Thanks for the quick reply. In our case we do have both Ethernet devices but one is not being seen. As you say, it’s odd it stops it booting. Shall continue discussions with Variscite support.

Thanks again. The device tree link may come in handy.
Re: Yocto iMX8M Plus boot kernel loop with "eth_lpi not found"

Hi, sorry to leave the post unanswered. I did resolve the issue;

Variscite responded to me with the following after I described the issue to them:

"The message you are reporting is just an expected harmless warning.
You may want to edit the device tree and remove the second ethernet here
https://github.com/varigit/linux-imx/blob/lf-6.1.y_var03/arch/arm64/boot/dts/freescale/imx8mp-var-da..."

Upon removing the &eqos and &fec blocks from the device tree, the warning message disappeared. Not sure why this seems to have prevented it from booting.

Hopefully this helps.

Re: Yocto iMX8M Plus boot kernel loop with "eth_lpi not found"Sorry to pull up an old thread, but did you get a resolution to this? We're in exactly the same situation with exactly the same error messages. We are in touch with Variscite but if you have a quick solution, or even just a pointer, we might get there quicker.Re: Yocto iMX8M Plus boot kernel loop with "eth_lpi not found"

Hi @cygnus.

If you are a Variscite customer, please register and create a ticket in the Variscite customer portal, and provide more details about the carrier board you are using: https://varisciteportal.axosoft.com/


Thanks,
Eran

Re: Yocto iMX8M Plus boot kernel loop with "eth_lpi not found"

Hello,

It could be problem with the connection, but maybe some @variscite could help.

regards

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 03:03 PM
更新者: