1988909_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1988909_en-US

1988909_en-US

imx93 DSI send command fail in some case

HI experts:


   I got a problem when intergrade a mipi panel to imx93 board ,  the log is:

   "dw-mipi-dsi-imx 4ae10000.dsi:failed to write command FIFo"

    and the function "mipi_dsi_device_transfer" return with error=-110.

   After more research,  and found that not all commands fail, but some command with too much parameters will fail, for example: the driver send the following commands:

jiangyaqiang_0-1730901400423.png

it will fail at command : 0xB4 , 0xD3, 0xD5 , 0xD6.

  If I don't send the commands failed, the panel can show picture , but the picture position is   offset,  and I have confirmed the board is ok wit DSI TO HDMI,  and the panel is ok with imx8mini.


    Dose anyone has any suggestion ?

    Best Regards .



LinuxRe: imx93 DSI send command fail in some case

Hi Zhiming:


Thanks.

And finally I found that add more timeout or don't send command in LPM will fix the problem.

Re: imx93 DSI send command fail in some case

Hello,

The DSI controller in i.MX93 is different from i.MX8MM. 

Please refer Table 526. Error Cause and Recover  in i.MX93 RM. For pld_w_err, the controller can send such long packet at one time.

Zhiming_Liu_1-1730944309000.png

Please check with your panel vendor to see if you can split these long cmd lists.


Best Regards

Zhiming

标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 03:20 PM
更新人: