1988746_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1988746_en-US

1988746_en-US

LS1046ARDB run rngtest very slowly on SDK scarthgap 5.0-lf-6.6.36

Hello,

I run 'rngtest -c 100 < /dev/hwrng' command on LS1046ARDB. But it takes about 7 minutes to complete it on the latest SDK. TinyLinux needs less than 1 second. What makes rngtest run so slowly on scarthgap SDK? Thanks.

On SDK (nxp-qoriq/yocto-sdk scarthgap YP 5.0-lf-6.6.36):

root@nxp-ls1046:~# rngd
root@nxp-ls1046:~# time rngtest -c 100 < /dev/hwrng
rngtest 6.16
Copyright (c) 2004 by Henrique de Moraes Holschuh
This is free software; see the source for copying conditions. There is NO warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

rngtest: starting FIPS tests...
rngtest: bits received from input: 2000032
rngtest: FIPS 140-2 successes: 100
rngtest: FIPS 140-2 failures: 0
rngtest: FIPS 140-2(2001-10-10) Monobit: 0
rngtest: FIPS 140-2(2001-10-10) Poker: 0
rngtest: FIPS 140-2(2001-10-10) Runs: 0
rngtest: FIPS 140-2(2001-10-10) Long run: 0
rngtest: FIPS 140-2(2001-10-10) Continuous run: 0
rngtest: input channel speed: (min=4.624; avg=4.674; max=4.683)Kibits/s
rngtest: FIPS tests speed: (min=29.031; avg=30.180; max=30.714)Mibits/s
rngtest: Program run time: 417908659 microseconds

real 6m57.930s
user 0m0.091s
sys 0m0.252s

U-boot information:

U-Boot 2019.10-g3cd9bc3993 (Apr 09 2020 - 05:25:58 +0800)

SoC: LS1046AE Rev1.0 (0x87070010)
Clock Configuration:
CPU0(A72):1800 MHz CPU1(A72):1800 MHz CPU2(A72):1800 MHz
CPU3(A72):1800 MHz
Bus: 600 MHz DDR: 2100 MT/s FMAN: 700 MHz
Reset Configuration Word (RCW):
00000000: 0c150012 0e000000 00000000 00000000
00000010: 11335559 40005012 60040000 c1000000
00000020: 00000000 00000000 00000000 00238800
00000030: 20124000 00003101 00000096 00000001
Model: LS1046A RDB Board
Board: LS1046ARDB, boot from SD
CPLD: V2.3
PCBA: V2.0
SERDES Reference Clocks:
SD1_CLK1 = 156.25MHZ, SD1_CLK2 = 100.00MHZ
DRAM: 7.9 GiB (DDR4, 64-bit, CL=15, ECC on)
DDR Chip-Select Interleaving Mode: CS0+CS1
SEC0: RNG instantiated
Using SERDES1 Protocol: 4403 (0x1133)
Using SERDES2 Protocol: 21849 (0x5559)
NAND: 512 MiB
MMC: FSL_SDHC: 0
Loading Environment from MMC... *** Warning - bad CRC, using default environment

EEPROM: NXID v1
In: serial
Out: serial
Err: serial
Net:
MMC read: dev # 0, block # 18432, count 128 ...
Fman1: Uploading microcode version 106.4.18
PCIe0: pcie@3400000 Root Complex: no link
PCIe1: pcie@3500000 Root Complex: no link
PCIe2: pcie@3600000 Root Complex: no link
FM1@DTSEC3 [PRIME], FM1@DTSEC4, FM1@DTSEC5, FM1@DTSEC6, FM1@TGEC1, FM1@TGEC2
Hit any key to stop autoboot: 0

On TinyLinux:

NXP LSDK tiny 2004 (based on Yocto)
TinyLinux login: root
root@TinyLinux:~# uname -a
Linux TinyLinux 5.4.3 #1 SMP PREEMPT Thu Apr 9 00:50:08 CST 2020 aarch64 aarch64 aarch64 GNU/Linux
root@TinyLinux:~# rngd

Initializing available sources

Initializing entropy source hwrng

Initializing AES buffer

Enabling JITTER rng support

Initializing entropy source jitter

root@TinyLinux:~# time rngtest -c 100 < /dev/hwrng
rngtest 6.7
Copyright (c) 2004 by Henrique de Moraes Holschuh
This is free software; see the source for copying conditions. There is NO warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

rngtest: starting FIPS tests...
rngtest: bits received from input: 2000032
rngtest: FIPS 140-2 successes: 100
rngtest: FIPS 140-2 failures: 0
rngtest: FIPS 140-2(2001-10-10) Monobit: 0
rngtest: FIPS 140-2(2001-10-10) Poker: 0
rngtest: FIPS 140-2(2001-10-10) Runs: 0
rngtest: FIPS 140-2(2001-10-10) Long run: 0
rngtest: FIPS 140-2(2001-10-10) Continuous run: 0
rngtest: input channel speed: (min=733.596; avg=1695.421; max=2384.186)Mibits/s
rngtest: FIPS tests speed: (min=28.215; avg=66.016; max=83.290)Mibits/s
rngtest: Program run time: 30115 microseconds

real 0m0.032s
user 0m0.032s
sys 0m0.000s

Would you please check it on your environment?

Thanks, MinWang@WindRiver

Re: LS1046ARDB run rngtest very slowly on SDK scarthgap 5.0-lf-6.6.36

This behavior  is expected.
Previously CAAM RNG was configured to run as a PRNG (Pseudo RNG). Currently it’s been fixed to run as a TRNG (True RNG), as required by the Linux kernel hwrng framework (which covers /dev/hwrng).

Re: LS1046ARDB run rngtest very slowly on SDK scarthgap 5.0-lf-6.6.36

Thanks. Can you give me the explanation why 7-minute is reasonable? I need it to convince our test team.  I used 'strace' command on testing and found it took about 4.2s for each read(0,xxx). See below log.

root@ls1046ardb:~# strace -tt -T -v -f rngtest -c 100 < /dev/hwrng
12:56:20.227293 execve("/usr/bin/rngtest", ["rngtest", "-c", "100"], ["SHELL=/bin/sh", "EDITOR=vi", "PWD=/home/root", "LOGNAME=root", "MOTD_SHOWN=pam", "HOME=/home/root", "TERM=vt102", "USER=root", "SHLVL=1", "PS1=\\u@\\h:\\w\\$ ", "HUSHLOGIN=FALSE", "PATH=/usr/local/bin:/usr/bin:/bi"..., "MAIL=/var/spool/mail/root", "_=/usr/bin/strace"]) = 0 <0.003006>
12:56:20.230603 brk(NULL) = 0xaaaad9703000 <0.000020>
12:56:20.230749 mmap(NULL, 8192, PROT_READ|PROT_WRITE, MAP_PRIVATE|MAP_ANONYMOUS, -1, 0) = 0xffff80df3000 <0.000026>
12:56:20.230878 faccessat(AT_FDCWD, "/etc/ld.so.preload", R_OK) = -1 ENOENT (No such file or directory) <0.000024>
12:56:20.230988 openat(AT_FDCWD, "/etc/ld.so.cache", O_RDONLY|O_CLOEXEC) = 3 <0.001364>
12:56:20.232419 fstat(3, {st_dev=makedev(0, 0x15), st_ino=16944659, st_mode=S_IFREG|0644, st_nlink=1, st_uid=0, st_gid=0, st_blksize=4096, st_blocks=80, st_size=37959, st_atime=1731896998 /* 2024-11-18T02:29:58.472686587+0000 */, st_atime_nsec=472686587, st_mtime=1520598896 /* 2018-03-09T12:34:56+0000 */, st_mtime_nsec=0, st_ctime=1730452190 /* 2024-11-01T09:09:50.401803864+0000 */, st_ctime_nsec=401803864}) = 0 <0.000021>
12:56:20.232682 mmap(NULL, 37959, PROT_READ, MAP_PRIVATE, 3, 0) = 0xffff80de9000 <0.000022>
12:56:20.232750 close(3) = 0 <0.000025>
12:56:20.232827 openat(AT_FDCWD, "/lib/libc.so.6", O_RDONLY|O_CLOEXEC) = 3 <0.007364>
12:56:20.240253 read(3, "\177ELF\2\1\1\3\0\0\0\0\0\0\0\0\3\0\267\0\1\0\0\0\0\207\2\0\0\0\0\0"..., 832) = 832 <0.000020>
12:56:20.240332 fstat(3, {st_dev=makedev(0, 0x15), st_ino=17986030, st_mode=S_IFREG|0755, st_nlink=1, st_uid=0, st_gid=0, st_blksize=4096, st_blocks=3232, st_size=1650968, st_atime=1731896998 /* 2024-11-18T02:29:58.479686587+0000 */, st_atime_nsec=479686587, st_mtime=1520598896 /* 2018-03-09T12:34:56+0000 */, st_mtime_nsec=0, st_ctime=1730452190 /* 2024-11-01T09:09:50.650803849+0000 */, st_ctime_nsec=650803849}) = 0 <0.000018>
12:56:20.240439 mmap(NULL, 1826688, PROT_NONE, MAP_PRIVATE|MAP_ANONYMOUS|MAP_DENYWRITE, -1, 0) = 0xffff80bfc000 <0.000022>
12:56:20.240506 mmap(0xffff80c00000, 1761152, PROT_READ|PROT_EXEC, MAP_PRIVATE|MAP_FIXED|MAP_DENYWRITE, 3, 0) = 0xffff80c00000 <0.000039>
12:56:20.240589 munmap(0xffff80bfc000, 16384) = 0 <0.000018>
12:56:20.240648 munmap(0xffff80dae000, 49024) = 0 <0.000016>
12:56:20.240705 mprotect(0xffff80d8b000, 73728, PROT_NONE) = 0 <0.000024>
12:56:20.240771 mmap(0xffff80d9d000, 20480, PROT_READ|PROT_WRITE, MAP_PRIVATE|MAP_FIXED|MAP_DENYWRITE, 3, 0x18d000) = 0xffff80d9d000 <0.000023>
12:56:20.240853 mmap(0xffff80da2000, 49024, PROT_READ|PROT_WRITE, MAP_PRIVATE|MAP_FIXED|MAP_ANONYMOUS, -1, 0) = 0xffff80da2000 <0.000024>
12:56:20.240944 close(3) = 0 <0.000015>
12:56:20.241028 set_tid_address(0xffff80df3ef0) = 1095 <0.000014>
12:56:20.241082 set_robust_list(0xffff80df3f00, 24) = 0 <0.000013>
12:56:20.241135 rseq(0xffff80df4540, 0x20, 0, 0xd428bc00) = 0 <0.000013>
12:56:20.241276 mprotect(0xffff80d9d000, 12288, PROT_READ) = 0 <0.000027>
12:56:20.241373 mprotect(0xaaaad712f000, 4096, PROT_READ) = 0 <0.000020>
12:56:20.241440 mprotect(0xffff80df8000, 8192, PROT_READ) = 0 <0.000022>
12:56:20.241533 prlimit64(0, RLIMIT_STACK, NULL, {rlim_cur=8192*1024, rlim_max=RLIM64_INFINITY}) = 0 <0.000015>
12:56:20.241642 munmap(0xffff80de9000, 37959) = 0 <0.000039>
12:56:20.241749 getrandom("\xb6\x24\x3c\x6e\x52\x70\x6a\x7c", 8, GRND_NONBLOCK) = 8 <0.000016>
12:56:20.241816 brk(NULL) = 0xaaaad9703000 <0.000014>
12:56:20.241870 brk(0xaaaad9724000) = 0xaaaad9724000 <0.000017>
12:56:20.241980 write(2, "rngtest 6.16\nCopyright (c) 2004 "..., 128rngtest 6.16
Copyright (c) 2004 by Henrique de Moraes Holschuh
This is free software; see the source for copying conditions. Th) = 128 <0.000024>
12:56:20.242052 write(2, "ere is NO warranty; not even for"..., 87ere is NO warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

) = 87 <0.000020>
12:56:20.242119 rt_sigaction(SIGTERM, {sa_handler=0xaaaad7111940, sa_mask=[], sa_flags=0}, NULL, = 0 <0.000015>
12:56:20.242187 rt_sigaction(SIGINT, {sa_handler=0xaaaad7111940, sa_mask=[], sa_flags=0}, NULL, = 0 <0.000014>
12:56:20.242255 write(2, "rngtest: starting FIPS tests...\n", 32rngtest: starting FIPS tests...
) = 32 <0.000067>
12:56:20.575329 read(0, "1`\305m", 4) = 4 <0.000058>
12:56:20.575493 read(0, "\0060;{sV\27\25\314\350=\322\16\300x\276q~r=\366\214?c\376,Z8\376\nP\24"..., 2500) = 2500 <4.171011>
12:56:24.747346 read(0, "q\327\205c\200\264q\363\331\236\234\334\261\360\242\261R3\3\10_\4/l?\237-xO\230\224<"..., 2500) = 2500 <4.170192>
12:56:28.918362 read(0, "\177\314\354\326\343\371z9\34\255n\7G\30\302\311\336`\t6Mi\340\17\316\346\221F\360j\21\10"..., 2500) = 2500 <4.170233>
12:56:33.089414 read(0, "\204~*\254X\214A\337\204\320\353\313Y\27\24D\323\226\34Q\365@\303\374O\32\326\321\253\242gV"..., 2500) = 2500 <4.196976>
12:56:37.287244 read(0, "\34\300\3308\32\235]\7%\363\16d\t)\234\253\204\361\34\206\247TV\341\254\201\261D\315\251F\234"..., 2500) = 2500 <4.170207>
12:56:41.458283 read(0, "\336\r\"M\235\10\262@\341\326\354J\256\321\\\224U\244\211\322TQ\263\232\363\233J:\314\n\316\256"..., 2500) = 2500 <4.170230>
12:56:45.629342 read(0, "\32`\222\205o\377\235\253\0~~\373:\274\311F\2636I\334!\352\267\306\345\220\234\360\341\375\23\226"..., 2500) = 2500 <4.170225>
12:56:49.800395 read(0, "\377\37\242\376\323\333\245\325\27\333\366\22\17M\342\233\234\265;0\257[\25\237VFk$\3535\326<"..., 2500) = 2500 <4.196967>
12:56:53.998191 read(0, "\270\221\335\236S\211Y]\273\363\367X\2w\341\33\226E\336g\316\315\313\220L\261\333\27\272\322Z\300"..., 2500) = 2500 <4.170222>
12:56:58.169226 read(0, "k\316/$o\2605~9\346\0\251\4\362\241l\37x\330!\270v\2\37\fV\255Z\324m\241}"..., 2500) = 2500 <4.170255>
12:57:02.340313 read(0, "\322\334c\326\242\236\317\363\250L\347\306(A\321\235}\333/)e\2\203\0006\247YD\37\324\246+"..., 2500) = 2500 <4.170247>
12:57:06.511398 read(0, "\212Z)X\233\253\37\360\24444\5\345R\354\354%d\266d]L\376\204\177\347\366i\34R\336\f"..., 2500) = 2500 <4.196931>
12:57:10.709180 read(0, "\263\265\335OE\202\302\331\305t\10\271/\16}ct\22\33)E\360\330\307\242pw\212\334/\202\234"..., 2500) = 2500 <4.196932>
12:57:14.906976 read(0, "?\230\363\227\315\372\24\214\212\375\311\221\246x84\336\2733\17\314\0P\27\311\341S'~*\225\241"..., 2500) = 2500 <4.170207>
12:57:19.078037 read(0, "\342\271\"\300\342)\\@\336w\37O\304!\376\371\4C\f\330T\0105\376\35\177\301\376\10\260\257c"..., 2500) = 2500 <4.170192>
12:57:23.249077 read(0, "Y\36#\262N\225\363\22\324\354\363\315\32\36\236U6W\241\242+3*C\0\262R\210\351\345g\273"..., 2500) = 2500 <4.196950>
12:57:27.446882 read(0, "~G\245Ot\306\303d\212\364\20,\257/h\300
12:57:31.617919 read(0, "\35\26\202\360)\302\0\267\0351\270\352\263q_J'e=G\233#\375\341t\216\363\350\241\327\313\277"..., 2500) = 2500 <4.170225>
12:57:35.788977 read(0, "\201}\36\232\251(\327\364\266s\332\306\242\311\177iu\305\323\356\0\222]c\247\335\2217\320F\330C"..., 2500) = 2500 <4.170224>
12:57:39.960039 read(0, "\f\31l\220J\255\316k0I\230-\371\224\214!$m\257\363\7\274\213^\353\334vM\30\340\273\261"..., 2500) = 2500 <4.196953>
12:57:44.157822 read(0, "\v\276\311\313\226I\320\304\3\25\371k\216V\24\34}i7_\tc\266\330C\26\301\232+q\21\337"..., 2500) = 2500 <4.170229>
12:57:48.328868 read(0, "\327$\235\200\246\322\210\366\246\342\351\331\325\202x\333\16T\377)\317\237\362D[\336\\\3\34\354W\2"..., 2500) = 2500 <4.170241>
12:57:52.499941 read(0, "I\305a#\202\370\2776p\213V\361{z\24\275\201\7[\26\203\307c\35\370C?%\307\1i_"..., 2500) = 2500 <4.170219>
12:57:56.671006 read(0, "Y&sp\320\227\340[\243\311\270i\330\211\f\273\16\245\236u\257\344u*\346\251\226\360_\262m\215"..., 2500) = 2500 <4.196958>
12:58:00.868809 read(0, "\265\330\354\16\321\344W$\251\311\300\375-\17\335\221C,\"\376\366\254\302M\304:\37\365\213\213\223h"..., 2500) = 2500 <4.170206>
12:58:05.039857 read(0, "\275\201AIwz\241+\35\255\2424\320\364\330\334\0o\353\261\27U\f\34oGMm\330Q\f\236"..., 2500) = 2500 <4.170209>
12:58:09.210927 read(0, "\35\27\323\252\274\252XL\360K\35\234O\245\367)\217!P\336\267\323v\375\376\227\300\360(\"~\""..., 2500) = 2500 <4.170202>
12:58:13.381960 read(0, "\277m\335?\330\307i\347\217>\6l\16M\316q\302\245\310\3\265Hq\7\210\327\241\272D\253T\226"..., 2500) = 2500 <4.223692>
12:58:17.606489 read(0, "M+\23\216\216B\355\367\372\24x\373}Cf\253\203\302\227 \2035\272\27\200z\217\245#\177\277!"..., 2500) = 2500 <4.170225>
12:58:21.777545 read(0, "\225&SZCo\205\22:73\263\215v\201L=\226\362\357\317\17!\33l\243\fC3\235\306\334"..., 2500) = 2500 <4.170215>
12:58:25.948581 read(0, "6bH\354r\215\324\203b5\204z#\217\2616\364\271\317D\252>\0\330\244\300\317\24\360\340\323\206"..., 2500) = 2500 <4.170242>
12:58:30.119648 read(0, "\376\302\304\35[\224\5\307I,L\311\03505A\207\252\356=\237\3555R\266\177v\374\17\215\363\262"..., 2500) = 2500 <4.196964>
12:58:34.317432 read(0, ".\265\316[O\26\266\27\375n\267\35?\231\300\366\206\234\340\224\337z\234s@rp\276\366\353\214\247"..., 2500) = 2500 <4.170241>
12:58:38.488491 read(0, "&~-]\10\373@BjIko*\"g\242f\256\347K\310e\326\227\271C\302\233\250E\ve"..., 2500) = 2500 <4.170236>
12:58:42.659544 read(0, "\201?\305\20\265&\333\240\34\211+\231\323\r\367\362\35o\251\351)\246\332q\223\354\301\3674\"\361\\"..., 2500) = 2500 <4.170245>
12:58:46.830647 read(0, "\0<\220O\302\350\342\354b\3100Oy\203\254\224'\209h\354\342\224\2720l\333\317\257\210\322\265"..., 2500) = 2500 <4.196935>
12:58:51.028399 read(0, "\227\352\226\\\314\0040\363\v\204\322\370{5\305D\203\326\240\35t\277\37\372\24\310\237Q_\232\261\254"..., 2500) = 2500 <4.170236>
12:58:55.199458 read(0, "\361\302H\203;@\364\36[\233\177e:\374\357{u?<\3074\34+\2110O\252\0\311\230.f"..., 2500) = 2500 <4.170232>
12:58:59.370500 read(0, "\201\320\324\225\352v\324p63\220\234\236\21\321\210Q\275C\362\224\250\323\263\36\347\35\214q$\204\7"..., 2500) = 2500 <4.170259>
12:59:03.541590 read(0, "G' )R\34\217H\0\317\277B\226c\212\vTTZ\302\3576\2767Y\251\317\2659H\375G"..., 2500) = 2500 <4.196897>
12:59:07.739333 read(0, "\255\274~\352\207\264xl!\17\336`p@fX\265\1\25&4\26\22\304\264\214\264\377\35\311\237\7"..., 2500) = 2500 <4.170284>
12:59:11.910471 read(0, "\237\324\360:7\307\261\235\376\17\24\365V\351\331\243\25\252nE\227fm\244\213\203\204%\211#\221\356"..., 2500) = 2500 <4.170190>
12:59:16.081501 read(0, "vc\331m\24MOX\301\32h\2629\336\315\3070\333Xt\265Z^\305\3701_\325\320\276\23\376"..., 2500) = 2500 <4.196967>
12:59:20.279350 read(0, "j\356\3214\220\221\n\232\242\260b\267vB3\253\31\206K\327\373\262\351\364\242@\225\207_\265\362M"..., 2500) = 2500 <4.196903>
12:59:24.477095 read(0, "\202\246\0\263\267\r\322\205t\5\330\2[10\1?\371\236\314\3\236\0175\272\260\320\325\311\267\35o"..., 2500) = 2500 <4.170204>
12:59:28.648131 read(0, "\254\323Y\301>`z\367NF\320\3752\231\244ZA))\34'o~H\224{\314e\374y:\316"..., 2500) = 2500 <4.170229>
12:59:32.819202 read(0, ";\365X\352U\355\27\31\v\25k2\1\36t\n4\314\262\235-\334\22N\323\300\345Q>-{e"..., 2500) = 2500 <4.170214>
12:59:36.990241 read(0, "K\v\301\254\301\216^\237\305\373\357\206q\4XY\316/\240:\345\2t}\267\376W\354M\260\26\262"..., 2500) = 2500 <4.196970>
12:59:41.188043 read(0, "\24\331@\310\377\331QRE\211\214L]n\216\202>\277\0043\n >\316\335\230Z\31\345\340\271'"..., 2500) = 2500 <4.170219>
12:59:45.359115 read(0, "\254\2\244\2030\317'\1\326\251\374\333.m&9'']\n\210\206a\207\335\357\n\310^w#z"..., 2500) = 2500 <4.170210>
12:59:49.530146 read(0, "1\222\336H\34\272$\236Tl\372\267\366i\375\365\347-\341\365\364\"\326\321s\373i,\302fS\225"..., 2500) = 2500 <4.170232>
12:59:53.701201 read(0, "\305\3053\204\311\217\2476\307\21\352\235\364\333\260&\230\315\212P\30c\260hQ\1\262\203(\266%\372"..., 2500) = 2500 <4.196972>
12:59:57.899020 read(0, "\341\317/\302\276\245\254\216\271\260Af\272\253\334l\362\303\231\2357S\375\316\2347\1P\7;\254\241"..., 2500) = 2500 <4.170220>
13:00:02.070082 read(0, "(\326\325s\234\315]\257\357\34\36\307\344\357;\352\205\353=\241\tG\313\335Z\323\4\6\343\271W\16"..., 2500) = 2500 <4.170206>
13:00:06.241124 read(0, ".\205\332\244\321\265H\331\20\3313\32O\340\334/\330\240\253\243\343\214F\\rh\17\201}E\30\244"..., 2500) = 2500 <4.170217>
13:00:10.412190 read(0, "\366\224\325X\212\340#[Y\5\372\341\303\5\377\366\220i~m>\306AQD\20>\305\361\250+\221"..., 2500) = 2500 <4.196959>
13:00:14.610001 read(0, "\26\312\32\203\336\305M_\353\33\316gDg@k\262\274)\350\300\318Y\342\322\r\35\311*\332'"..., 2500) = 2500 <4.196911>
13:00:18.807742 read(0, "\303\21h\2470\263\0307y\263&\267\227\250\342\302R\\\16\341\263\272\332|\233!\263\\\310\247\367&"..., 2500) = 2500 <4.170256>
13:00:22.978857 read(0, "\21k5\344\223\22Jfcy^\304e\273E\205A\23\230\364w\262\7\242\351\310\224lM)\222\202"..., 2500) = 2500 <4.170192>
13:00:27.149872 read(0, "~\220TQ\3\303\351\24'\16\224\22\245<\366ZM\347\210\260\"\334?^\2\30\3628\32B\2\177"..., 2500) = 2500 <4.196981>
13:00:31.347685 read(0, "\334nj]\307\177\177\r\3322\322\35o<\301\216\204\227\212(\202--\321\222\316\257\216@?a\226"..., 2500) = 2500 <4.170222>
13:00:35.518769 read(0, "\7EW\347O\230 \3451\320d2\315\246Us8\271\205\334\277Z\371sQ\365\376\341@\235\331\372"..., 2500) = 2500 <4.170197>
13:00:39.689791 read(0, "T\24\316\267\35\6\367=\33I\f\204\2565\311\354\35\240c\234 \21\334\321\243\332\33:\275\307\210T"..., 2500) = 2500 <4.170230>
13:00:43.860842 read(0, "\2252\312\345\226\v\315f\10}\250~\255q\324\267\344?\7\4\255|$G\330\203Xm\321\264\314\361"..., 2500) = 2500 <4.196974>
13:00:48.058653 read(0, "X\4\366\227l\232/\34\203\272\343\374EB\354Q\202\345\2470\337rI\37.M\26\232\37\216]\266"..., 2500) = 2500 <4.170220>
13:00:52.229708 read(0, "\306\264\337b\373\10\373~\203\\\257\225\344^\253,\\\30~\314<\36\235\275\3\337H\220;X\7\304"..., 2500) = 2500 <4.170222>
13:00:56.400761 read(0, "X\241\5\351\374\35\2554\311\352\262(!\337<\240\"\7[\346Te\3531m4>YQ\277:Z"..., 2500) = 2500 <4.170223>
13:01:00.571814 read(0, "\244r;X\203if@+\274\324\371i\342\272\10\"\233\273\30W\\\4\356m\315`\350\367[\211:"..., 2500) = 2500 <4.196972>
13:01:04.769613 read(0, "m\2331\336?\2465\250RV\202R\365l{^:\"\177\314\273\223_]q|w\350\257\274U\227"..., 2500) = 2500 <4.170217>
13:01:08.940665 read(0, "\344\233\350\263u2Z\240b\230\221\262h\246\246ux\255\26n\235\10\313T$\351T\351\3179VK"..., 2500) = 2500 <4.170225>
13:01:13.111716 read(0, "\377\266\354\t\203\257\340iX\3208\355\224\21\305\22\201w\270\224\25(c\253\237k\222\231\327\206\16\213"..., 2500) = 2500 <4.170238>
13:01:17.282834 read(0, "qx\232o\346\16!\3358\27\2028\264\357\302\372\4^\204tAY\304\231\23\344;.z+\362\201"..., 2500) = 2500 <4.223633>
13:01:21.507346 read(0, "\33s\245Im\226/\303H\241O\343\32\rwOZ/\312\242v\301\31\30\241\376\222\244r\315l\345"..., 2500) = 2500 <4.170186>
13:01:25.678347 read(0, "(\365S\263nL\363\265M\3408\27i\333W\345\224\353x\373yH\376\366\253\301\206\363\353\22\210g"..., 2500) = 2500 <4.170238>
13:01:29.849411 read(0, "3\343\3\351?\352\3753\324\250y\33\21f5\345@-PGg\331\305\305c\277\362\374cEn\t"..., 2500) = 2500 <4.170233>
13:01:34.020465 read(0, "}\210Z\36J\347\341\354\6J\217(\335\254\342J\21\231\205\266\340\274\332\365\211\1m\27\241\26\32\316"..., 2500) = 2500 <4.196971>
13:01:38.218261 read(0, "\274:_\17\17?\246\244c\5\2214\21G\v\370\335\22\2544\3\324r\3362kW\210\316\301U1"..., 2500) = 2500 <4.170234>
13:01:42.389321 read(0, "\233\203\242@\2\352\301\371\253P\224r\322\24\206\214&@\207\223\344\232:\342\336Sf\"*\16\254\342"..., 2500) = 2500 <4.170226>
13:01:46.560373 read(0, "v\302\235r\24?}\261\253\2525\252\266T\37\317\254\302\200\301\tk\330\3\356R\270\226\276;\252h"..., 2500) = 2500 <4.170239>
13:01:50.731439 read(0, "\235;u\21\232X.Z\247\365\264\362j5K~\327\244\247\357Ab+\232\362w\264\16\210\3056!"..., 2500) = 2500 <4.196961>
13:01:54.929226 read(0, "H\334v\n\254_\366Q\277UhX\177\374Bx\203\202\177o[\344\317,U\327\ru\221\27\363\304"..., 2500) = 2500 <4.170234>
13:01:59.100278 read(0, "y\332\16\247w6\300\264\236\243\340,\262\2A\257S\205\3404\366\372\n\354\347\16z+Z,'\7"..., 2500) = 2500 <4.170272>
13:02:03.271393 read(0, "z\223W\2721\227\241S\204kM\373D6\30C\245\216\302\314!,\334\356<\226\343\263 !\3k"..., 2500) = 2500 <4.170181>
13:02:07.442428 read(0, "!\3\212\267K\352\251\275W|\340\350\10\265\240\356\275vY\332\1\314\223b\34\240\231\246\202\204\207U"..., 2500) = 2500 <4.196931>
13:02:11.640192 read(0, "\2364\347\226f\350}\0$\223:\31\222s\335\245\4\330\377\353x\205\344vn\3237\233\320Td6"..., 2500) = 2500 <4.170240>
13:02:15.811314 read(0, "\22C#\225\332a\222\343\37U\321\234P\241\3128\341\204\245)\354\vzu1.\356\2020=\2426"..., 2500) = 2500 <4.170161>
13:02:19.982299 read(0, "\7f\204s\365o\363\371]\222\16f\331\25t\372\312x\2\263\252A:\6\322\322\205\350\261h\n\360"..., 2500) = 2500 <4.196990>
13:02:24.180128 read(0, "./Gzs\245?\30\271q\\\223g\323\377&m\244I\275\223\t\222Q\n\364[8\306H\323\357"..., 2500) = 2500 <4.196945>
13:02:28.377896 read(0, "\32\363\322\264\272\242\215\372\0237\342\246\276\364\237\247-c\265\3\321:\241\324Q\244_nR\352\ni"..., 2500) = 2500 <4.170240>
13:02:32.548968 read(0, "\330\307:\213\tDh\262\347%<\252d\337\355L\264dLi}\375\372P^m\373\364\247-:\233"..., 2500) = 2500 <4.170222>
13:02:36.720012 read(0, "\332t\364\277\347\372\351\370\376\"\254\257\361\275\356h\225$\324\275\342^\313\32\311M#\361T\221\301$"..., 2500) = 2500 <4.170234>
13:02:40.891104 read(0, "\262\220<\323\341\21rY\33\327\3353p\247RI\206\31O_X\342\351\232\3\32\303\350\252\251\354\355"..., 2500) = 2500 <4.196938>
13:02:45.088873 read(0, "\257\30\317\36\274\351QE%\6\211\363\23\256\354\376m\252\223?Q!\353-N?}V#\360\26["..., 2500) = 2500 <4.170223>
13:02:49.259925 read(0, "/\264\300\203g\3\2P\2W\272\324\246{\3a\220\2\333~\23\244\313~\374\rL\354aF\331I"..., 2500) = 2500 <4.170235>
13:02:53.431018 read(0, "\241v\211\303\256\224\252\32S\23\t}lM\234\255\10\233\334\221\330\33\275\265\356B\362\25k)\331\\"..., 2500) = 2500 <4.170188>
13:02:57.602035 read(0, "\311\234\5\215\17]\203\0\315m(\374\352\273\243\v\25\314\203\374\214z\232\226\216\2025*\217,\317!"..., 2500) = 2500 <4.196977>
13:03:01.799851 read(0, "\242i\27h\32\351\215\206\337\243j\247xwZ\211\30G\320\242d_\252\203t\343\255@\203\333\1\260"..., 2500) = 2500 <4.170212>
13:03:05.970927 read(0, ",\24\224=\ts70\255\26y\330Z\307<\10\231>\27\221\221\234X\23=\2172%\217H}\326"..., 2500) = 2500 <4.170191>
13:03:10.141947 read(0, "\256\307\367T\2302\362\31\274\322d\373\\S`t\341\263\271\211{A1&U\37\24os\\\271\206"..., 2500) = 2500 <4.170228>
13:03:14.312999 read(0, "<\232\362\314\240K\324C\377\322\315\252Q\177Z\201'W\222\307g\35\212?\277\343e.\244\2633\25"..., 2500) = 2500 <4.196972>
13:03:18.510843 write(2, "rngtest: bits received from inpu"..., 43rngtest: bits received from input: 2000032
) = 43 <0.000068>
13:03:18.511079 write(2, "rngtest: FIPS 140-2 successes: 1"..., 35rngtest: FIPS 140-2 successes: 100
) = 35 <0.000063>
13:03:18.511288 write(2, "rngtest: FIPS 140-2 failures: 0\n", 32rngtest: FIPS 140-2 failures: 0
) = 32 <0.000065>
13:03:18.511485 write(2, "rngtest: FIPS 140-2(2001-10-10) "..., 43rngtest: FIPS 140-2(2001-10-10) Monobit: 0
) = 43 <0.000048>
13:03:18.511658 write(2, "rngtest: FIPS 140-2(2001-10-10) "..., 41rngtest: FIPS 140-2(2001-10-10) Poker: 0
) = 41 <0.000046>
13:03:18.511827 write(2, "rngtest: FIPS 140-2(2001-10-10) "..., 40rngtest: FIPS 140-2(2001-10-10) Runs: 0
) = 40 <0.000046>
13:03:18.511995 write(2, "rngtest: FIPS 140-2(2001-10-10) "..., 44rngtest: FIPS 140-2(2001-10-10) Long run: 0
) = 44 <0.000046>
13:03:18.512164 write(2, "rngtest: FIPS 140-2(2001-10-10) "..., 50rngtest: FIPS 140-2(2001-10-10) Continuous run: 0
) = 50 <0.000046>
13:03:18.512342 write(2, "rngtest: input channel speed: (m"..., 72rngtest: input channel speed: (min=4.624; avg=4.674; max=4.683)Kibits/s
) = 72 <0.000049>
13:03:18.512524 write(2, "rngtest: FIPS tests speed: (min="..., 72rngtest: FIPS tests speed: (min=28.856; avg=30.231; max=30.863)Mibits/s
) = 72 <0.000048>
13:03:18.512694 write(2, "rngtest: Program run time: 41827"..., 50rngtest: Program run time: 418270423 microseconds
) = 50 <0.000049>
13:03:18.512907 exit_group(0) = ?
13:03:18.513303 +++ exited with 0 +++


Re: LS1046ARDB run rngtest very slowly on SDK scarthgap 5.0-lf-6.6.36

Yes, I believe 7-minute result is reasonable. 

Re: LS1046ARDB run rngtest very slowly on SDK scarthgap 5.0-lf-6.6.36

Thanks for your help. I want to know whether it is a bug or not. Or you think about 7-minute result is reasonable.

Re: LS1046ARDB run rngtest very slowly on SDK scarthgap 5.0-lf-6.6.36

I did replicate your test in the ls1046afrwy and the result is as expected:

Oswalag_0-1731601343361.png

The difference with tiny linux is faster due to the configuration, system service and daemons running on the SDK.

For tinyLinux its core system can run entirely in RAM, contributing to rapid boot times and efficient resource utilization.


Re: LS1046ARDB run rngtest very slowly on SDK scarthgap 5.0-lf-6.6.36

Hello,

Thanks for your help. My test step lists as below:

1. Power on LS1046ARDB and hit any key to stop autoboot when uboot runs.

2. Load image and dtb file by uboot.  The image and dtb are built by SDK scarthgap-6.6.36. Use NFS as rootfs.

=> setenv dir qoriq-6.6.36/ls1046;setenv imgfile $dir/Image;setenv fdtfile $dir/fsl-ls1046a-rdb-sdk.dtb;setenv serverip 128.224.34.139;setenv ipaddr 128.224.166.226;setenv gatewayip 128.224.166.1;setenv netmask 255.255.255.0;setenv fdt_high 0xffffffff
=> setenv nfsboot 'setenv bootargs root=/dev/nfs rw nfsroot=$serverip:/tftpboot/$dir/rootfs,v3,tcp ip=dhcp console=ttyS0,115200 earlycon=uart8250,mmio,0x21c0500;tftp 0x81000000 $imgfile;tftp 0x90000000 $fdtfile;booti 0x81000000 - 0x90000000'
=> run nfsboot

3. After system boots up, run test commands:

root@ls1046ardb:~# rngd
root@ls1046ardb:~# time rngtest -c 100 < /dev/hwrng

The entire logs list below as your reference: 

NOTICE: UDIMM 18ASF1G72AZ-2G6B1

NOTICE: 8 GB DDR4, 64-bit, CL=15, ECC on, CS0+CS1
NOTICE: BL2: v2.8(release):lf-6.6.3-1.0.0-0-g8dbe28631-dirty
NOTICE: BL2: Built : 17:57:56, Jan 22 2024
NOTICE: BL2: Booting BL31
NOTICE: BL31: v2.8(release):lf-6.6.3-1.0.0-0-g8dbe28631-dirty
NOTICE: BL31: Built : 17:57:56, Jan 22 2024
NOTICE: Welcome to ls1046ardb BL31 Phase


U-Boot 2023.04+fsl+gf8a2983ec83+p0 (Mar 04 2024 - 07:25:04 +0000)

SoC: LS1046AE Rev1.0 (0x87070010)
Clock Configuration:
CPU0(A72):1800 MHz CPU1(A72):1800 MHz CPU2(A72):1800 MHz
CPU3(A72):1800 MHz
Bus: 600 MHz DDR: 2100 MT/s FMAN: 700 MHz
Reset Configuration Word (RCW):
00000000: 0c150012 0e000000 00000000 00000000
00000010: 11335559 40005012 60040000 c1000000
00000020: 00000000 00000000 00000000 00238800
00000030: 20124000 00003101 00000096 00000001
Model: LS1046A RDB Board
Board: LS1046ARDB, boot from SD
CPLD: V2.3
PCBA: V2.0
SERDES Reference Clocks:
SD1_CLK1 = 156.25MHZ, SD1_CLK2 = 100.00MHZ
DRAM: 7.9 GiB (DDR4, 64-bit, CL=15, ECC on)
DDR Chip-Select Interleaving Mode: CS0+CS1
Using SERDES1 Protocol: 4403 (0x1133)
Using SERDES2 Protocol: 21849 (0x5559)
PCIe1: pcie@3400000 Root Complex: no link
PCIe2: pcie@3500000 Root Complex: no link
PCIe3: pcie@3600000 Root Complex: no link
Core: 58 devices, 19 uclasses, devicetree: separate
NAND: 512 MiB
MMC: FSL_SDHC: 0
Loading Environment from MMC... *** Warning - bad CRC, using default environment

EEPROM: NXID v1
In: serial
Out: serial
Err: serial
SEC0: RNG instantiated
Net:
MMC read: dev # 0, block # 18432, count 128 ...
Fman1: Uploading microcode version 106.4.18
eth0: fm1-mac3, eth1: fm1-mac4, eth2: fm1-mac5, eth3: fm1-mac6, eth4: fm1-mac9, eth5: fm1-mac10
Hit any key to stop autoboot: 0
=> setenv dir qoriq-6.6.36/ls1046;setenv imgfile $dir/Image;setenv fdtfile $dir/fsl-ls1046a-rdb-sdk.dtb;setenv serverip 128.224.34.139;setenv ipaddr 128.224.166.226;setenv gatewayip 128.224.166.1;setenv netmask 255.255.255.0;setenv fdt_high 0xffffffff
=> setenv nfsboot 'setenv bootargs root=/dev/nfs rw nfsroot=$serverip:/tftpboot/$dir/rootfs,v3,tcp ip=dhcp console=ttyS0,115200 earlycon=uart8250,mmio,0x21c0500;tftp 0x81000000 $imgfile;tftp 0x90000000 $fdtfile;booti 0x81000000 - 0x90000000'
=> run nfsboot
Using fm1-mac3 device
TFTP from server 128.224.34.139; our IP address is 128.224.166.226; sending through gateway 128.224.166.1
Filename 'qoriq-6.6.36/ls1046/Image'.
Load address: 0x81000000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
###################
886.7 KiB/s
done
Bytes transferred = 49889792 (2f94200 hex)
Using fm1-mac3 device
TFTP from server 128.224.34.139; our IP address is 128.224.166.226; sending through gateway 128.224.166.1
Filename 'qoriq-6.6.36/ls1046/fsl-ls1046a-rdb-sdk.dtb'.
Load address: 0x90000000
Loading: ###
778.3 KiB/s
done
Bytes transferred = 31894 (7c96 hex)
## Flattened Device Tree blob at 90000000
Booting using the fdt blob at 0x90000000
Working FDT set to 90000000
Loading Device Tree to 000000008ffe5000, end 000000008ffffc95 ... OK
Working FDT set to 8ffe5000
WARNING failed to get smmu node: FDT_ERR_NOTFOUND
WARNING failed to get smmu node: FDT_ERR_NOTFOUND

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd082]
[ 0.000000] Linux version 6.6.36-gd23d64eea511 (oe-user@oe-host) (aarch64-fsl-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240716) #1 SMP PREEMPT Wed Sep 4 08:22:45 UTC 2024
[ 0.000000] KASLR enabled
[ 0.000000] Machine model: LS1046A RDB Board
[ 0.000000] earlycon: uart8250 at MMIO 0x00000000021c0500 (options '')
[ 0.000000] printk: bootconsole [uart8250] enabled
[ 0.000000] efi: UEFI not found.
[ 0.000000] OF: reserved mem: initialized node bman-fbpr, compatible id fsl,bman-fbpr
[ 0.000000] OF: reserved mem: 0x00000009ff000000..0x00000009ffffffff (16384 KiB) nomap non-reusable bman-fbpr
[ 0.000000] OF: reserved mem: initialized node qman-fqd, compatible id fsl,qman-fqd
[ 0.000000] OF: reserved mem: 0x00000009fe800000..0x00000009feffffff (8192 KiB) nomap non-reusable qman-fqd
[ 0.000000] OF: reserved mem: initialized node qman-pfdr, compatible id fsl,qman-pfdr
[ 0.000000] OF: reserved mem: 0x00000009fc000000..0x00000009fdffffff (32768 KiB) nomap non-reusable qman-pfdr
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000080000000-0x00000009ffffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0x9fb8069c0-0x9fb808fff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal [mem 0x0000000100000000-0x00000009ffffffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x00000000fbdfffff]
[ 0.000000] node 0: [mem 0x0000000880000000-0x00000009fbffffff]
[ 0.000000] node 0: [mem 0x00000009fc000000-0x00000009fdffffff]
[ 0.000000] node 0: [mem 0x00000009fe000000-0x00000009fe7fffff]
[ 0.000000] node 0: [mem 0x00000009fe800000-0x00000009ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000009ffffffff]
[ 0.000000] On node 0, zone Normal: 16896 pages in unavailable ranges
[ 0.000000] cma: Reserved 32 MiB at 0x00000000f9e00000 on node -1
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 23 pages/cpu s54248 r8192 d31768 u94208
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] CPU features: detected: Spectre-v2
[ 0.000000] CPU features: detected: Spectre-v3a
[ 0.000000] CPU features: detected: Spectre-BHB
[ 0.000000] CPU features: kernel page table isolation forced ON by KASLR
[ 0.000000] CPU features: detected: Kernel page table isolation (KPTI)
[ 0.000000] CPU features: detected: ARM erratum 1742098
[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[ 0.000000] alternatives: applying boot alternatives
[ 0.000000] Kernel command line: root=/dev/nfs rw nfsroot=128.224.34.139:/tftpboot/qoriq-6.6.36/ls1046/rootfs,v3,tcp ip=dhcp console=ttyS0,115200 earlycon=uart8250,mmio,0x21c0500
[ 0.000000] Dentry cache hash table entries: 1048576 (order: 11, 8388608 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[ 0.000000] Fallback order for Node 0: 0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 2047488
[ 0.000000] Policy zone: Normal
[ 0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[ 0.000000] software IO TLB: area num 4.
[ 0.000000] software IO TLB: mapped [mem 0x00000000f5e00000-0x00000000f9e00000] (64MB)
[ 0.000000] Memory: 7954524K/8321024K available (22208K kernel code, 4496K rwdata, 12120K rodata, 9728K init, 1142K bss, 333732K reserved, 32768K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=16 to nr_cpu_ids=4.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GIC: Adjusting CPU interface base to 0x000000000142f000
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GIC: Using split EOI/Deactivate mode
[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[ 0.000000] arch_timer: cp15 timer(s) running at 25.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x5c40939b5, max_idle_ns: 440795202646 ns
[ 0.000000] sched_clock: 56 bits at 25MHz, resolution 40ns, wraps every 4398046511100ns
[ 0.008558] Console: colour dummy device 80x25
[ 0.013061] Calibrating delay loop (skipped), value calculated using timer frequency.. 50.00 BogoMIPS (lpj=100000)
[ 0.023482] pid_max: default: 32768 minimum: 301
[ 0.028157] LSM: initializing lsm=capability,integrity
[ 0.033378] Mount-cache hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.041015] Mountpoint-cache hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.049808] RCU Tasks: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1.
[ 0.056944] RCU Tasks Trace: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1.
[ 0.064656] rcu: Hierarchical SRCU implementation.
[ 0.069477] rcu: Max phase no-delay instances is 1000.
[ 0.075681] EFI services will not be available.
[ 0.080353] smp: Bringing up secondary CPUs ...
[ 0.085176] Detected PIPT I-cache on CPU1
[ 0.085213] CPU1: Booted secondary processor 0x0000000001 [0x410fd082]
[ 0.085504] Detected PIPT I-cache on CPU2
[ 0.085533] CPU2: Booted secondary processor 0x0000000002 [0x410fd082]
[ 0.085808] Detected PIPT I-cache on CPU3
[ 0.085838] CPU3: Booted secondary processor 0x0000000003 [0x410fd082]
[ 0.085873] smp: Brought up 1 node, 4 CPUs
[ 0.121780] SMP: Total of 4 processors activated.
[ 0.126512] CPU features: detected: 32-bit EL0 Support
[ 0.131687] CPU features: detected: 32-bit EL1 Support
[ 0.136857] CPU features: detected: CRC32 instructions
[ 0.142069] CPU: All CPU(s) started at EL2
[ 0.146200] alternatives: applying system-wide alternatives
[ 0.152757] devtmpfs: initialized
[ 0.159701] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.169517] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.176702] pinctrl core: initialized pinctrl subsystem
[ 0.182431] Machine: LS1046A RDB Board
[ 0.186202] SoC family: QorIQ LS1046A
[ 0.189879] SoC ID: svr:0x87070010, Revision: 1.0
[ 0.194775] DMI not present or invalid.
[ 0.198936] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.205304] DMA: preallocated 1024 KiB GFP_KERNEL pool for atomic allocations
[ 0.212647] DMA: preallocated 1024 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.220717] DMA: preallocated 1024 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.228793] audit: initializing netlink subsys (disabled)
[ 0.234282] audit: type=2000 audit(0.152:1): state=initialized audit_enabled=0 res=1
[ 0.234791] thermal_sys: Registered thermal governor 'step_wise'
[ 0.242081] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.248146] cpuidle: using governor menu
[ 0.258721] Bman ver:0a02,02,01
[ 0.263086] qman-fqd addr 0x00000009fe800000 size 0x800000
[ 0.268605] qman-pfdr addr 0x00000009fc000000 size 0x2000000
[ 0.274301] Qman ver:0a01,03,02,01
[ 0.277786] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.284654] ASID allocator initialised with 32768 entries
[ 0.290957] Serial: AMBA PL011 UART driver
[ 0.295135] imx mu driver is registered.
[ 0.299104] imx rpmsg driver is registered.
[ 0.323271] Modules: 2G module region forced by RANDOMIZE_MODULE_REGION_FULL
[ 0.330373] Modules: 0 pages in range for non-PLT usage
[ 0.330375] Modules: 511808 pages in range for PLT usage
[ 0.335917] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.348098] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[ 0.354405] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.361234] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[ 0.367539] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.374368] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[ 0.380673] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.387502] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[ 0.461845] raid6: neonx8 gen() 5328 MB/s
[ 0.534172] raid6: neonx4 gen() 5170 MB/s
[ 0.606500] raid6: neonx2 gen() 4304 MB/s
[ 0.678832] raid6: neonx1 gen() 3132 MB/s
[ 0.751160] raid6: int64x8 gen() 3016 MB/s
[ 0.823490] raid6: int64x4 gen() 2935 MB/s
[ 0.895822] raid6: int64x2 gen() 2844 MB/s
[ 0.968170] raid6: int64x1 gen() 2200 MB/s
[ 0.972465] raid6: using algorithm neonx8 gen() 5328 MB/s
[ 1.045930] raid6: .... xor() 3885 MB/s, rmw enabled
[ 1.050922] raid6: using neon recovery algorithm
[ 1.055964] ACPI: Interpreter disabled.
[ 1.062910] iommu: Default domain type: Passthrough
[ 1.067933] SCSI subsystem initialized
[ 1.071849] usbcore: registered new interface driver usbfs
[ 1.077380] usbcore: registered new interface driver hub
[ 1.082735] usbcore: registered new device driver usb
[ 1.088161] imx-i2c 2180000.i2c: scl-gpios not found
[ 1.093173] imx-i2c 2180000.i2c: using dma0chan16 (tx) and dma0chan17 (rx) for DMA transfers
[ 1.101830] i2c i2c-0: IMX I2C adapter registered
[ 1.106764] i2c i2c-1: IMX I2C adapter registered
[ 1.112199] pps_core: LinuxPPS API ver. 1 registered
[ 1.117193] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti
[ 1.126392] PTP clock support registered
[ 1.130452] EDAC MC: Ver: 3.0.0
[ 1.133957] scmi_core: SCMI protocol bus registered
[ 1.139087] bman-fbpr addr 0x00000009ff000000 size 0x1000000
[ 1.144813] Bman err interrupt handler present
[ 1.149875] Bman portal initialised, cpu 0
[ 1.154073] Bman portal initialised, cpu 1
[ 1.158273] Bman portal initialised, cpu 2
[ 1.162468] Bman portal initialised, cpu 3
[ 1.166587] Bman portals initialised
[ 1.175538] Qman err interrupt handler present
[ 1.180299] QMan: Allocated lookup table at (____ptrval____), entry count 131073
[ 1.188299] QMan doesn't need cleanup, uninhibiting IRQs
[ 1.193645] Qman portal initialised, cpu 0
[ 1.197833] QMan doesn't need cleanup, uninhibiting IRQs
[ 1.203176] Qman portal initialised, cpu 1
[ 1.207368] QMan doesn't need cleanup, uninhibiting IRQs
[ 1.212715] Qman portal initialised, cpu 2
[ 1.216901] QMan doesn't need cleanup, uninhibiting IRQs
[ 1.222245] Qman portal initialised, cpu 3
[ 1.226362] Qman portals initialised
[ 1.229998] Bman: BPID allocator includes range 32:32
[ 1.235106] Qman: FQID allocator includes range 256:256
[ 1.240361] Qman: FQID allocator includes range 32768:32768
[ 1.245996] Qman: CGRID allocator includes range 0:256
[ 1.251292] Qman: pool channel allocator includes range 1025:15
[ 1.257301] No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree
[ 1.263646] fsl-ifc 1530000.memory-controller: Freescale Integrated Flash Controller
[ 1.271457] fsl-ifc 1530000.memory-controller: IFC version 1.4, 8 banks
[ 1.278710] FPGA manager framework
[ 1.282171] Advanced Linux Sound Architecture Driver Initialized.
[ 1.288730] vgaarb: loaded
[ 1.291688] clocksource: Switched to clocksource arch_sys_counter
[ 1.297919] VFS: Disk quotas dquot_6.6.0
[ 1.301881] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 1.308881] pnp: PnP ACPI: disabled
[ 1.315703] NET: Registered PF_INET protocol family
[ 1.320778] IP idents hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 1.331172] tcp_listen_portaddr_hash hash table entries: 4096 (order: 4, 65536 bytes, linear)
[ 1.339805] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 1.347607] TCP established hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 1.355807] TCP bind hash table entries: 65536 (order: 9, 2097152 bytes, linear)
[ 1.364108] TCP: Hash tables configured (established 65536 bind 65536)
[ 1.370742] UDP hash table entries: 4096 (order: 5, 131072 bytes, linear)
[ 1.377670] UDP-Lite hash table entries: 4096 (order: 5, 131072 bytes, linear)
[ 1.385103] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 1.390996] RPC: Registered named UNIX socket transport module.
[ 1.396959] RPC: Registered udp transport module.
[ 1.401691] RPC: Registered tcp transport module.
[ 1.406421] RPC: Registered tcp-with-tls transport module.
[ 1.411939] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 1.418421] NET: Registered PF_XDP protocol family
[ 1.423246] PCI: CLS 0 bytes, default 64
[ 1.427356] kvm [1]: IPA Size Limit: 44 bits
[ 1.432710] kvm [1]: vgic interrupt IRQ9
[ 1.436674] kvm [1]: Hyp mode initialized successfully
[ 1.442454] Initialise system trusted keyrings
[ 1.446999] workingset: timestamp_bits=42 max_order=21 bucket_order=0
[ 1.453613] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 1.459584] NFS: Registering the id_resolver key type
[ 1.464678] Key type id_resolver registered
[ 1.468885] Key type id_legacy registered
[ 1.472923] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 1.479668] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 1.487119] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 1.493338] fuse: init (API version 7.39)
[ 1.497432] 9p: Installing v9fs 9p2000 file system support
[ 1.514632] jitterentropy: Initialization failed with host not compliant with requirements: 9
[ 1.523215] xor: measuring software checksum speed
[ 1.529168] 8regs : 8683 MB/sec
[ 1.534597] 32regs : 9391 MB/sec
[ 1.540288] arm64_neon : 7537 MB/sec
[ 1.544669] xor: using function: 32regs (9391 MB/sec)
[ 1.549751] Key type asymmetric registered
[ 1.553874] Asymmetric key parser 'x509' registered
[ 1.558800] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 1.566295] io scheduler mq-deadline registered
[ 1.570854] io scheduler kyber registered
[ 1.574896] io scheduler bfq registered
[ 1.583707] lynx-10g 1ea0000.phy: PLLF: enabled, locked, reference clock 100MHz, clock net 5GHz
[ 1.592468] lynx-10g 1ea0000.phy: Supported interfaces and link modes:
[ 1.599125] lynx-10g 1ea0000.phy: sgmii
[ 1.603156] lynx-10g 1ea0000.phy: 1000base-x
[ 1.607626] lynx-10g 1ea0000.phy: 1000baseKX/Full
[ 1.612532] lynx-10g 1ea0000.phy: qsgmii
[ 1.616651] lynx-10g 1ea0000.phy: PLLS: enabled, locked, reference clock 156.25MHz, clock net 5.15625GHz
[ 1.626194] lynx-10g 1ea0000.phy: Supported interfaces and link modes:
[ 1.632849] lynx-10g 1ea0000.phy: 10gbase-r
[ 1.637231] lynx-10g 1ea0000.phy: 10000baseKR/Full
[ 1.642383] lynx-10g 1eb0000.phy: PLLF: enabled, locked, reference clock 100MHz, clock net unknown
[ 1.651406] lynx-10g 1eb0000.phy: Supported interfaces and link modes:
[ 1.658061] lynx-10g 1eb0000.phy: PLLS: enabled, locked, reference clock 100MHz, clock net 5GHz
[ 1.666816] lynx-10g 1eb0000.phy: Supported interfaces and link modes:
[ 1.673471] lynx-10g 1eb0000.phy: sgmii
[ 1.677506] lynx-10g 1eb0000.phy: 1000base-x
[ 1.681974] lynx-10g 1eb0000.phy: 1000baseKX/Full
[ 1.695421] layerscape-pcie 3400000.pcie: host bridge /soc/pcie@3400000 ranges:
[ 1.702798] layerscape-pcie 3400000.pcie: IO 0x4000010000..0x400001ffff -> 0x0000000000
[ 1.711387] layerscape-pcie 3400000.pcie: MEM 0x4040000000..0x407fffffff -> 0x0040000000
[ 1.719996] layerscape-pcie 3400000.pcie: iATU: unroll F, 8 ob, 6 ib, align 4K, limit 4G
[ 2.728233] layerscape-pcie 3400000.pcie: Phy link never came up
[ 2.734382] layerscape-pcie 3400000.pcie: PCI host bridge to bus 0000:00
[ 2.741129] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 2.746649] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 2.752869] pci_bus 0000:00: root bus resource [mem 0x4040000000-0x407fffffff] (bus address [0x40000000-0x7fffffff])
[ 2.763477] pci 0000:00:00.0: [1957:81c0] type 01 class 0x060400
[ 2.769560] pci 0000:00:00.0: supports D1 D2
[ 2.773856] pci 0000:00:00.0: PME# supported from D0 D1 D2 D3hot
[ 2.780777] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[ 2.786181] pcieport 0000:00:00.0: PME: Signaling with IRQ 57
[ 2.792065] pcieport 0000:00:00.0: AER: enabled with IRQ 56
[ 2.797809] layerscape-pcie 3500000.pcie: host bridge /soc/pcie@3500000 ranges:
[ 2.805181] layerscape-pcie 3500000.pcie: IO 0x4800010000..0x480001ffff -> 0x0000000000
[ 2.813769] layerscape-pcie 3500000.pcie: MEM 0x4840000000..0x487fffffff -> 0x0040000000
[ 2.822374] layerscape-pcie 3500000.pcie: iATU: unroll F, 8 ob, 6 ib, align 4K, limit 4G
[ 3.830597] layerscape-pcie 3500000.pcie: Phy link never came up
[ 3.836688] layerscape-pcie 3500000.pcie: PCI host bridge to bus 0001:00
[ 3.843434] pci_bus 0001:00: root bus resource [bus 00-ff]
[ 3.848955] pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x0000-0xffff])
[ 3.857974] pci_bus 0001:00: root bus resource [mem 0x4840000000-0x487fffffff] (bus address [0x40000000-0x7fffffff])
[ 3.868578] pci 0001:00:00.0: [1957:81c0] type 01 class 0x060400
[ 3.874656] pci 0001:00:00.0: supports D1 D2
[ 3.878951] pci 0001:00:00.0: PME# supported from D0 D1 D2 D3hot
[ 3.885850] pci 0001:00:00.0: PCI bridge to [bus 01-ff]
[ 3.891239] pcieport 0001:00:00.0: PME: Signaling with IRQ 60
[ 3.897136] pcieport 0001:00:00.0: AER: enabled with IRQ 59
[ 3.902870] layerscape-pcie 3600000.pcie: host bridge /soc/pcie@3600000 ranges:
[ 3.910242] layerscape-pcie 3600000.pcie: IO 0x5000010000..0x500001ffff -> 0x0000000000
[ 3.918829] layerscape-pcie 3600000.pcie: MEM 0x5040000000..0x507fffffff -> 0x0040000000
[ 3.927434] layerscape-pcie 3600000.pcie: iATU: unroll F, 8 ob, 6 ib, align 4K, limit 4G
[ 4.935653] layerscape-pcie 3600000.pcie: Phy link never came up
[ 4.941746] layerscape-pcie 3600000.pcie: PCI host bridge to bus 0002:00
[ 4.948502] pci_bus 0002:00: root bus resource [bus 00-ff]
[ 4.954023] pci_bus 0002:00: root bus resource [io 0x20000-0x2ffff] (bus address [0x0000-0xffff])
[ 4.963043] pci_bus 0002:00: root bus resource [mem 0x5040000000-0x507fffffff] (bus address [0x40000000-0x7fffffff])
[ 4.973645] pci 0002:00:00.0: [1957:81c0] type 01 class 0x060400
[ 4.979724] pci 0002:00:00.0: supports D1 D2
[ 4.984020] pci 0002:00:00.0: PME# supported from D0 D1 D2 D3hot
[ 4.990913] pci 0002:00:00.0: PCI bridge to [bus 01-ff]
[ 4.996298] pcieport 0002:00:00.0: PME: Signaling with IRQ 63
[ 5.002195] pcieport 0002:00:00.0: AER: enabled with IRQ 62
[ 5.008954] EINJ: ACPI disabled.
[ 5.028654] Bus freq driver module loaded
[ 5.040694] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 5.048861] printk: console [ttyS0] disabled
[ 5.053293] 21c0500.serial: ttyS0 at MMIO 0x21c0500 (irq = 64, base_baud = 18750000) is a 16550A
[ 5.062159] printk: console [ttyS0] enabled
[ 5.062159] printk: console [ttyS0] enabled
[ 5.070552] printk: bootconsole [uart8250] disabled
[ 5.070552] printk: bootconsole [uart8250] disabled
[ 5.084081] 21c0600.serial: ttyS1 at MMIO 0x21c0600 (irq = 64, base_baud = 18750000) is a 16550A
[ 5.093301] SuperH (H)SCI(F) driver initialized
[ 5.098346] msm_serial: driver initialized
[ 5.103021] STM32 USART driver initialized
[ 5.112700] brd: module loaded
[ 5.117940] loop: module loaded
[ 5.121929] megasas: 07.725.01.00-rc1
[ 5.126431] ahci-qoriq 3200000.sata: supply ahci not found, using dummy regulator
[ 5.133966] ahci-qoriq 3200000.sata: supply phy not found, using dummy regulator
[ 5.141386] ahci-qoriq 3200000.sata: supply target not found, using dummy regulator
[ 5.149136] ahci-qoriq 3200000.sata: AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl platform mode
[ 5.158110] ahci-qoriq 3200000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst
[ 5.168153] scsi host0: ahci-qoriq
[ 5.171631] ata1: SATA max UDMA/133 mmio [mem 0x03200000-0x0320ffff] port 0x100 irq 65
[ 5.180707] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xac
[ 5.187068] nand: Micron MT29F4G08ABBEAH4
[ 5.191075] nand: 512 MiB, SLC, erase size: 256 KiB, page size: 4096, OOB size: 224
[ 5.199422] Bad block table found at page 131008, version 0x01
[ 5.206586] Bad block table found at page 130944, version 0x01
[ 5.213816] fsl,ifc-nand 7e800000.nand: IFC NAND device at 0x7e800000, bank 0
[ 5.222230] spi-nor spi0.0: s25fs512s (65536 Kbytes)
[ 5.227833] spi-nor spi0.1: s25fs512s (65536 Kbytes)
[ 5.234499] MACsec IEEE 802.1AE
[ 5.239512] tun: Universal TUN/TAP device driver, 1.6
[ 5.245377] thunder_xcv, ver 1.0
[ 5.248619] thunder_bgx, ver 1.0
[ 5.251859] nicpf, ver 1.0
[ 5.263921] hwmon hwmon0: temp1_input not attached to any thermal zone
[ 5.288983] Freescale FM module, FMD API version 21.1.0
[ 5.296964] Freescale FM Ports module
[ 5.300632] fsl_mac: fsl_mac: FSL FMan MAC API based driver
[ 5.306393] fsl_mac 1ae4000.ethernet: FMan MEMAC
[ 5.311016] fsl_mac 1ae4000.ethernet: FMan MAC address: 00:04:9f:05:ad:cc
[ 5.317911] fsl_mac 1ae6000.ethernet: FMan MEMAC
[ 5.322532] fsl_mac 1ae6000.ethernet: FMan MAC address: 00:04:9f:05:ad:cd
[ 5.329475] fsl_mac 1ae8000.ethernet: FMan MEMAC
[ 5.334096] fsl_mac 1ae8000.ethernet: FMan MAC address: 00:04:9f:05:ad:c8
[ 5.341048] fsl_mac 1aea000.ethernet: FMan MEMAC
[ 5.345667] fsl_mac 1aea000.ethernet: FMan MAC address: 00:04:9f:05:ad:c9
[ 5.352567] fsl_mac 1af0000.ethernet: FMan MEMAC
[ 5.357188] fsl_mac 1af0000.ethernet: FMan MAC address: 00:04:9f:05:ad:cb
[ 5.364322] fsl_mac 1af2000.ethernet: FMan MEMAC
[ 5.368947] fsl_mac 1af2000.ethernet: FMan MAC address: 00:04:9f:05:ad:ca
[ 5.375776] fsl_dpa: FSL DPAA Ethernet driver
[ 5.381473] fsl_dpa: fsl_dpa: Probed interface eth0
[ 5.387650] fsl_dpa: fsl_dpa: Probed interface eth1
[ 5.393938] fsl_dpa: fsl_dpa: Probed interface eth2
[ 5.400354] fsl_dpa: fsl_dpa: Probed interface eth3
[ 5.406867] fsl_dpa: fsl_dpa: Probed interface eth4
[ 5.413469] fsl_dpa: fsl_dpa: Probed interface eth5
[ 5.418380] fsl_advanced: FSL DPAA Advanced drivers:
[ 5.423345] fsl_proxy: FSL DPAA Proxy initialization driver
[ 5.429079] fsl_oh: FSL FMan Offline Parsing port driver
[ 5.435018] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 5.442244] hns3: Copyright (c) 2017 Huawei Corporation.
[ 5.447570] hclge is initializing
[ 5.450894] e1000: Intel(R) PRO/1000 Network Driver
[ 5.455771] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 5.461530] e1000e: Intel(R) PRO/1000 Network Driver
[ 5.466493] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 5.472425] igb: Intel(R) Gigabit Ethernet Network Driver
[ 5.477823] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 5.483406] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 5.489674] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 5.495882] sky2: driver version 1.30
[ 5.500536] usbcore: registered new device driver r8152-cfgselector
[ 5.501854] ata1: SATA link down (SStatus 0 SControl 300)
[ 5.506818] usbcore: registered new interface driver r8152
[ 5.517711] usbcore: registered new interface driver asix
[ 5.523125] usbcore: registered new interface driver ax88179_178a
[ 5.529586] VFIO - User Level meta-driver version: 0.3
[ 5.538432] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 5.543935] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[ 5.551657] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f66d hci version 0x100 quirks 0x0000008002000810
[ 5.561073] xhci-hcd xhci-hcd.0.auto: irq 69, io mem 0x02f00000
[ 5.567058] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 5.572548] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[ 5.580210] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed
[ 5.587053] hub 1-0:1.0: USB hub found
[ 5.590823] hub 1-0:1.0: 1 port detected
[ 5.595184] hub 2-0:1.0: USB hub found
[ 5.598953] hub 2-0:1.0: 1 port detected
[ 5.603067] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 5.608565] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 3
[ 5.616273] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220f66d hci version 0x100 quirks 0x0000008002000810
[ 5.625686] xhci-hcd xhci-hcd.1.auto: irq 71, io mem 0x03100000
[ 5.631669] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 5.637160] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 4
[ 5.644823] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed
[ 5.651605] hub 3-0:1.0: USB hub found
[ 5.655376] hub 3-0:1.0: 1 port detected
[ 5.659724] hub 4-0:1.0: USB hub found
[ 5.663482] hub 4-0:1.0: 1 port detected
[ 5.668030] usbcore: registered new interface driver uas
[ 5.673370] usbcore: registered new interface driver usb-storage
[ 5.681982] i2c_dev: i2c /dev entries driver
[ 5.688382] ptp_qoriq: device tree node missing required elements, try automatic configuration
[ 5.697068] pps pps0: new PPS source ptp0
[ 5.715696] qoriq-cpufreq qoriq-cpufreq: Freescale QorIQ CPU frequency scaling driver
[ 5.724247] sdhci: Secure Digital Host Controller Interface driver
[ 5.730432] sdhci: Copyright(c) Pierre Ossman
[ 5.735495] Synopsys Designware Multimedia Card Interface Driver
[ 5.742412] sdhci-pltfm: SDHCI platform and OF driver helper
[ 5.750119] ledtrig-cpu: registered to indicate activity on CPUs
[ 5.757191] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 5.764358] usbcore: registered new interface driver usbhid
[ 5.769937] usbhid: USB HID core driver
[ 5.771696] mmc0: SDHCI controller on 1560000.esdhc [1560000.esdhc] using ADMA 64-bit
[ 5.774321] Freescale USDPAA process driver
[ 5.785791] fsl-usdpaa: no region found
[ 5.789625] Freescale USDPAA process IRQ driver
[ 5.797060] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
[ 5.806167] cs_system_cfg: CoreSight Configuration manager initialised
[ 5.814227] optee: probing for conduit method.
[ 5.818676] optee: api uid mismatch
[ 5.822164] optee: probe of firmware:optee failed with error -22
[ 5.830641] NET: Registered PF_LLC protocol family
[ 5.835479] u32 classifier
[ 5.838200] input device check on
[ 5.841862] Actions configured
[ 5.846313] Initializing XFRM netlink socket
[ 5.850614] NET: Registered PF_INET6 protocol family
[ 5.856121] Segment Routing with IPv6
[ 5.859806] In-situ OAM (IOAM) with IPv6
[ 5.863769] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 5.869911] NET: Registered PF_PACKET protocol family
[ 5.874969] NET: Registered PF_KEY protocol family
[ 5.879779] Bridge firewalling registered
[ 5.883932] 8021q: 802.1Q VLAN Support v1.8
[ 5.888125] lib80211: common routines for IEEE802.11 drivers
[ 5.893810] 9pnet: Installing 9P2000 support
[ 5.898135] Key type dns_resolver registered
[ 5.910932] registered taskstats version 1
[ 5.915098] Loading compiled-in X.509 certificates
[ 5.924142] Btrfs loaded, zoned=no, fsverity=no
[ 5.943764] mmc0: new ultra high speed SDR104 SDHC card at address ffb5
[ 5.950695] mmcblk0: mmc0:ffb5 UC0D5 29.8 GiB
[ 5.957137] mmcblk0: p1 p2
[ 6.303724] Sending DHCP requests ..., OK
[ 14.867761] IP-Config: Got DHCP answer from 128.224.167.20, my address is 128.224.167.251
[ 14.875998] IP-Config: Complete:
[ 14.879226] device=eth0, hwaddr=00:04:9f:05:ad:cc, ipaddr=128.224.167.251, mask=255.255.254.0, gw=128.224.166.1
[ 14.889775] host=128.224.167.251, domain=pek-tuxlab.wrs.com, nis-domain=(none)
[ 14.897449] bootserver=128.224.161.77, rootserver=128.224.34.139, rootpath=
[ 14.897458] nameserver0=128.224.160.11, nameserver1=147.11.100.30, nameserver2=147.11.1.11
[ 14.913599] ntpserver0=147.11.100.50
[ 15.009986] cpu 1: > WARNING (FM-Port) [CPU01, /drivers/net/ethernet/freescale/sdk_fman/Peripherals/FM/Port/fm_port.c:3552 FM_PORT_Disable]:
[ 15.009998] cpu 1: FM-0-port-10g-TX-1: BMI or QMI is Busy. Port forced down
[ 15.022718] cpu 1:
[ 15.039954] clk: Disabling unused clocks
[ 15.043944] ALSA device list:
[ 15.046915] No soundcards found.
[ 15.077658] VFS: Mounted root (nfs filesystem) on device 0:21.
[ 15.087588] devtmpfs: mounted
[ 15.094705] Freeing unused kernel memory: 9728K
[ 15.099395] Run /sbin/init as init process
INIT: version 3.04 booting
Starting udev
[ 16.780192] udevd[147]: starting version 3.2.14
[ 17.031698] random: crng init done
[ 17.288169] udevd[148]: starting eudev-3.2.14
[ 17.483193] mtdblock: MTD device '7e800000.flash' is NAND, please consider using UBI block devices instead.
[ 17.540246] EDAC MC0: Giving out device to module fsl_ddr_edac controller fsl_mc_err: DEV fsl_mc_err (INTERRUPT)
[ 17.567155] fsl_ddr_edac acquired irq 78 for MC
[ 17.575023] fsl_ddr_edac MC err registered
[ 17.595212] caam 1700000.crypto: Linux CAAM Queue I/F driver initialised
[ 17.607818] caam 1700000.crypto: device ID = 0x0a11030100000000 (Era
[ 17.615053] caam 1700000.crypto: job rings = 3, qi = 1
[ 17.667125] lm90 0-004c: supply vcc not found, using dummy regulator
[ 17.678559] ina2xx 0-0040: supply vs not found, using dummy regulator
[ 17.681942] hwmon hwmon6: temp1_input not attached to any thermal zone
[ 17.691112] ina2xx 0-0040: power monitor ina220 (Rshunt = 1000 uOhm)
[ 17.691690] hwmon hwmon6: temp2_input not attached to any thermal zone
[ 17.705382] ftm-alarm 29d0000.timer: registered as rtc1
[ 17.736619] rtc-pcf2127-i2c 1-0051: registered as rtc0
[ 17.744136] rtc-pcf2127-i2c 1-0051: setting system clock to 2020-04-10T10:26:25 UTC (1586514385)
[ 17.833135] at24 0-0052: supply vcc not found, using dummy regulator
[ 17.840859] at24 0-0052: 512 byte cat24c05 EEPROM, writable, 1 bytes/write
[ 17.896153] fsl_dpa soc:fsl,dpaa:ethernet@5 fm1-mac6: renamed from eth3
[ 17.931888] fsl_dpa soc:fsl,dpaa:ethernet@3 fm1-mac4: renamed from eth1
[ 17.955859] fsl_dpa soc:fsl,dpaa:ethernet@8 fm1-mac9: renamed from eth4
[ 17.988580] fsl_dpa soc:fsl,dpaa:ethernet@9 fm1-mac10: renamed from eth5
[ 18.036719] fsl_dpa soc:fsl,dpaa:ethernet@2 fm1-mac3: renamed from eth0 (while UP)
[ 18.078011] fsl_dpa soc:fsl,dpaa:ethernet@4 fm1-mac5: renamed from eth2
[ 18.404087] caam algorithms registered in /proc/crypto
[ 18.409418] caam 1700000.crypto: caam pkc algorithms registered in /proc/crypto
[ 18.416807] caam 1700000.crypto: rng crypto API alg registered prng-caam
[ 18.423953] caam 1700000.crypto: algorithms registered in /proc/crypto
[ 18.430513] caam 1700000.crypto: registering rng-caam
[ 18.435789] Device caam-keygen registered
[ 18.616557] mtdblock: MTD device '7e800000.flash' is NAND, please consider using UBI block devices instead.
[ 19.083182] EXT4-fs (mmcblk0p2): mounted filesystem 39d83a26-6557-4087-bdfb-4c98539f46e7 r/w with ordered data mode. Quota mode: none.
sysctl: cannot stat /proc/sys/net/ipv4/tcp_syncookies: No such file or directory
INIT: Entering runlevel: 5
Configuring network interfaces... Error: ipv4: Address already assigned.
Starting system message bus: dbus.
Mounting cgroups...Done
Starting OpenBSD Secure Shell server: sshd
done.
Starting OP-TEE Supplicant: ERR [692] TSUP:main:907: make_daemon(): -1
Starting rpcbind daemon...done.
starting statd: done
Starting atd: OK
Starting domain name service: named.
Starting bluetooth: bluetoothd.
egrep: warning: egrep is obsolescent; using grep -E
starting DNS forwarder and DHCP server: dnsmasq...
dnsmasq: failed to create listening socket for 128.224.167.251: Address already in use
Starting dockerd:

Starting HOSTAP Daemon: [ 33.139644] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 33.461035] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 33.467468] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
[ 33.525324] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 33.534103] cfg80211: failed to load regulatory.db
Could not read interface wlan0 flags: No such device
nl80211: Driver does not support authentication/association or connect commands
nl80211: deinit ifname=wlan0 disabled_11b_rates=0
Could not read interface wlan0 flags: No such device
nl80211 driver initialization failed.
wlan0: interface state UNINITIALIZED->DISABLED
wlan0: AP-DISABLED
wlan0: CTRL-EVENT-TERMINATING
hostapd_free_hapd_data: Interface wlan0 wasn't started
Starting LXC autoboot containers:
Starting network benchmark server: netserver.
NFS daemon support not enabled in kernel
Starting ntpd: done
[ 37.314738] overlayfs: upper fs does not support tmpfile.
[ 37.346918] overlayfs: upper fs does not support RENAME_WHITEOUT.
[ 37.353080] overlayfs: failed to set xattr on upper
[ 37.358091] overlayfs: ...falling back to redirect_dir=nofollow.
[ 37.364170] overlayfs: ...falling back to uuid=null.
[ 37.369245] overlayfs: upper fs missing required features.
Starting system log daemon...0
Starting internet superserver: xinetd.
Starting watchdog daemon...done
No makedumpfile found.
* Starting virtualization library daemon: libvirtd
No /usr/bin/dnsmasq found running; none killed.
libvirt: error : failed to open /var/log/libvirt/libvirtd.log: No such file or directory
*bvirt: error : failed to open /var/log/libvirt/libvirtd.log: No such f[fail] directory
sed: -e expression #1, char 23: unterminated address regex
sed: -e expression #1, char 23: unterminated address regex
sed: -e expression #1, char 23: unterminated address regex
Starting crond: OK
Starting tcf-agent: OK

QorIQ SDK (FSL Reference Distro) 5.0.2 ls1046ardb ttyS0

ls1046ardb login: root
root@ls1046ardb:~# date
Fri Apr 10 10:27:02 UTC 2020
root@ls1046ardb:~# hwclock
2020-04-10 10:27:08.610907+00:00
root@ls1046ardb:~# date 110811332024
Fri Nov 8 11:33:00 UTC 2024
root@ls1046ardb:~# hwclock -w
root@ls1046ardb:~# date
Fri Nov 8 11:33:13 UTC 2024
root@ls1046ardb:~# uname -a
Linux ls1046ardb 6.6.36-gd23d64eea511 #1 SMP PREEMPT Wed Sep 4 08:22:45 UTC 2024 aarch64 GNU/Linux
root@ls1046ardb:~# cat /proc/cmdline
root=/dev/nfs rw nfsroot=128.224.34.139:/tftpboot/qoriq-6.6.36/ls1046/rootfs,v3,tcp ip=dhcp console=ttyS0,115200 earlycon=uart8250,mmio,0x21c0500
root@ls1046ardb:~# rngd
root@ls1046ardb:~# time rngtest -c 100 < /dev/hwrng
rngtest 6.16
Copyright (c) 2004 by Henrique de Moraes Holschuh
This is free software; see the source for copying conditions. There is NO warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

rngtest: starting FIPS tests...
rngtest: bits received from input: 2000032
rngtest: FIPS 140-2 successes: 100
rngtest: FIPS 140-2 failures: 0
rngtest: FIPS 140-2(2001-10-10) Monobit: 0
rngtest: FIPS 140-2(2001-10-10) Poker: 0
rngtest: FIPS 140-2(2001-10-10) Runs: 0
rngtest: FIPS 140-2(2001-10-10) Long run: 0
rngtest: FIPS 140-2(2001-10-10) Continuous run: 0
rngtest: input channel speed: (min=3.095; avg=4.650; max=4.683)Kibits/s
rngtest: FIPS tests speed: (min=28.899; avg=30.492; max=77.851)Mibits/s
rngtest: Program run time: 420141440 microseconds

real 7m0.163s
user 0m0.065s
sys 0m0.197s

Re: LS1046ARDB run rngtest very slowly on SDK scarthgap 5.0-lf-6.6.36

Hello,

Please provide the step by step you followed to flash the image on the sd card to make the test on my side and compare the results.

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 10:28 PM
Updated by: