Hello, I'm using IMX8ULP EVK9 board and i have onboard LED. I'm able to control LED using "gpioset -c /dev/gpiochip4 20=1" command. Now I'm trying to control LED using C code but on that time i'm getting "Request lines failed: Invalid argument" error. I'm using libgpiod 2.0. Following is my C code const char *chipname = "/dev/gpiochip4"; unsigned int line_num = 20; struct gpiod_chip *chip; struct gpiod_request_config *req_cfg; struct gpiod_line_config *line_cfg; struct gpiod_line_request *request; // Open the GPIO chip chip = gpiod_chip_open(chipname); if (!chip) { perror("Open chip failed"); return 1; } // Allocate and configure the request config req_cfg = gpiod_request_config_new(); gpiod_request_config_set_consumer(req_cfg, "led_control"); // Allocate line config line_cfg = gpiod_line_config_new(); // Request the line unsigned int offsets[] = {line_num}; request = gpiod_chip_request_lines(chip, req_cfg, line_cfg); if (!request) { perror("Request lines failed"); gpiod_chip_close(chip); return 1; } // Blink the LED for (int i = 0; i < 10; i++) { gpiod_line_request_set_value(request, line_num, GPIOD_LINE_VALUE_ACTIVE); // Turn on LED sleep(1); gpiod_line_request_set_value(request, line_num, GPIOD_LINE_VALUE_INACTIVE); // Turn off LED sleep(1); } // Clean up gpiod_line_request_release(request); gpiod_request_config_free(req_cfg); gpiod_line_config_free(line_cfg); // Free line_cfg gpiod_chip_close(chip);
Hi @Zhiming_Liu ,
I'm trying to read GPIO line values in imx91 using libgpiod by c application. But showing gpiod.h is not found. I installed libgpiod-tools and able to see gpiod.h in /usr/include/. But when I compile recipe it is showing error undefined reference to API used. It is linking error is there any way to read value of GPIO using C application.
Thanks
Hello,
Please refer libgpiod 2.0 examples to modify your code.
https://github.com/brgl/libgpiod/tree/v2.2.x/examples
Best Regards,
Zhiming