1986713_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1986713_en-US

1986713_en-US

CAN TX reset issue

Hi NXP,

    I need to operate CAN operation with Blocking mode to send data in faster rate. I have tried non blocking mode , there I have not faced any issue. Once I start using Blocking mode , COntroller will reset whenever I configure non zero value.

FLEXCAN_DRV_SendBlocking(INST_FLEXCAN_CONFIG_1, E_MB_MSG_TX, &arrayMessageBufferInfo[E_MB_MSG_TX].rx_info, psCanFrameToSend->u32Identifier, psCanFrameToSend->au8Data, (uint32_t)10UL/* Found Timeout error and operate at 0 */);


Here it works only with 0, For other Timeout configs it's resetting the board. Could you please help me out? It's failing in semaphore wait might. Which are all the configs I need to consider when I want to use blocking mode operation

Re: CAN TX reset issue

Hi@AbhiMR

In the attachment, I have made sample codes for both non-blocking and blocking sending methods.

You can test these two sample projects. If you have any questions or problems, you can point them out and I will help you reproduce and analyze it

This is my test, you can send frame ID = 2 from PC to S32K116, S32K116 will send back the received frame counter and transmited frame counter.

Senlent_0-1731486023335.png


Re: CAN TX reset issue

Hi NXP,

Please find more details. Could you please share 8byte CAN TX operation example with attached setting. Need example in Blocking mode.


Note: CAN TX not working in Blocking mode, it's not hitting any ISR. If not how to get SUCCESS notification?


I have attached all CAN related configuration. 


Re: CAN TX reset issue

Hi NXP,

I am sharing all my CAN config. Better if you can provide working example with 8byte TX payload. 


Please refer the details that we elaborated more 

In our application we have the following configuration, which are of initialization and run time operation to transmit the can frame.


/*-------------------------------------------------INIT PART ---------------------------------------------------------------------------------------------------*/


flexcan_user_config_t flexcanInitConfig_500k = {

  .flexcanMode = FLEXCAN_NORMAL_MODE,

  .fd_enable = false,

  .payload = FLEXCAN_PAYLOAD_SIZE_8,

  .max_num_mb = 16UL,

  .num_id_filters = FLEXCAN_RX_FIFO_ID_FILTERS_8,

  .is_rx_fifo_needed = false,

  .transfer_type = FLEXCAN_RXFIFO_USING_INTERRUPTS,

  .rxFifoDMAChannel = 0U,

  .pe_clock = FLEXCAN_CLK_SOURCE_OSC,

  .bitrate = {

    .propSeg = 7UL,

    .phaseSeg1 = 4UL,

    .phaseSeg2 = 1UL,

    .preDivider = 1UL,

    .rJumpwidth = 1UL

  }

};

FLEXCAN_DRV_Init(INST_FLEXCAN_CONFIG_1, &flexcanState0, &flexcanInitConfig_500k);

/* Install callback function */

FLEXCAN_DRV_InstallEventCallback(INST_FLEXCAN_CONFIG_1, flexcanCallBack, NULL);

FLEXCAN_DRV_InstallErrorCallback(INST_FLEXCAN_CONFIG_1, flexcanErrorCallBack, NULL);


/*--------------------------------------------------INIT Completed --------------------------------------------------------------------------------------------*/

Non-Blocking Mode

We have developed our application to transmit CAN frame at every 100ms. In non-blocking mode able to use FLEXCAN_DRV_Send method to transfer CAN Buffer , where we can get FLEXCAN_EVENT_TX_COMPLETE response in the above configured callback "flexcanCallBack". It behaves as expected.

/*------------------------------ Runtime operation ----------------------------------------------*/

 

FLEXCAN_DRV_Send(INST_FLEXCAN_CONFIG_1, E_MB_MSG_TX, &arrayMessageBufferInfo[E_MB_MSG_TX].rx_info, psCanFrameToSend->u32Identifier, psCanFrameToSend->au8Data);

/*------------------------------ Runtime operation ----------------------------------------------*/


In the above implementation we have drawback in transmission of frame at higher speed in non-blocking mode. Transmission is getting delayed whenever we have CAN request on the same time.


Blocking mode

Thought of trying blocking mode and facing the following issues


  1. With Timeout 0UL able to send the CAN frame with expected speed in our application without notifying success message. It will always return STATUS_TIMEOUT from blocking callWe suspect not safer in implementation.

/*-----------------------------------Runtime Operation -------------------------------------------------------------------*/

Returnvalue=FLEXCAN_DRV_SendBlocking(INST_FLEXCAN_CONFIG_1, E_MB_MSG_TX, &arrayMessageBufferInfo[E_MB_MSG_TX].rx_info, psCanFrameToSend->u32Identifier, psCanFrameToSend->au8Data, (uint32_t)0UL);

/*-----------------------------------Runtime Operation -------------------------------------------------------------------*/


  1. I tried sending data with timeout(Any Value from 1UL ) to get STATUS_SUCCESS   . In this case controller will go for hang state.

/*-----------------------------------Runtime Operation -------------------------------------------------------------------*/

Returnvalue=FLEXCAN_DRV_SendBlocking(INST_FLEXCAN_CONFIG_1, E_MB_MSG_TX, &arrayMessageBufferInfo[E_MB_MSG_TX].rx_info, psCanFrameToSend->u32Identifier, psCanFrameToSend->au8Data, (uint32_t)10UL);

/*-----------------------------------Runtime Operation -------------------------------------------------------------------*/

  1.             Observation is that controller is stuck at OSIF_SemaWait function, because stopped producing osif_Tick. The following line of controller got hang, observed delta is 0 to hang the controller.

              if ((timeoutTicks != OSIF_WAIT_FOREVER) && (delta > max))     /* Line number 349 in osif_baremetal.c  */

  1.             Not received any TX completion interrupt to post semaphore from ISR. Since Post semaphore we have at FLEXCAN_CompleteTransfer function.

NOTE: It's not hitting any ISR in CAN Blocking mode 

Since we don’t have to process anything in non-blocking mode for TX operation. We want to try blocking mode with STATUS_SUCCESS   message.

Could you please review the above details and provide us the detail to fix the same and let us know the list of methods to improve CAN TX frame transmission from the application. Share suitable examples to explore all the methods.


Additional note:

Controller: S32k116

SDK Version : S32SDK_S32K1XX_RTM_4.0.2

Referred link : file:///C:/NXP/S32DS.3.4/S32DS/software/S32SDK_S32K1XX_RTM_4.0.2/doc/html_S32K116/group__flexcan__driver.html

Re: CAN TX reset issue

Hi@AbhiMR

Sorry for the long waiting, cause we overloaded recently.

Could you please provided your project and then i will help you to check it.

Re: CAN TX reset issue

Further to my debugging info. The semaphore has not been posted to continue the operation. It has to happen from  FLEXCAN_CompleteTransfer(instance, mb_idx); .  It will happen only when I receive a TX_Complete interrupt even in blocking mode, It's not happening. The config I am using is of for CAN init 

flexcan_user_config_t flexcanInitConfig_500k_listen = {
.flexcanMode = FLEXCAN_LISTEN_ONLY_MODE,
.fd_enable = false,
.payload = FLEXCAN_PAYLOAD_SIZE_8,
.max_num_mb = 16UL,
.num_id_filters = FLEXCAN_RX_FIFO_ID_FILTERS_8,
.is_rx_fifo_needed = false,
.transfer_type = FLEXCAN_RXFIFO_USING_INTERRUPTS,
.rxFifoDMAChannel = 0U,
.pe_clock = FLEXCAN_CLK_SOURCE_OSC,
.bitrate = {
.propSeg = 7UL,
.phaseSeg1 = 4UL,
.phaseSeg2 = 1UL,
.preDivider = 1UL,
.rJumpwidth = 1UL
}
};flexcan_user_config_t flexcanInitConfig_500k_listen = {
.flexcanMode = FLEXCAN_LISTEN_ONLY_MODE,
.fd_enable = false,
.payload = FLEXCAN_PAYLOAD_SIZE_8,
.max_num_mb = 16UL,
.num_id_filters = FLEXCAN_RX_FIFO_ID_FILTERS_8,
.is_rx_fifo_needed = false,
.transfer_type = FLEXCAN_RXFIFO_USING_INTERRUPTS,
.rxFifoDMAChannel = 0U,
.pe_clock = FLEXCAN_CLK_SOURCE_OSC,
.bitrate = {
.propSeg = 7UL,
.phaseSeg1 = 4UL,
.phaseSeg2 = 1UL,
.preDivider = 1UL,
.rJumpwidth = 1UL
}
};

FLEXCAN_DRV_Init(INST_FLEXCAN_CONFIG_1, &flexcanState0, &flexcanInitConfig_500k_listen);

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 03:28 PM
更新者: