Dear NXP fellows,
This question is a sequel to my previous topic:
Questions regarding multi-core networking in S32G399A
Right now, I have enabled PFE Master/Slave on our custom board based on S32G399A-RDB3 by appending pfe-slave to the Yocto distro-features:
DISTRO_FEATURES:append = " pfe pfe-slave"This enables the PFE Slave to run on the A53 cores (Linux BSP).
On the slave side, it seems to be working as expected, I can assign IP addresses to the three PFE interfaces and the ping is working from both sides.
For your reference, the command libfci_cli phyif-print returns:
DISCLAIMER: This is a DEMO application. It is not part of the production code deliverables.
0: emac0
ingress: 57 egress: 45 discarded: 0 malformed: 0
flexible-filter: ---
ptp-mgmt-if: ---
MAC:
00:04:9f:be:ef:00
33:33:00:00:00:01
01:00:5e:00:00:01
33:33:ff:be:ef:00
01:80:c2:00:00:00
01:80:c2:00:00:03
01:80:c2:00:00:0e
33:33:00:01:00:03
01:00:5e:00:00:fc
mirrors:
rxmirr0: ---
rxmirr1: ---
txmirr0: ---
txmirr1: ---
logical interfaces:
0: emac0
accepted: 57 rejected: 0 discarded: 0 processed: 57
egress: hif0
match-rules: ---
1: emac1
ingress: 75 egress: 53 discarded: 0 malformed: 0
flexible-filter: ---
ptp-mgmt-if: ---
MAC:
00:04:9f:be:ef:01
33:33:00:00:00:01
01:00:5e:00:00:01
33:33:ff:be:ef:01
mirrors:
rxmirr0: ---
rxmirr1: ---
txmirr0: ---
txmirr1: ---
logical interfaces:
1: emac1
accepted: 75 rejected: 0 discarded: 0 processed: 75
egress: hif1
match-rules: ---
2: emac2
ingress: 13 egress: 37 discarded: 0 malformed: 0
flexible-filter: ---
ptp-mgmt-if: ---
MAC:
00:04:9f:be:ef:02
33:33:00:00:00:01
01:00:5e:00:00:01
33:33:ff:be:ef:02
01:80:c2:00:00:00
01:80:c2:00:00:03
01:80:c2:00:00:0e
01:00:5e:00:00:fc
33:33:00:01:00:03
mirrors:
rxmirr0: ---
rxmirr1: ---
txmirr0: ---
txmirr1: ---
logical interfaces:
2: emac2
accepted: 13 rejected: 0 discarded: 0 processed: 13
egress: hif2
match-rules: ---
5: util
ingress: 0 egress: 0 discarded: 0 malformed: 0
flexible-filter: ---
ptp-mgmt-if: ---
MAC: ---
mirrors:
rxmirr0: ---
rxmirr1: ---
txmirr0: ---
txmirr1: ---
logical interfaces: ---
6: hif0
ingress: 105 egress: 57 discarded: 0 malformed: 0
flexible-filter: ---
ptp-mgmt-if: ---
MAC: ---
mirrors:
rxmirr0: ---
rxmirr1: ---
txmirr0: ---
txmirr1: ---
logical interfaces:
3: hif0
accepted: 29 rejected: 0 discarded: 0 processed: 29
egress: ---
match-rules: ---
7: hif1
ingress: 53 egress: 75 discarded: 0 malformed: 0
flexible-filter: ---
ptp-mgmt-if: ---
MAC: ---
mirrors:
rxmirr0: ---
rxmirr1: ---
txmirr0: ---
txmirr1: ---
logical interfaces:
4: hif1
accepted: 0 rejected: 0 discarded: 0 processed: 0
egress: ---
match-rules: ---
8: hif2
ingress: 37 egress: 13 discarded: 0 malformed: 0
flexible-filter: ---
ptp-mgmt-if: ---
MAC: ---
mirrors:
rxmirr0: ---
rxmirr1: ---
txmirr0: ---
txmirr1: ---
logical interfaces:
5: hif2
accepted: 0 rejected: 0 discarded: 0 processed: 0
egress: ---
match-rules: ---
9: hif3
ingress: 0 egress: 0 discarded: 31 malformed: 0
flexible-filter: ---
ptp-mgmt-if: ---
MAC: ---
mirrors:
rxmirr0: ---
rxmirr1: ---
txmirr0: ---
txmirr1: ---
logical interfaces:
6: hif3
accepted: 0 rejected: 0 discarded: 0 processed: 0
egress: ---
match-rules: ---
Command successfully executed. and the command libfci_cli logif-print returns:
DISCLAIMER: This is a DEMO application. It is not part of the production code deliverables.
0: emac0
accepted: 57 rejected: 0 discarded: 0 processed: 57
parent: emac0
egress: hif0
match-rules: ---
1: emac1
accepted: 75 rejected: 0 discarded: 0 processed: 75
parent: emac1
egress: hif1
match-rules: ---
2: emac2
accepted: 13 rejected: 0 discarded: 0 processed: 13
parent: emac2
egress: hif2
match-rules: ---
3: hif0
accepted: 29 rejected: 0 discarded: 0 processed: 29
parent: hif0
egress: ---
match-rules: ---
4: hif1
accepted: 0 rejected: 0 discarded: 0 processed: 0
parent: hif1
egress: ---
match-rules: ---
5: hif2
accepted: 0 rejected: 0 discarded: 0 processed: 0
parent: hif2
egress: ---
match-rules: ---
6: hif3
accepted: 0 rejected: 0 discarded: 0 processed: 0
parent: hif3
egress: ---
match-rules: ---
Command successfully executed. However, I would like to configure the M7 core PFE-master now.
My questions are:
Thank you for your support!
Best regards,
Guilherme
Hello @Joey_z ,
Ok, thank you very much.
Best regards,
Guilherme
hi,GuilhermeS32G
Thank you for your reply.
PFE MCAL driver does not have this function, thank you for your suggestion, I will report this problem.
BR
Joey
Hello @Joey_z ,
Thank you for your explanation.
I can see that the latest releases of the S32G Real-Time Driver AUTOSAR 4.4 for Cortex-M7 can be configured, built, and debugged using the S32 Design Studio. However, the S32G PFE MCAL 4.4 driver still requires EB Tresos Studio.
Is there any work in progress to make the future releases of the S32G PFE MCAL driver compatible with the S32 Design Studio?
Thanks again.
Best regards,
Guilherme
hi,GuilhermeS32G
It is recommended that you debug using Lauterbach Trace32 according to readme.txt requirements. The S32 Debug Probe can be debuggable by loading .elf files, but this is unstable and does not ensure that you can debug successfully, you can see the following way.
Joey_z_0-1730964157981.png
Joey_z_1-1730964169114.png
If the following problems occur, try loading the main.c file.
Joey_z_2-1730964191889.png
BR
Joey
Hello @Joey_z ,
Thank you for your reply.
I see, so that means I require the Lauterbach Trace32 debugger and the EB Tresos Studio IDE for successfully running this example.
Do you know if there is any movement inside NXP to migrate the PFE-DRV_S32G_M7_MCAL software to the S32 Design Studio IDE and supporting the S32 Debug Probe instead?
Best regards,
Guilherme
hi,GuilhermeS32G
To configure PFE-master for M7 core, you can refer to the PFE-DRV_S32G_M7_MCAL package MasterProject_RDB3 project. In the meantime, you can refer to the readme for more details to complete the setup. You can set IP_ADDRESS_CTRL_0 to set the IP address . RTD drivers must be installed, copy the installed RTD driver plugins and PFE driver plugin to Tresos plugins directory. Also, Run and debug the application with Lauterbach TRACE32.
Joey_z_0-1730879600804.png
Joey_z_1-1730879608076.png
BR
Joey