Hi everyone!
I've tried to compile an image for the t1024 based board. For the building I've used a Buildroot tools and fresh kernel 6.1.44. But ethernet interfaces doesn't up although
ip ashow me a list of interfaces
1: lo: mtu 65536 qdisc noqueue qlen 1000
link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
inet 127.0.0.1/8 scope host lo
valid_lft forever preferred_lft forever
inet6 ::1/128 scope host
valid_lft forever preferred_lft forever
2: eth0: mtu 1500 qdisc noop qlen 1000
link/ether 00:00:00:00:01:00 brd ff:ff:ff:ff:ff:ff
3: eth1: mtu 1500 qdisc noop qlen 1000
link/ether 00:00:00:00:01:01 brd ff:ff:ff:ff:ff:ff
4: eth2: mtu 1500 qdisc noop qlen 1000
link/ether 00:00:00:00:01:02 brd ff:ff:ff:ff:ff:ff
5: eth3: mtu 1500 qdisc noop qlen 1000
link/ether 00:00:00:00:01:03 brd ff:ff:ff:ff:ff:ff
6: tunl0@NONE: mtu 1480 qdisc noop qlen 1000
link/ipip 0.0.0.0 brd 0.0.0.0
7: sit0@NONE: mtu 1480 qdisc noop qlen 1000
link/sit 0.0.0.0 brd 0.0.0.0 trying
ip link set dev eth0 up give me an error
fsl_dpaa_mac ffe4e0000.ethernet eth0: init_phy() failedDuring a boot log I can watch this:
mdio_bus 0x0000000ffe4fc000: MDIO device at address 2 is missing.
mdio_bus 0x0000000ffe4fc000: MDIO device at address 6 is missing.
mdio_bus 0x0000000ffe4fd000: MDIO device at address 1 is missing.
mdio_bus 0x0000000ffe4fd000: MDIO device at address 2 is missing.
platform ffe488000.port: Adding to iommu group 15
platform ffe489000.port: Adding to iommu group 16
platform ffe48a000.port: Adding to iommu group 17
platform ffe48b000.port: Adding to iommu group 18
fsl_dpaa_mac ffe4e0000.ethernet: FMan MEMAC
fsl_dpaa_mac ffe4e0000.ethernet: FMan MAC address: 00:00:00:00:01:00
fsl_dpaa_mac ffe4e2000.ethernet: FMan MEMAC
fsl_dpaa_mac ffe4e2000.ethernet: FMan MAC address: 00:00:00:00:01:01
fsl_dpaa_mac ffe4e4000.ethernet: FMan MEMAC
fsl_dpaa_mac ffe4e4000.ethernet: FMan MAC address: 00:00:00:00:01:02
fsl_dpaa_mac ffe4e6000.ethernet: FMan MEMAC
fsl_dpaa_mac ffe4e6000.ethernet: FMan MAC address: 00:00:00:00:01:03
fsl_dpaa_mac ffe4e0000.ethernet eth0: Probed interface eth0
fsl_dpaa_mac ffe4e2000.ethernet eth1: Probed interface eth1
fsl_dpaa_mac ffe4e4000.ethernet eth2: Probed interface eth2
fsl_dpaa_mac ffe4e6000.ethernet eth3: Probed interface eth3Is it true that the MDIO is not configured correctly? I use a device tree from kernel source, Uboot has been kept from previous image (kernel version 3.12.27). I've loaded a new rootfs, dtb and uImage into ram and ran from there.
ethtool show me the next:
ethtool eth0
Settings for eth0:
Supported ports: [ ]
Supported link modes: Not reported
Supported pause frame use: No
Supports auto-negotiation: No
Supported FEC modes: Not reported
Advertised link modes: Not reported
Advertised pause frame use: No
Advertised auto-negotiation: No
Advertised FEC modes: Not reported
Speed: Unknown!
Duplex: Half
Port: Twisted Pair
PHYAD: 0
Transceiver: internal
Auto-negotiation: off
MDI-X: Unknown
Current message level: 0x00002037 (8247)
drv probe link ifdown ifup hw
Link detected: no Is there some tricks to use ethernet on T1024?
I tried to compile new image from QorIQ SDK 2.0, but it has a very old tools and stopped with a lot of errors.
Please modify the dts file arch/powerpc/boot/dts/fsl/t1024rdb.dts according to your custom board. Please modify "reg" values to your real PHY addresses at mdio@fc000 and mdio@fd000.
fman@400000 {
enet0: ethernet@e0000 {
phy-handle = <&xg_aqr105_phy3>;
phy-connection-type = "xgmii";
sleep = <&rcpm 0x80000000>;
};
enet1: ethernet@e2000 {
sleep = <&rcpm 0x40000000>;
};
enet2: ethernet@e4000 {
phy-handle = <&rgmii_phy2>;
phy-connection-type = "rgmii";
sleep = <&rcpm 0x20000000>;
};
enet3: ethernet@e6000 {
phy-handle = <&rgmii_phy1>;
phy-connection-type = "rgmii";
sleep = <&rcpm 0x10000000>;
};
mdio0: mdio@fc000 {
rgmii_phy1: ethernet-phy@2 {
reg = <0x2>;
};
rgmii_phy2: ethernet-phy@6 {
reg = <0x6>;
};
};
xmdio0: mdio@fd000 {
xg_aqr105_phy3: ethernet-phy@1 {
compatible = "ethernet-phy-ieee802.3-c45";
reg = <0x1>;
};
sg_2500_aqr105_phy4: ethernet-phy@2 {
compatible = "ethernet-phy-ieee802.3-c45";
reg = <0x2>;
};
};
};