Hello, @Robin_Shen
I am currently developing firmware for the S32K314 series without using the RTD.
While searching for clock drivers, I came across a response you posted and checked the project.
It seems that there is a driver folder in the project, which leads me to believe that there might be drivers available for the non-RTD version.
Is there any way I can get access to the drivers for each module?
Hi
The Baremetal Example Codes used to be available for download from docstore.nxp.com. But this was before the release of S32K3 RTD and is no longer available for download and is not recommended.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------