親愛なる専門家の皆様、
meta-qt6機能を使用してイメージをビルドしようとしていますが、Bitbakeの実行中に次のエラーが発生しました。何度も試行しても、問題は解決しません。以下のエラーを解決するのを手伝ってもらえますか?
calixto-systems@calixtosystems-HP-Notebook:/media/drive_A/eagle/nxp-linux-platform/yocto/calixto-yocto-bsp/build-xwayland$ bitbake imx-image-full
WARNING: You have included the meta-virtualization layer, but 'virtualization' has not been enabled in your DISTRO_FEATURES. Some bbappend files may not take effect. See the meta-virtualization README for details on enabling virtualization support.
Loading cache: 100% |##########################################################################################################| Time: 0:00:01
Loaded 4742 entries from dependency cache.
Parsing recipes: 100% |########################################################################################################| Time: 0:00:01
Parsing of 3195 .bb files complete (3194 cached, 1 parsed). 4743 targets, 371 skipped, 3 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "2.0.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6ull-versa256"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "5.15-kirkstone"
TUNE_FEATURES = "arm vfp cortexa7 neon thumb callconvention-hard"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:24a3f7b3648185e33133f5d96b184a6cb6524f3d"
meta-oe
meta-multimedia
meta-python = "HEAD:744a4b6eda88b9a9ca1cf0df6e18be384d9054e3"
meta-freescale = "HEAD:c82d4634e7aba8bc0de73ce1dfc997b630051571"
meta-freescale-3rdparty = "HEAD:5977197340c7a7db17fe3e02a4e014ad997565ae"
meta-freescale-distro = "HEAD:d5bbb487b2816dfc74984a78b67f7361ce404253"
meta-calixto-nxp = "HEAD:c547c4347d887a7212bd3d306f0601c21ff36d65"
meta-bsp
meta-sdk
meta-ml
meta-v2x = "HEAD:ca68ab5d25322b51f54564275c84ab8de3c74ea6"
meta-nxp-demo-experience = "HEAD:52eaf8bf42f8eda2917a1c8c046003c8c2c8f629"
meta-chromium = "HEAD:e232c2e21b96dc092d9af8bea4b3a528e7a46dd6"
meta-clang = "HEAD:c728c3f9168c8a4ed05163a51dd48ca1ad8ac21d"
meta-gnome
meta-networking
meta-filesystems = "HEAD:744a4b6eda88b9a9ca1cf0df6e18be384d9054e3"
meta-qt6 = "HEAD:ed785a25d12e365d1054700d4fc94a053176eb14"
meta-virtualization = "HEAD:9482648daf0bb42ff3475e7892542cf99f3b8d48"
Initialising tasks: 100% |#####################################################################################################| Time: 0:00:13
Sstate summary: Wanted 3349 Local 0 Mirrors 0 Missed 3349 Current 101 (0% match, 2% complete)
NOTE: Executing Tasks
WARNING: cracklib-2.9.8-r0 do_fetch: Failed to fetch URL git://github.com/cracklib/cracklib;protocol=https;branch=master, attempting MIRRORS if available
ERROR: cracklib-2.9.8-r0 do_fetch: Fetcher failure: Unable to find revision d9e8f9f47718539aeba80f90f4e072549926dc9c in branch master even from upstream
ERROR: cracklib-2.9.8-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'git://github.com/cracklib/cracklib;protocol=https;branch=master')
ERROR: Logfile of failure stored in: /media/drive_A/eagle/nxp-linux-platform/yocto/calixto-yocto-bsp/build-xwayland/tmp/work/cortexa7t2hf-neon-poky-linux-gnueabi/cracklib/2.9.8-r0/temp/log.do_fetch.919291
ERROR: Task (/media/drive_A/eagle/nxp-linux-platform/yocto/calixto-yocto-bsp/sources/poky/meta/recipes-extended/cracklib/cracklib_2.9.8.bb:do_fetch) failed with exit code '1'
WARNING: cracklib-native-2.9.8-r0 do_fetch: Failed to fetch URL git://github.com/cracklib/cracklib;protocol=https;branch=master, attempting MIRRORS if available
ERROR: cracklib-native-2.9.8-r0 do_fetch: Fetcher failure: Unable to find revision d9e8f9f47718539aeba80f90f4e072549926dc9c in branch master even from upstream
ERROR: cracklib-native-2.9.8-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'git://github.com/cracklib/cracklib;protocol=https;branch=master')
ERROR: Logfile of failure stored in: /media/drive_A/eagle/nxp-linux-platform/yocto/calixto-yocto-bsp/build-xwayland/tmp/work/x86_64-linux/cracklib-native/2.9.8-r0/temp/log.do_fetch.930524
ERROR: Task (virtual:native:/media/drive_A/eagle/nxp-linux-platform/yocto/calixto-yocto-bsp/sources/poky/meta/recipes-extended/cracklib/cracklib_2.9.8.bb:do_fetch) failed with exit code '1'また、上記のそれぞれのリポジトリを取得するための適切なリンクを共有してください。
よろしく
ラビクマール