1977952_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1977952_en-US

1977952_en-US

imx8-image-full but not need machine learning function features.

Hi All,

kernel:5.4

evk:imx8mq-evk

I can build code by imx8-image-full command, but I not need machine learning fearures.

How to remove the Machine Learning features ?

or, How to add QT 5 on imx8-image-multimedia build?

Re: imx8-image-full but not need machine learning function features.

The section <5.6.6 Qt 6 and QtWebEngine browsers> and <5.6.7 NXP eIQ machine learning> from Yocto User Guide can be a reference for such add or remove the required features.

Embedded Linux for i.MX Applications Processors | NXP Semiconductors

To add QT, a reference can be like, add IMAGE_INSTALL:append = " packagegroup-qt5-imx qtbase" to conf/local.conf


Regards

Harvey

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 05:06 PM
更新者: