1977598_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1977598_en-US

1977598_en-US

What CRC16 standard is being implemented?

I've been trying to write software to set the EAS flag on an ICODE SLIX IC. According to the datasheet, the SET EAS and RESET EAS flags both require a CRC16 check on the command, but I can't seem to find a consistent reference for which standards (e.g., polynomial, initialiser, etc.) is being used. Is anyone able to point me to an NXP official source for the CRC16 standard being used?

Re: What CRC16 standard is being implemented?

Thanks Daniel - that ISO standard had everything I need.

Re: What CRC16 standard is being implemented?

Hi  @BenDund :


CRC16 is calculated by the VCD once the request is sent to the VICC (in that case the ICODE SLIX) - details on that can be found in the ISO15693 standard.


Regards

Daniel

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 11:11 PM
更新者: