1976702_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1976702_en-US

1976702_en-US

eMIOS PWM output disable(OPWMB MODE)

hello experts:

when (OPWMB mode)PWM dutycylce is 100%, it can not be output disabled by ODIS register.

But if the dutycycle <100%,the (OPWMB mode) PWM can be disabled output by ODIS register.Such as the dutycle is 99% the PWM(OPWMB mode) can be disable by ODIS register.

And if the PWM mode is OPWFMB,it can be disbled by ODIS when it's dutycle is 100%.

why?And have any method to solve?

FRIDAY618_1-1729231871069.png

FRIDAY618_2-1729231892122.png

FRIDAY618_3-1729231907646.png

FRIDAY618_4-1729232169442.png







Re: eMIOS PWM output disable(OPWMB MODE)

thanks,it works。i knew how to do。

Re: eMIOS PWM output disable(OPWMB MODE)

FRIDAY618_0-1729501145812.png

FRIDAY618_1-1729501206920.png

FRIDAY618_2-1729501254757.png

 I used the demo but not solved problem?

I toggled gpio_34 pin and connect gpio_34 with PTB4(TRGMUX_in,1).when the pwm dutycle is 50%.it can be disabled by ODIS.

when the pwm dutycle is 100%.it still can not be disable.




Re: eMIOS PWM output disable(OPWMB MODE)

Hi@FRIDAY618

This is a test demo i made before and please have a try.

Senlent_0-1729494502461.png


タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 10:44 PM
更新者: