Trying to write the imx 8 nano EVK Linux image that I download from NXP to my imx 8 nano EVK via UUU. I think that should be a very simple, ordinary thing to do. But it fails.
I downloaded LF_v6.6.36-2.1.0_images_IMX8MNDDR3LEVK.
Using the latest UUU, v 1.5.182.
UUU recognizes the nano and starts processing but fails quickly with error: LIBUSB_ERROR_TIMEOUT.
I've retried many times, but fails the same every time.
FWIW: I also have a mini EVK and I can write the mini EVK image to it without issue.
Any ideas what is causing the failure? And how to fix?
Here's the output from my run:
PS i.MX-8M-Nano-EVK\LF_v6.6.36-2.1.0_images_IMX8MNDDR3LEVK> .\uuu.exe -lsusb
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.182-0-gda3cd53
Connected Known USB Devices
Path Chip Pro Vid Pid BcdVersion Serial_no
====================================================================
2:1 MX815 SDPS: 0x1FC9 0x013E 0x0001 2D2A6A09DAB58857
PS i.MX-8M-Nano-EVK\LF_v6.6.36-2.1.0_images_IMX8MNDDR3LEVK> .\uuu.exe -V .
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.182-0-gda3cd53
Build in config:
Pctl Chip Vid Pid BcdVersion Serial_No
==================================================
SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]
SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]
SDPS: MX8DXL 0x1fc9 0x0147
SDPS: MX28 0x15a2 0x004f
SDPS: MX815 0x1fc9 0x013e
SDPS: MX865 0x1fc9 0x0146
SDPS: MX8ULP 0x1fc9 0x014a
SDPS: MX8ULP 0x1fc9 0x014b
SDPS: MX93 0x1fc9 0x014e
SDPS: MX91 0x1fc9 0x0159
SDPS: MX95 0x1fc9 0x015d
SDPS: MX95 0x1fc9 0x015c
SDP: MX7D 0x15a2 0x0076
SDP: MX6Q 0x15a2 0x0054
SDP: MX6D 0x15a2 0x0061
SDP: MX6SL 0x15a2 0x0063
SDP: MX6SX 0x15a2 0x0071
SDP: MX6UL 0x15a2 0x007d
SDP: MX6ULL 0x15a2 0x0080
SDP: MX6SLL 0x1fc9 0x0128
SDP: MX7ULP 0x1fc9 0x0126
SDP: MXRT106X 0x1fc9 0x0135
SDP: MX8MM 0x1fc9 0x0134
SDP: MX8MQ 0x1fc9 0x012b
SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]
SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]
SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998]
SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]
SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]
SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]
FBK: 0x066f 0x9afe
FBK: 0x066f 0x9bff
FBK: 0x1fc9 0x0153
FB: 0x0525 0xa4a5
FB: 0x18d1 0x0d02
FB: 0x3016 0x0001
FB: 0x1fc9 0x0152
FB: 0x0483 0x0afb
Wait for Known USB Device Appear...
New USB Device Attached at 2:1-2D2A6A09DAB58857
2:1-2D2A6A09DAB58857>Start Cmd:SDPS: boot -f imx-boot-imx8mnddr3levk-sd.bin-flash_ddr3l_evk
10%2:1-2D2A6A09DAB58857>Fail HID(W): LIBUSB_ERROR_TIMEOUT (-7)(20.05s)
libusb: warning [libusb_exit] device 2.0 still referenced
libusb: warning [libusb_exit] device 1.0 still referenced
libusb: warning [libusb_exit] device 2.6 still referenced
libusb: warning [libusb_exit] device 1.1 still referenced
libusb: warning [libusb_exit] device 2.2 still referenced
PS i.MX-8M-Nano-EVK\LF_v6.6.36-2.1.0_images_IMX8MNDDR3LEVK>Hi,
You are flashing DDR3 binaries to LPDDR4 board, please try flashing the proper LPDDR4 board.
uuu -b imx-boot-imx8mnevk-sd.bin-flash_evk imx-image-full-imx8mnevk.wic
Regards
Trying again to attach pics. Seems to work better with jpg files instead of .zip.
I did attach a zip file with images, but I don't see it in the thread now. I then tried replying again and attaching a simple text file, but I don't think it worked. The file seems to start to upload; showing in the drag and drop box, but then it disappears. And the message 'maximum attachments allowed' count stays at 5. So, I doubt the pic zip got attached in my last msg.
Maybe you mean top side and bottom side pics. Attached.
Hi,
Thank you for your interest in NXP Semiconductor products,
Could you share top and bottom pictures of both of your boards?
Regards