1971656_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1971656_en-US

1971656_en-US

LPC54628 usb0 FS HC transfer failed after a USB connection inactive for a long

I use LPC54628 controller usb0 FS HC connect to a usb device, and it runs 24/7. I was told USB device is configured never go to sleep or deep-sleep, or Deep power-down mode.

The issue is when a USB connection inactive for a long time period, the first usb transfer always failed (kStatus_USB_TransferFailed) after usb reset, communication recovered. Base on user manual, by default, usb0 deep-sleep is sw configured,  and Deep power-down mode is "off"

Question:
1. if "deep-sleep" is sw configured, what is by default?
2. could you send me a demo code to explicitly to turn  deep-sleep off?

Thank you,

LPC546xxLPC54xxxUSBRe: LPC54628 usb0 FS HC transfer failed after a USB connection inactive for a longLPC54628 operate as a USB host

"By default, it is in active mode." I think this is the answer I need. Thanks
Re: LPC54628 usb0 FS HC transfer failed after a USB connection inactive for a long

Hello @changlin_ren 


LPC54628  operate as a USB device or host?  By default, it is in active mode. We need to check the code to determine the exact configuration. How about first running a USB demo from the SDK? Then I can help you check it.


BR

Alice


Re: LPC54628 usb0 FS HC transfer failed after a USB connection inactive for a longrewrite the issue:
The issue is when a USB connection inactive for a long time period, the first usb transfer always failed (kStatus_USB_TransferFailed).
After usb reset, communication recovered
Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 08:22 PM
Updated by: