1968889_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1968889_en-US

1968889_en-US

emios trigger

Hi

I am trying to test the system so that the BCTU is triggered via PWM  at every flag generation. I would like to plot the flag that triggers the BCTU on an oscilloscope. How do I do that?

I am trying to get the generating emios_pwm flag outputted on an oscilloscope, by using the EMIOS_PWM_IP_INTERRUPT_REQUEST callback function, but i am not sure the interrupt for EMIOS is working. I have attached the project below

RTD 4.00

S32K344 T172

Re: emios trigger

Hi@Ayaz

This is a demo i made before and the RTD version is 2.0.3, maybe you can refer to it.

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 04:29 PM
Updated by: